Skip to main content
50_ohm
Visitor II
Jan 8, 2026 11:48 AM UTC
Solved

STM32WL5MOC LSE 32kHz accuracy

Hi, 
 
In the STM32WL5MOC datasheet I can find the 32MHz TXCO HSE accurancy, but not the LSE 32kHz RTC clock accuracy. Could someone look into this and provide the min/max values similar to TXCO characteristics in Table 10?
 
Best Regards,
Dave
Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
Jan 8, 2026 1:41 PM UTC

Welcome @50_ohm, to the community!

I am very sorry that this specification is not mentioned in the data sheet. However, I would like to point out that the frequency accuracy of the 32MHz HSE is an essential prerequisite for proper functioning in some frequency bands.

The built-in LSE crystal has a frequency tolerance of ±20ppm at 25°C and a parabolic coefficient of -0.04ppm/°C². If there are any deviations, you can use the smooth calibration function included in the built-in STM32WL55JC, together with the temperature sensor if necessary. I have also explained the smooth calibration in a more understandable way in this thread. There is also a Knowledge Base article describing the smooth calibration for the STM32U575 which uses a similar RTC.

Hope this answers your question?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

1 reply

Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
Jan 8, 2026 1:41 PM UTC

Welcome @50_ohm, to the community!

I am very sorry that this specification is not mentioned in the data sheet. However, I would like to point out that the frequency accuracy of the 32MHz HSE is an essential prerequisite for proper functioning in some frequency bands.

The built-in LSE crystal has a frequency tolerance of ±20ppm at 25°C and a parabolic coefficient of -0.04ppm/°C². If there are any deviations, you can use the smooth calibration function included in the built-in STM32WL55JC, together with the temperature sensor if necessary. I have also explained the smooth calibration in a more understandable way in this thread. There is also a Knowledge Base article describing the smooth calibration for the STM32U575 which uses a similar RTC.

Hope this answers your question?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.