Skip to main content
LVanr.1
Associate II
Dec 12, 2024 8:55 AM UTC
Solved

stm32wb0x error on build of stm32cube example projects

I'm trying to import the sample project BLE_Skeleton. On build I get the following error:

fatal error: osal.h: No such file or directory

The same error occurs for other BLE sample projects.
The error also happened for BLE_p2pServer but was fixed.

When can the problem be fixed for the other sample projects ?

This topic has been closed for replies.
LVanr.1
LVanr.1Best answer
Associate II
Dec 20, 2024 10:28 AM UTC

(I got the solution via direct contact with an ST employee)

CubeMX > Project Manager > Code Generation > select 'Add necessary library files as reference.....'
Save and compile.

8 replies

Andrew Neil
Super User
Dec 12, 2024 9:47 AM UTC

how are you obtaining the sample project BLE_Skeleton?

If downloading from GitHub, see:

https://community.st.com/t5/stm32-mcus/downloading-stm32cube-packages-from-github-correctly/ta-p/725288 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
LVanr.1
LVanr.1Author
Associate II
Dec 12, 2024 9:57 AM UTC

In stm32Cube I do: File > Import > Import STM32Cube Example

ST Technical Moderator
Dec 12, 2024 1:49 PM UTC

Hello @LVanr.1 ,

Maybe you have wrong paths! Try adding correct paths to the include directories (Go to Project options ->C/C++ tab->Include paths)

Otherwise, please provide more details on your CubeWB0 firmware package version and CubeIDE version used, the exact project path and steps?

 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
LVanr.1
LVanr.1Author
Associate II
Dec 12, 2024 2:25 PM UTC

Let me mention that I am learning about BLE development on ST (but I am very familiar with BLE development in Eclipse on other hardware platforms).

I had installed STM32Cube version 1.16.0. I installed BLE_Sketeton as well as other example projects BLE_p2pServer  and BLE_Beacon. All of these compiled properly and worked on my development board SRM32wb09KE.
A while ago some example projects did not compile and required an upgrade of MX. When warned that a new version of Cube was available I accepted doing the upgrade -- STM32Cube was automatically upgraded to version 1.17.0. MX was also upgraded. To make sure that the example projects were in sync I deleted them and installed them. That is where the compile error occurred. At first, project BLE_p2pServer also had the compile error. Little later I re-installed BLE_p2pServer and the compile error had gone but not for the other BLE sample projects.

I now desperately need BLE_Skeleton to start product development, hence my error posting.

I may assume that example projects are correct and working. It is not up to me to set paths or whatever.

About installing BLE_Skeleton. In stm32Cube I do: File > Import > Import STM32Cube Example. In MCU/MPU select STM32WB09KEV6TR. From the list of sample projects, select BLE_Skeleton, then Next --> project gets installed. Compile ==> error.

LVanr.1
LVanr.1Author
Associate II
Dec 20, 2024 8:49 AM UTC

This issue is resolved.

Andrew Neil
Super User
Dec 20, 2024 10:22 AM UTC

For the benefit of future readers who may come here looking for solutions to the same problem, please describe how you resolved it.

Then mark your description as The Solution.

See: https://community.st.com/t5/community-guidelines/help-others-to-solve-their-issues/ta-p/575256

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
LVanr.1
LVanr.1AuthorBest answer
Associate II
Dec 20, 2024 10:28 AM UTC

(I got the solution via direct contact with an ST employee)

CubeMX > Project Manager > Code Generation > select 'Add necessary library files as reference.....'
Save and compile.

Andrew Neil
Super User
Dec 20, 2024 10:46 AM UTC

Thanks.  Now please mark that as the solution.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.