Skip to main content
OTOMA.2
Associate
May 12, 2022 9:44 AM UTC
Question

Problem loading stack on a nucleo STM32WB55

It's a board I've been using for a while, and I'm struggling loading a new stack onto it.

Here are the steps I've executed:

1/ powercycle

2/ start FUS

3/ delete image

4/ powercycle

5/ start FUS

6/ get FUS info: FUS_IDLE | FUD_NO_ERROR | Version=1.1.1.0 | stackversion=1.13.3.2 | FUS opeatorver = 3.1.0

7/ erase memory to load the stack (stack full basic v1.13.3.2, address @0x080D0000)

8/ firmware upgrade of the stack (with verify download enabled, and first install (tested without too))

9/ ERR_IMG_NOT_FOUND.

The weird part is that after a firmware delete and a powercycle, the fus still report the current stack version being v1.13.3.2. However, after checking with a getfwinfo, I get the stack_type == 0. And the SFSA is 0xF4, so only the FUS is protected, leaving the whole Flash writable for the image (which has been verified!)

Can you advise?

This topic has been closed for replies.

18 replies

MM..1
Super User
May 12, 2022 1:10 PM UTC

Maybe you need FUS update.

OTOMA.2
OTOMA.2Author
Associate
May 12, 2022 1:40 PM UTC

I'll try that !

OTOMA.2
OTOMA.2Author
Associate
May 12, 2022 1:44 PM UTC

Ok, just tested, trying to install the firmware update with the FUS_fw.bin @ 0x080EC000, and I get the same error IMG_NOT_FOUND.

Could any ST support reply with a procedure to recover the nucleo?

Remi QUINTIN
ST Technical Moderator
May 12, 2022 1:46 PM UTC

Indeed you should better used the FUS available in the FW package version of the new FW you want to update.

Note that FUS V1.2.0 is the latest and definite version. So once you updated this version, you should never have to load a new FUS. I see your FUS version is 1.1.1. So I would recommend to update it to FUS v1.2.0 which is available in WB FW package V1.13.x.

OTOMA.2
OTOMA.2Author
Associate
May 12, 2022 1:48 PM UTC

So, As the latest FUS fw from the WB_1.13.3 package is not loading (IMG_NOT_FOUND, as stated before), what should I do?

OTOMA.2
OTOMA.2Author
Associate
May 12, 2022 1:50 PM UTC

Here is the stm32cubeprogrammer log:

 15:49:56 : Firmware delete Success

 15:49:56 : Download Stack/FUS image at address 0x80ec000 ...

 15:49:56 : Memory Programming ...

 15:49:56 : Opening and parsing file: stm32wb5x_FUS_fw.bin

 15:49:56 :  File         : stm32wb5x_FUS_fw.bin

 15:49:56 :  Size         : 23,92 KB

 15:49:56 :  Address      : 0x080EC000

 15:49:56 : Erasing memory corresponding to segment 0:

 15:49:56 : Erasing internal memory sectors [236 241]

 15:49:56 : Download in Progress:

 15:49:57 : File download complete

 15:49:57 : Time elapsed during download operation: 00:00:00.634

 15:49:57 : Verifying ...

 15:49:57 : Read progress:

 15:49:57 : Download verified successfully

 15:49:57 : Firmware Upgrade process started ...

 15:49:57 : Application is running, Please Hold on...

 15:50:09 : Reconnecting...

 15:50:09 : Reconnected !

 15:50:09 : Error: FUS_STATE_IMG_NOT_FOUND

OTOMA.2
OTOMA.2Author
Associate
May 12, 2022 2:58 PM UTC

Could any ST member advise on why is the device stuck. I'm not sure if this is a serious issue, but from production reliability it clearly is not acceptable. I'm wondering what sequence could have led the chip to such a state.

Remi QUINTIN
ST Technical Moderator
May 12, 2022 3:05 PM UTC

Strange!

I assume your are using the ST LINK port to download the FUS.

Could you erase the user space by setting the RDP value to 0xBB and then back to 0xAA.

Then retry to upgrade the FUS.

OTOMA.2
OTOMA.2Author
Associate
May 12, 2022 4:42 PM UTC

Thanks Remi for your reply.

However, it didn't go well.

1/ I changed to BB,

2/ powercycle

3/ I changed to AA

4/ powercycle

5/ I loaded FUS upgrade to 0x080EC000

6/ IMG_NOT_FOUND

7/ I slipped onto Start wireless stack

8/ The chip FUS is unresponsive

9/ powercycle

10/ The chip FUS is unresponsive.

I guess this is a terminal state for the chip, I don't have much hope. However this is clearly a critical tearing condition. Ths chip is not functional anymore. If you have services who can investigate I can arrange a shipment for the board.

BR

MM..1
Super User
May 12, 2022 4:54 PM UTC

Seems as you firmware files is placed on long path with spaces. Copy folder with bin files to for example C:\STWBFW

OTOMA.2
OTOMA.2Author
Associate
May 12, 2022 6:33 PM UTC

Actually I've checked, and I don't have any space in the path:

/home/user/STM32Cube/Repository/STM32Cube_FW_WB_V1.13.3/Projects/STM32WB_Copro_Wireless_Binaries/STM32WB5x/stm32wb5x_FUS_fw.bin

MM..1
Super User
May 13, 2022 6:29 AM UTC
First update LOG show ok upgrade for FUS, after this FUS report no image say BLE fw not loaded or using user keys.
Try use latest STMProgrammer version ... Check flash size and install addr table.