Skip to main content
Visitor II
Jun 3, 2025 8:57 AM UTC
Question

LRWAN2 end node and gateway setup

 

Hello sir/mam

 

  1. .When I am trying to connect my NUCLEO-F746ZG LRWAN2 gateway board to TTN network I am not able to do can you guide me with this gateway connection with the network

==> in this explain whether we need DHCP connection or with the static IP can we connect.

  1. Also parallelly I am trying to setup the end node The board is not responding means There is only a blank screen in the tera term though i have flashed the firmware

Steps follows for end node setup

  1. Downloaded I-CUBE-LRWAN package
  2. In this navigated to the location projects->NUCLEO-LO73RZ->Applications->LoRaWANEndNode->sx1272 In this added the board EUI , APP keys frequency etc...

but still in the tera term Its blank black screen

 

Kindly help me in setting the end node and gateway setup

 

 

earliest response is very much helpful

 

This topic has been closed for replies.

1 reply

Andrew Neil
Super User
Jun 4, 2025 9:37 AM UTC
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.