Skip to main content
CKim.8
Associate
Jul 23, 2021 6:45 AM UTC
Solved

LRWAN_V2.0.0 PingPong doesn't work.

I'm using NUCLEO_L073RZ with LRWAN NS1 which included in P-NUCLEO LRWAN 3.

​

I tried to communicate two end devices with SubGhz_Phy project in STM32CubeExpansion_LRWAN_V2.0.0, but it doesn't work.

It seems to using SPI, but MOSI(PA7) and MISO(PA6) is connected with LIS3MDL and NSS(PB6) and CLK(PA5) is not connected to anywhere.

Am I using wrong project, or missed somthing?

Sorry for my English.

This topic has been closed for replies.
Imen.DBest answer
ST Technical Moderator
Jul 23, 2021 9:37 AM UTC

Hello @CKim.8​ and welcome to the Community :)

It seems there is an issue with I-CUBE-LRWAN and fixes will be integrated in the new package released version.

The root cause of the problem : the missing "sys_conf.h" header file in uart.c, in addition to there was a memory allocation problem.

Please have a look at this post for more details, which contains the fixes proposed by JCOUP in his last comments, and check if you have the same conditions as described.

Hope this helps you!

When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks

3 replies

Imen.DBest answer
ST Technical Moderator
Jul 23, 2021 9:37 AM UTC

Hello @CKim.8​ and welcome to the Community :)

It seems there is an issue with I-CUBE-LRWAN and fixes will be integrated in the new package released version.

The root cause of the problem : the missing "sys_conf.h" header file in uart.c, in addition to there was a memory allocation problem.

Please have a look at this post for more details, which contains the fixes proposed by JCOUP in his last comments, and check if you have the same conditions as described.

Hope this helps you!

When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Tesla DeLorean
Guru
Jul 23, 2021 1:05 PM UTC

Are the LRWAN-NS1 boards available individually?  RisingHF RHF0M003-LF20

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..