Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Most recent activity
Due to to much emails, I overead the confirmation Mail with the Confirmation Button. Is there a chance to participate like I have confirmed correct?Thanks Martin
Hi,Like many others, I received an email stating that after not confirming my booking, my seat has been allocated to another participant. I had failed to notice the original email, as it had been marked as spam by my email filters... This is really unfortunate, as I had been really looking forward to the workshop. Any advice on how to still get in?
I'm confirming myattendance at IoT connectivity with STM32 LoRa-enabled SoC, from theory to practice - March 30.Regards,Ondrej
..
I have soldered up my first STM32WLE5CCU6 project board, and it buzzed out nicely before I gave it power. Now VDD is permanently shorted to ground...I'm happy to try again, but: what is the minimum number of pins/components that I need to connect just to boot the MCU? If I leave various peripherals (especially the RF stage!) unconnected - and don't activate them in the software - what is the minimum I can get away with?Thanks!
Hi,we've been developing with stm32wb55 for some time and found that some combinations of STOP2 and radio usage causes permanent damage to RX path.It looks like that: device announce stops at some point and power consumption raises(+10mA). After reset device starts announce again, but doesn't receive anything.Flashing TransparentVCP and checking RX with CubeMonitorRF shows RSSI -108dBmWiping flash and re-flashing radio and firmware doesn't help.Overall we've been following all application notes on power, radio, LSE/HSE. The only significant difference is antenna(we use IMD by Ethertronics/AVX 1001312) and software(we use STOP2 in between announces and prevent sleep only when connection arrives). Disabling STOP2 prevents damage, but completely unacceptable in terms of UX and power consumption.Since radio is a black box we are completely puzzled by this behavior and were unable to trace cause of damage.Is there any way to examine radio path internals (like on st25)? As I understand AT0,
Hi all, I'm reading some code and compiling some examples before receive NUCLEO-WL55JC board.Problems with this Example: [CM0PLUS]en.stm32cubewl\STM32Cube_FW_WL_V1.0.0\Projects\NUCLEO-WL55JC\Applications\LoRaWAN\LoRaWAN_End_Node_DualCoreFreeRTOSConsola Error:c:\st\stm32cubeide_1.2.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.7-2018-q2-update.win32_1.5.0.202011040924\tools\arm-none-eabi\bin\ld.exe: LoRaWAN_End_Node_DualCoreFreeRTOS_CM0PLUS.elf section `.text' will not fit in region `ROM'c:\st\stm32cubeide_1.2.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.7-2018-q2-update.win32_1.5.0.202011040924\tools\arm-none-eabi\bin\ld.exe: region `ROM' overflowed by 7360 bytescollect2.exe: error: ld returned 1 exit statusmake: *** [makefile:69: LoRaWAN_End_Node_DualCoreFreeRTOS_CM0PLUS.elf] Error 1"make -j4 all" terminated with exit code 2. Build might be incomplete.To try to correct this error, I add optimization (-Os) to redu
This is for the STM32WB5MMG, on page 11/31 of the datasheet.
Hi,Is there was a way to easily force a double bit ECC error to test recovery path?I'd like to verify that my application can recover from an unexpected watchdog / shutdown while a write to internal flash is in progress (i.e during an OTA update).I found this related thread about the STM32L4 and I see there is no way to test this path for the L4 series but was wondering if there's a way with the WB series.Thanks!
Currently I have decided to use the P-Nucleo WB55 pack that has Nucle 68 WB55RG and a dongle both of which have 2.4 Ghz radio transceivers to facilitate BLE interaction between the wearables. But the dongle does not have a PWM pin using which I could control a vibrating motor. I need suggestions to replace both of my micro-controllers.
I'm very new to this and it would be nice to have someone to talk to and exchange thoughts and get help to navigate STM32CubeWL LoRaWan/Sigfox examples.
Since Friday, generate an example from STM32CubeMX plugin is impossible for STM32WB series. Plugin is looking for a firmware package V1.11.0 which doesn't exist (no release in github repo, and newest tag is v1.10.1)does anyone already experienced this issue?ThanksPierre
I'm trying to make the "BLE_Beacon" example found inside the "STM32CubeWB" file work with the STM32CubeIDE and the P-NUCLEO WB55 board. The program compiles correctly but I can't see the beacons. Debugging I saw that when it arrives in the UTIL_SEQ_Run( UTIL_SEQ_DEFAULT ); I'm running STM32CubeIDE 1.5.1. I've used the nRF Connect and STBLE Toolbox but I don't see the beacon. Is there something I can try to get more visibility?
Hi I have two custom boards with stm32wb55 with a external crystal oscillator for the rtc. One device should be the master and the other is the slave. Master should set the rtc for the slave. Is it possible to sync them over ble with a precision of 1 ms? My other option is nfc, to exchange the data between them, to set the rtc.What is the best way to sync this two devices?Thanks
Hi,I am starting a project for the STM32WL using the SubGhz example application.I want to change the content of the subghz application to have my own behavior with my own frames sent and received.If I modify the file and I regenerate code using CubeMX, my functions are deleted and are replaced with the example application (Ping Pong).Is there a way to exclude some files from code generation ? Or maybe a way to tell CubeMX that my project is no longer just the PingPong example project ?Regards.
Hello. What is the value of the internal reference voltage of STM32WB55RGV6 MCU?Is it 1,212 V or 2,048 / 2,5 V?
Hello. What is the exact value of T_coeff_vrefint? I'm planning to use internal reference voltage buffer (VREFBUF) output pin in my application.
Stm32wb BLE callback function: void hci_disconnection_complete_event( uint8_t Status, uint16_t Connection_Handle, uint8_t Reason ){ printf("hci_disconnection_complete_event");}not working.STM32WB use a utility function to control the BLE functionality.some observed points are -connection/disconnection event monitor using SVCCTL_App_Notification() function only. ble functionality is control by UTIL_SEQ_Run() function, which is call in loop. UTIL_SEQ_Run() function run a single task on calling.Connection complete and disconnection complete events are detected using IPCC_C1_RX_IRQHandler() and IPCC_C1_TX_IRQHandler() interrupt handlers, which are called after every IPCC transmission/reception event.
I am working on a project using the STM32WB55xx series. I'm trying to read the Device Information Table (AN5185 Section 6.6.1, pg 17) using a bash script and the STM32 Programmer CLI.According to the documentation (AN5185 Section 1.2 page 3) I should be reading the IPCCDBA option byte to get the device info table address at the start of SRAM2a. The IPCCDBA value is 0x0, so the device info table address should be located at address 0x20030000. If I try to use the CLI to read at address 0x20030000, I get all zeroes in response.If I read the same address using the STM32 Programmer GUI, at first I get the same thing:However, if I switch to the CPU tab in the GUI and hit 'Run' first, I can check address 0x20030000 and I find a value of 20030890: Then, I can read address 0x20030890, and I find the device info table, including the 'table valid' bytes 0xA94656B9: Success! It seems that hitting the Run button makes all the difference for the GUI.So now going back to the CLI, it appear
Hello,We are working on integrating Wi-Fi module Murata Type1 MW LBEE5HY1MW(Cypress CYW43455) with STM32F4 based micro-controller using SDIO interface.We are looking for SDIO Driver and Murata Wi-Fi driver for STM32F4 based micro-controller.anyone here having any reference for the same? oranyone know where we can get them to integrate it in our system?Regards,Dipak Sharma
The ERRATA says essentially that port activity on PA2/PC13 will disturb LSE (WCLSP100)Does that mean that I can use PA2 still as LSCO ?Does that also mean that I still can use PC13 as RTC_TS / RTC_TAMP, or as WKUP2 ?Which ones will be a problem, or is it in general hands off those 2 GPIOs ? Thanx a lot for the help there.
Hi, Can anyone please explain the difference between Radio.StartCad and Radio.SetRxDutyCycle in LoRa?I am clear with the SetRxDutyCycle function but not sure what is the difference between CAD and duty cycle?
Hi, I am developing a sigfox app using stm32WLE5JC. I am reading it using cube programmer and on sigfox tab the chip certificate reads all FFFFFFFFFF . I also tried to read the sigfox PAC and ID on the 0x0803 E500 but its al FFFF. I want to ask how can I retrieve the chip certificate?
Hello,today I just ran the heart rate demo and suddenly the board seems to be bricked. The onboard debugger is running, but the CubeIDE is unable to start a GDB server. Using the ST-LINK utility I wasn't able to establish any connection to chip. So is it bricked?
WATCH ON-DEMAND | STM32 Summit 2026
Already have an account? Login
Enter your E-mail address. We'll send you an e-mail with instructions to reset your password.