Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Most recent activity
The BLE nodes are the NUCLEOWB55RG and dongle from the P-NUCLEOWB55 board.
STM32WB firmware updates v1.10.0 introduces large no of data packet loss in high-speed data transmission.
I'm using STM32CubeMoinitor-RF to establish a link between 2 devices but the PER is always 100%. I used ACI utilities and have both devices into Advertising mode, it does work on both devices with a pretty decent signal level of ~ -40 dbm. (I'm using an app on mobile phone to check RSSI). so I have no problem with the transmitter but the receiver seems no working. is this a known problem to ST? Is there any errata on the receiver? here is my RF path, "RF" signal comes direct from STM32WB55RGThis is my OSC connection:I very much appreciate any help on this.
Hi,I am advertising I-Beacons using STM32WB. I need blink a led during the whole time of advertising. I have initialized below functions,I-Beacon Process()I-Beacon Initialization()but I am unable blink the led at this moment. (I was able to advertise the beacon).Can anyone solve the problem and give me the exact point where I have to include the codes for blink led?
Hello, I used STM32WB55 HEARTRATE engineering test, and now the power consumption is at least 2.3mA. Is this normal?Is it possible to further reduce the power consumption by modifying the connection parameters? I tried to configure it with the aci_l2cap_connection_parameter_update_req function, but the tests found no change in power consumption.I didn't use it, did I?Besides modifying the connection parameters, is there any other way to reduce the power consumption? Thank you!
Hello, after playing a bit with P-NUCLEO-WB55 pack I bricked the board.The board is visible by Cube Programmer in DFU mode. Programmer can see the ST-Link but ST-Link does not detect the target. Are there any suggestions to recover ST-Link connection to STM32WB ?Is there a FW image containing FUS, BLE Stack and Application to bring the board to it's initial (factory) state? Thanks.
..
Hi,I am using STM32WB55CG nucleo board. I wrote a program as follows.Reset the devicerun BLE sequencer for 1 minute ( advertise BLE for i minute)read the time and datesave the time and date in flashenter shutdown modeWakeup from shutdown mode (using RTC wakeup) in every 10s and execute 3,4 and 5 stepsshutdown mode wake up does not works. But when I remove the second step in the program wakeup is working. After integrating the BLE in to the code wakeup does not works. My program as follows. Can anyone help me ? if( (__HAL_PWR_GET_FLAG(PWR_FLAG_C2SB) == RESET) ) { APPE_Init(); BLE_MODE =1; }while(BLE_MODE){ UTIL_SEQ_Run(~0); if(HAL_GetTick()>60000){ BLE_MODE=0; }}while(1){ HAL_RTC_GetTime(&hrtc, &time_struct_t, RTC_FORMAT_BIN); HAL_RTC_GetDate(&hrtc, &date_struct_t, RTC_FORMAT_BIN); temperature_value = Get_Temperature(); log_data(date_struct_t,time_struct_t,temp
Currently I plug it into my computer and the computer no longer recognizes it "device descriptor request failed (error43)" in both mode options 0 and 1. I want to set it to factory default so I can connect. be with the computer.Please help me!
In STM32CubeWB v1.10.0, the definitions of RCC_CR_HSEBYP (HSE bypass control) were removed from the CMSIS files for STM32WB5x MCUs. Also parts of the HAL that configure HSE bypass mode were removed. In the release notes it says "Remove RCC_CR_HSEBYP" but there is no further detail about this.I could not find any mention of HSEBYP in the latest errata for the STM32WB5x.What is the reason this definition was removed from the CMSIS and HAL, does this HSE bypass feature still work on STM32WB5x parts?
Hello I would like to use Mac802.15.4 with BLE included in the Wireless Stack. Is that possible? I was developing F/W using stm32wb5x_Mac_802_15_4_fw.bin for Wireless Stack, but now I need to support BLE as well. I wrote stm32wb5x_BLE_Stack_full.bin and stm32wb5x_BLE_Zigbee_FFD_dynamic.bin in the experiment, but MAC802.15.4 could not be initialized normally.
Question 1) ST has recently removed the deign of MB1389 (NUCLEO-WL55JC1) form the website. Were there any known issues (perhaps recently found) with the MB1389 design? Question 2) I have found the design of MB1720 in this forum but nowhere in ST website, is the design of MB1720 ready for production/proto?Question 3) Is there any other reference designs for WL55 somewhere?Many thanks,Mahdi
Hi there,I'm using the STM32WB55 to build a ultra low power sensor. The low power is working very well on the M4 with my firmware but the M0 with the Thread MTD stack is giving back unexpected results.Since the sensor can sleep for a while (also 10 minutes and also more) between samplings, I'm setting it as a SED by using the otLinkSetPollPeriod and the otThreadSetLinkMode to tell the radio to sleep and poll the parent every 5 minutes and it seemed to work.During the consumption tests we noticed that while the M4 was still asleep, the M0 started an high consumption (~10mA) after 3 exact minutes of inactivity (no tx from us and poll period at 5 minutes). The high consumption stops after other 2 minutes (so, after a total of 5, as the poll period set).I really don't know what's happening, am I missing something? Thank you in advance for your helpHave a nice dayPaul
Is it still Possible?
Hello All...I posted this in the MCU section and got no response so I figured I would ask here.I am new to ST Micro tools and have never used them. My background has been hardware and I have been 'hacking' at code on MSP430FR for a good 10 years. I am used to Code Composer Studio and writing register level C code. This is a complete IDE with compiler, debugger, etc all wrapped up in one, free from TI.I am interested in the new STM32WLE IC's for an upcoming prj. My question is if I download just the CubeIDE and the CubeProgrammer is this enough to write, compile, link and debug on the STM32WLE? Also for flashing / debugging hardware is the STLINK-V3SET the correct tool?thank you
I did not receive any mail asking for confirmation... anyway, Do you still have a seat for me ?Thanks a lot
I've just received an email to tell me you missed my confirmation to attend the online workshop for new STM32 LoRa SoC. I don't know how it was on my SPAM folder. I'm still interested to join the online workshop, is it possible?
Due to my holidays last week, I missed to confirm the E-mail. Would this be possible to join? Still seats available?
I am using STM32WB55RG with SDK version 1.10.0. I want to create BLE mesh, which will contain nodes with sensors. But firstly, I need to create mesh with 2 nodes: first has sensor client model, second has sensor server model. The server should have publish periodically.I am using BLE_MeshLightingProvisioner example. Device with sensor client is also embedded provisioner. I make these changes in the following files:For sensor client device:mesh_cfg_usr.h - #define ENABLE_SENSOR_MODEL_CLIENT (1), #define NUMBER_OF_SENSOR 1sensor_cfg_usr.h - #define TOTAL_SENSORS_COUNT 1appli_config_client.c - #define DEFAULT_PUBLISH_PERIOD ((0x01 << 6) | 0x01)For sensor server device:mesh_cfg_usr.h - #define NUMBER_OF_SENSOR 1, #define ENABLE_SENSOR_PUBLICATION, #define ENABLE_SENSOR_MODEL_SERVER (1)sensor_cfg_usr.h - #define TOTAL_SENSORS_COUNT 1So, publish period for sensor server model should be 1 second. After build and creating mesh via the terminal (atep root, atep prvn-0) it
Just got this:However, as we did not receive your confirmation within 3 days, we have allocated your seat to another participant.How was I supposed to confirm?
I'm trying to import an example project for STM32WB using STM32CubeIDE V1.5.1 and got the following error:I tried doing package updates, uninstall and reinstall and everything I could think of but I wasn't able to figure out how to resolve this (tried googling/forum searching it but no luck). Following I report you the Package installed: How can I resolve this issue?
Like several other people, I missed the confirmation email that was sent - unfortunately I was on vacation on Friday, and the window to reply to the email included the weekend. I would still very much like to attend the course. Is there any way that I can still confirm and get a seat?Thanks in advance,Chris
Dear all,same as others I missed the window of opportunity to reply over the weekend, but still would like to take part in the workshop. If there's anything you can do, thanks!Best,T.Pirk
WATCH ON-DEMAND | STM32 Summit 2026
Already have an account? Login
Enter your E-mail address. We'll send you an e-mail with instructions to reset your password.