Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Most recent activity
Hello,I'm struggling with BLE scanning on an STM32WB55 based application as GAP_CENTRAL_ROLE.We need to scan for beacons, and can't see any with ADV_NONCONN_IND, if device Advertises as connectable everything works perfectly.Any suggestions welcomed.Massimo
since the board has Lora embed with the kit. i want was set up the rf connectivity to transfer data between two such device.Any one please guide me with setup and code
I want to enable Terminal I/O using SWO for printf() function. I can't figure out why Iit doesn't work on that examples. It work on other examples (FreeRTOS and HAL Template).I follow the instructions from the IAR EW app manual and it doesn't worked. I read that it might be from the clock configuration but I don't know how to set it. :sad_but_relieved_face:
The button "Join the workshop" in the email is just a download link for a calendar invite, not an invitation to a teams meeting or similar.
..
Hi STI'm right now preparing for the WS tomorrow and would like to setup my system so I'm ready. One issue I face is this part:This is under "Network connections configuration" Proxy entries for HTTPHTTPS and SOSKS.Thank you in advance :)BRLars Munch
I need to check if this technology and your system is useful for our new projects. I will follow the MOOC, but I need some hw systems to put my hands -on. What starter pack do I need and how can I get it?
Further investigating I see that the problem seems related to symbols exported for the se_interface, compiled into the 2_Images_SBSFU_CM0PLUS project and exported as .elf and .o file, thus included in the 2_Images_UserA__CM0PLUS project linking phase. Running STM32CubeIDE 1.6.0 on Windows 10 with WL firmware pack 1.0.0. I'm no more able to proceed... Is there something I'm missing?Thank you A quick update after further investigation:Looking for the 1st problem returned by the linker:c:\st\stm32cubeide_1.6.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.9-2020-q2-update.win32_1.5.0.202011040924\tools\arm-none-eabi\bin\ld.exe: ../../../2_Images_SBSFU/STM32CubeIDE/CM0PLUS/Debug\se_interface_app.o: in function `SE_KMS_CloseSession':(.SE_IF_Code+0xbd8): multiple definition of `SE_KMS_CloseSession'; ../../../2_Images_SBSFU/STM32CubeIDE/CM0PLUS/Debug\se_interface_app.o:(.SE_IF_Code+0xbd8): first defined hereSeems that the linker is finding twice the symb
Hi ,We have designed the custom PCB based on "MB1720", tried the LORAWAN_end_node example on our custom board. but there is no signal out from RF antenna. do we need to modify anything related to MB1720? We have the NUCLIO-WL55JC devboard, the same is working fine with default code(updated Region parameters to India).Can you please suggest me if i need to make any changes in code with respect to MB1720.just for your info: custom board with MB1720 is working fine with other examples, also Lorawan_end_node running fine without any error's, but i could not see any data on packet forwarder in gateway.Thanks in Advance.Regards,SaiRam.
Hi, is it possible to provide me with a tracking number to see when the p-nucleo-lrwan and wl55jc devkits will be delivered? I'm booked for the session on the 19th of March
Hello,I wonder if this exist or will exist in a near future. The wireless firmware for the STM32WB are clearly indicated they are not compatible with Border Router use case. I have seen similar solution at Nordic Semiconductor, but I wonder if ST will provide something for this.I wonder also if the "Thread_Cli_Cmd" demo application can be used for this purpose ?Reference : https://openthread.io/guides/border-routerIf you have information, I'm clearly interested.Joel
M2SA or M2SP device looks promising. What isn't clear to me is if this module needs to interact with a separate micro for my program? or is there room for my program in this module? I am trying to do an energy analysis.
I created custom pcbs with STM32WB35CC with 256KB flash. If I understand correctly, controller shipped with no ble stack installed. So, i need to program one, but all information i found is only about wb55 and Nucleo boards. I couldn't find addresses to write FUS and stack files.I tried to use cubeprogrammer and connect via SWD and USB to my controller. When I connect via SWD, it cannot read the FUS version. Is it pre-installed? I tried to write BLE_stack file to 0x0800b000 (analogy with wb55 manual), but i-m not shure this is correct.When I connect via USB, cubeprogrammer generates a lot of errors and freezes.
So I am trying to synchronize microphones with a clap board; that works nicely as-is but when I tried to change the N_MS_PER_INTERRUPT to 10 (on both BVOPUS_PER and BVOPUS_CEN), I get clicks in my audio signal.I've changedN_MS_PER_INTERRUPTAUDIO_OUT_MSand the N_MS_PER_INTERRUPT in cca02m2_conf.hBut still clicks... is there somewhere I'm missing? Can BLE handle a 10ms buffer?
Hello, I have also missed the confirmation e-mail for the STM32WL Hands-On Workshop. Is it still possible to be a part of the session?Thank you!Radek
Hi community,I like to make my life a bit more difficult than necessary.Using a Quectel modem, connected via USART to the STM32WB5MMG, I want to enable OTA upgradeability over LTE CAT-M1/GSM. The downloading part is already figured out from older projects using a STM32F429. But now I am struggling with the programming part. With the STM32F429 you could just download the firmware from the modem over USART and save it to the not used memory bank. With the STM32WB5 there is no second memory bank. How is that process supposed to go ?Thank you in advance !
I am doing my first steps on the NUCLEO-WL55JC1 and one of the first things I like to get working is of course some debug printfs. Though I could of course use the VCP via the integrated STLink I'd like to use ITM_SendChar() to output some informtion. Though I think I did everything the same as when I also configured the STM32H735-Discovery, where I got ITM working, nothing is output with the WL55 board. As far as I understood from the documentation SWO output via PB3 should be possible on this board as well? Using WL55 Firmware pack v1.0.0 with CubeIDE 1.6.0Below are the steps I did to configure my app:Create an empty STM32 project for the NUCLEO-WL55JC1Initialize all peripherals with their default configuration: NoIn CubeMX: Set Debug/Trace: JTAG and Trace: Trace asynchronous swIn CubeMX: Clock config: Set MSI RC to 48000 setzen, to get output clock of 48 MHzSave CubeMX config and auto-generate sourceAdd to <Projectname>_CM4/Core/Src/main.c in the central while(1)-Loop in main(
I have a custom board having STm32WBCE on it. I have tried to call a function in stead of using in while (1)(Which I used to call in it and was working fine), implemented using sequencer + timer server in a repeated fashion which I create and start in "APP_BLE_Init()" function. I have created a task for my function to run repeatedly. To debug, I am using USB TX to print anything on the terminal software. I am able to send data on BLE and also able to receive. But after it receives data, the device stops printing my messages.What could be the reason?Also, how can I know how much time my function takes to complete once? -->( To set the TIMEOUT value for timer server repeating task)Currently I have set a random timeout and it is working fine. But I don't know whether due to this, the code is running fine or not.Thank you.
I bought p-nucleo-lrwan2 package at two weeks ago.so I have searched p-nucleo-lrwan2 reference source.I get p-nucleo-lrwan1 endless board source, but I haven't find p-nucleo-lrwan2 gateway source.please I hope to get p-nucleo-lrwan2 gateway source.have a good day
Hello,I have ran two examples of Zigbee applications on Nucleo STM32WB.One with end device device type and the other one with router device type (both with FFD stack).I have registered the node on my existing Zigbee network.I can see that the device type of the node is changing but when I look at the code, I could not find any difference (in app_zigbee.c).Can you point at to me where the device type is set in the code?Thank you for your answer,Best regards,LéoPS: is there a complete documentation of the API/stack available where I can find that kind of information?
The example "DAC_SignalGenerator" is not working as expected for me using a NUCLEO-WL55JC1 board. Using CubeIDE 1.6 with FW Pack 1.0Using the on board button one should be able to switch between a triangle and a "escalator" waveform. While the triangle waveform works as expected the escalator waveform is not really recognizable and it just looks like a lot of noise.I tried replacing the generation of the escalator with the code for the generation of a sine wave which worked on a stand alone project on the same board. Again, this didn't looked correctly but more interestingly when I observed the output with an oscilloscope it looked as if in the escalator resp. sine mode both signals were output superimposed to each other. The triangle was still very visible even in the Non-Triangle mode.My first idea was, that potentially the generation of the triangle did not really stop and both waveforms are generated at the same time.Could you please verify the escalator signal is working as expect
WATCH ON-DEMAND | STM32 Summit 2026
Already have an account? Login
Enter your E-mail address. We'll send you an e-mail with instructions to reset your password.