Does sequencer and timer server togather effect USB operation? Also I am unable to set the timer server TIMEOUT value to repeat the task continuously.
I have a custom board having STm32WBCE on it. I have tried to call a function in stead of using in while (1)(Which I used to call in it and was working fine), implemented using sequencer + timer server in a repeated fashion which I create and start in "APP_BLE_Init()" function. I have created a task for my function to run repeatedly. To debug, I am using USB TX to print anything on the terminal software. I am able to send data on BLE and also able to receive. But after it receives data, the device stops printing my messages.
What could be the reason?
Also, how can I know how much time my function takes to complete once? -->( To set the TIMEOUT value for timer server repeating task)
Currently I have set a random timeout and it is working fine. But I don't know whether due to this, the code is running fine or not.
Thank you.