Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Most recent activity
Greetings friendsI'm trying to find the workflow to effectively set-up a STM32WB55 to work with a HSE and LSI (no LSE) and just can't seem to be able make this work while others claims it works fine. Everything works perfectly with HSE and LSE using the p2pserver example however as soon as I set the CubeIDE's clock settings to LSI the device refuse to connect.I've read in another thread that you are required to set HSE/1024. How do you achieve this? In CubeIDE or this is a hardcoded function somewhere? Thanks
Hi,I'm working with the new STM32WLE5 MCU. I switched to our custom board recently, and because of that I'm using a Segger debugger. Prior we used a Nucleo board with the STLink debugger and that worked fine. Now I adjusted my debug settings for the segger and the CubeIDE tells me that the target device STM32WLE5JC ist not supported. And when I go through the list of devices (which then poped up) there are in fact none of this type.I have installed IDE version 1.6.0. Then I downloaded the J-Link tools from segger V6.98c and when I'm starting the J-Link commander I can connect and download my program. In their device list the STM32WLE5 devices are there...So my question: Can you fix this? When can we expect, that the IDE supports this MCU? Otherwise we might switch the IDE, so that we are able to debug. But we would rather not...Thanks!Stefan
Hello,I'm working on a project in which I want to connect to a tag that sends a Bluetooth signal with a L072Z-LRWAN1 board having a STM32L072CZYx MCU and the SPBTLE-RF Bluetooth component. There is the X-CUBE-BLE1 software pack that could help me realize that but I don't quite understand which application should I use. I think the eddystone beacon is the most appropriate but there is no tutorial or explanation on how to use the functions related to that. All I want is to connect to my tag and I cannot find this particular function and I really don't understand the settings of the beacon. For example when they ask you to configure a MAC address, is it the MAC address of my module or of my tag?If anyone knows anything regarding the BLE topic please let me know.Thanks,Mohamed
The datasheet for STM32WB5MMG says there are 2× DMA controllers (seven channels each) supporting ADC, SPI, I2C, USART, QSPI, SAI, AES, timers. It also says to reference DS11929 (The datasheet for STM32WB55) on page 2. DS11929 shows there only certain pins dedicated to SPI. Hence, I'm confused.
Hello.I have a task to evaluate RF range and penetration of the STM32WB based module. We plan to migrate from Microchip module to STM32WB5MMG module. The +6dBm output power of the ST module is a bit concerning compared to +20dBm we had from Microchip.What is the best way to make an evaluation and field testing using P-NUCLEO-WB55pack ?I have installed all the STM32WB ecosystem and even managed to brick one of the Nucleo boards. But still have one board and two USB dongles operating.Thanks.
Hello!I'm new to the STM32 tools. I'm trying to use the X-CUBE-EEPROM_V3.0.0 package in the CubeIDE with a uC from the STM32WL series. It seems more difficult than expected.1) In the package, there are example projects for Keil uVision AND CubeIDE for all uC families, except for the STM32WLxx. For this family, only an example project for Keil uVision is provided. Why? Is there a way to use this example in the CubeIDE (kind of project migration)?2) In CubeMX tool, there isn't the option to enable the eeprom emulator library. So my question is: How can properly integrate this library into my project?3) I tried to create a new project with default settings for the NUCLEO-WL55JC1, then copy/paste all the necessary files in my project folder and replacing "user" files, like main, STM32wlxx_hal_msp, and stm32wl_it (.h and .c). Then, I linked new files in my project by using "New\Files...", Advanced, tick "Link to file in the file system" and select the needed files (one by one... yes that wa
..
I am using SAI protocol to get the audio output...For now I am directly using the bin file provided in the sample code...I just wanted to know if we have mp3 file or any other format other then bin file, how it can be dumped to board using STM32CubeProgrammer.
Dear Hosts! I seem to have a problem joining the meeting. The link I recieved is not working. Yesterday I had no problem with joining the help-me session. Could you please resend the link to me?
Morning, I cannot find the link to join. Please resend
Hi -- AN5434 refers to using the MB1623 MCU reference design board with several add-on antenna PCBs without specific PCB part numbers, but AN5434 links only to a PDF and it doesn't include either all the needed antenna trace / PCB CAD dimensions or a ZIP with the full drawings / CAD files for the MB1623 + antenna reference design PCBs.Please provide the MB1623 + antenna PCBs gerber CAM manufacturing files and / or the Altium / DXF CAD design data for the PCB and trace patterns in AN5434 / MB1623 related antenna PCB boards.Without the full dimension specifications (e.g. trace diameters, and also full trace shape / length / position data vs. the PCB edges) it is literally impossible to use *any* of the reference design antenna / board shapes in AN5434 for making subsequent simulation or PCB design because of the missing dimensional information.I realize *some* of the the dimensions of the antenna traces and PCB edges are given in AN5434 PDF, however if you look closely many necessar
Hello all,Thanks for your supportI'm using STM32WB55cc MCU and I want to read the LDR and PIR sensor value using ADC. In ADC1, channel 6 (CH6), channel 11(CH11) are using. how to configure and read the data From ADC1. NOTE: STM32WB55cc MCU has a single adc ADC1.Kindly do the needful.Regards,Srikanth
I am using B-L072Z-LRWAN1. I ran the ping pong application ready here. I wanted to set up timer interrupt myself but there is no .ioc file. I opened another project, set up a timer in cubemx, tried and run it, and added it to the ping pong project. but timer interrupt ping pong did not work in the project. I wonder if you have a solution.
We figure that the STM32WB55 support only sending audio data through opus codec and doesn't have an A2DP behavior like other traditional BL. Could integrate an audio profile to the STM32WB for MP3, AAC, WAV
Hi, I am using STM32WB55RG as the MCU and LSM6DSO32 as the ACCELEROMETER in my project. In order to get my project CE certified, I require the Certificate Of Conformity for the both components.Hope you guide me to the right path.Thank You and Warm Regards,Pavan Kumar PerapuEmbedded Firmware DeveloperNext Step Dynamics
Hello, I have already received package STM32 Nucleo Pack - LoRa HF band sensor and gateway - containing sensor board with USI chip.Today I attended pre-workshop with Bartosz Boryna and it looks like that the board with USI is useless now, I need some other board STM32WL...Could you please verify, if I received correct parcel for tomorrow workshop ?If not, please, could you send me correct HW parts and re-schedule my training to date, when I have correct HW ?The original package was CR743573138DE and arrived on 10th March.Thanks,Ondrej
Hi, Is there any way to read register data in STM32WL? Since it uses SX1262 chip, I want to read register data using the register address. Since STM32WL does not have SPI support, can anyone please suggest how to read register data using STM32WL? For example, how can I read Data Buffer values?
Hi,I need to advertise free data, as I understand it is located in manufacturer data section.When I advertise only the manufacturer data, with aci_gap_update_adv_data function, I can see with Application BLE Scanner, the data, as raw data.But when I advertise the Service UUID, the data is different.What I do wrong? What do I miss?Thanks,Lior
HiI couldn't find a specific definition of the total length that I can advertise.On one place I saw 37 bytes, on another place only 25 bytes.Can someone tell me, how many bytes can I advertise? Thanks,Lior
I tried flashing PWR_STANDBY_RTC and PWR_EnterStandbyMode examples both has sleep current of 590uA. How do i get the datasheet value of 600nA standby current or atleast something less than 10uA.
I have started to go through the course pre-requisites and am familiarising myself with the kit and feeling much more confident, particularly as I have the gateway setup on TTN an seeing the L073RZ dev board ping in. I am still going through the prerequisites for the course but have run into a few problems, I was wondering if you could help ahead of the course as it seems important that I get to complete all the sections ahead of the course please?Using the UM2587 getting started guide, I have a few queries on the below sections,1. OK2. OK 3. OK but could you confirm what I need to install please as the guide states to run “demonstration application�? PG 6 section 5.1 of UM2592. I cannot communicate with the STM32WL55 (I can’t send commands), although it does report back correctly after a reset on the serial port terminal.4. OK but (currently using putty with setting of, 115200 8N1) but this doe
My project requires a RS-232 cable with TX inverted to connect the PC with CubeProgrammer CLI to STM32WB55. In application, I am able to configure the UART with "UART_ADVFEATURE_TXINVERT_INIT", and the STM32WB55 transmission works fine through the RS-232 cable, but does not work on bootloader, since by default the TX pin is not inverted.Any idea on how to workaround this?A custom bootloader is an option to consider, but since I am using CubeProgrammer I would like to use the default bootloader from ST.
Hi,Im using STM32WB55 USB dongle board. I want to send data from the dongle board to PC using USB pheriperal. i used the command CDC_Transmit() to send data and I visualized the recieved data using realterm in PC . It was working. But I want to send data at the same time BLE sequencer is running. When I run the sequencer CDC_transmit() is not sending data to the PC.Can anyone help me?
WATCH ON-DEMAND | STM32 Summit 2026
Already have an account? Login
Enter your E-mail address. We'll send you an e-mail with instructions to reset your password.