Skip to main content
Associate II
March 26, 2021
Solved

WB55: Sleep current too high

  • March 26, 2021
  • 3 replies
  • 1030 views

I tried flashing PWR_STANDBY_RTC and PWR_EnterStandbyMode examples both has sleep current of 590uA. How do i get the datasheet value of 600nA standby current or atleast something less than 10uA.

This topic has been closed for replies.
Best answer by G5658

It seems once flashing is done, i need to remove the jumper in JP5 that connects VDD to T_VDD or else the level shifter will burn 600uA+ of current.

3 replies

G5658Author
Associate II
March 26, 2021

Shouldn't current be measured at JP3 and not JP2?

Peter BENSCH
ST Technical Moderator
March 26, 2021

Well, JP3 and JP2 are connected in series, so either one would make the measurement of the current consumption possible.

JP3 relates to the VDD of the WB55, while JP2 also includes VDDSMPS.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
G5658AuthorBest answer
Associate II
March 26, 2021

It seems once flashing is done, i need to remove the jumper in JP5 that connects VDD to T_VDD or else the level shifter will burn 600uA+ of current.