Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Most recent activity
I have followed instructions from many threads but none seems to work. I am not sure if I tweaked the Anti-Rollback before a FUS update. Please help.So is there a way to revive my board ??If I have bricked my board and cannot REVERT back I need to know what was wrong and shouldn't be done.
Development Environment: KEIL (Free License)보드 : DISCO-L072CZ-LRWAN1HelloTo build a monitoring system with the LoRa protocol now.It is being developed as a 'DISCO-L072CZ-LRWAN1' board.I turned off the 'ST-LINK' built into the board to check the minimum current in the 'STANDBY mode' (removed SB37).I have a 'ST-LINK V2'.Can I connect my current 'ST-LINK' to 'DISCO-L072CZ-LRWAN1' for flashing?I thought using the SWD interface in CN8 would be a flash.So we connected SWD PINs of 'ST-LINK' and 'DISCO-L072CZ-LRWAN1'. I tried to flash by connecting 'SWCLK' pin and 'SWDIO' pin on 'CN8' No.2 and No.4However, neither 'KEIL' nor 'ST-LINK utility' recognized the board.I would appreciate it if you could let me know if I'm taking the wrong approach.
Could you get the binary data of STM32 of LRWAN3 which is loaded in NUCLEO-LRWAN3 by default?thank you for your help..*Moderation Edit: please do not post your email in the public area of this website*
Can anyone tell me what Update_Type parameter does in this fucntion?tBleStatus aci_gatt_update_char_value_ext( uint16_t Conn_Handle_To_Notify, uint16_t Service_Handle, uint16_t Char_Handle, uint8_t Update_Type, // -------> What values can it get? What does it do? uint16_t Char_Length, uint16_t Value_Offset, uint8_t Value_Length, const uint8_t* Value ) Is there any description documentation regarding the hci BLE messaging to BLE side?Thansk?
HiUsing a P-NUCLEO-WB55 dev board.Looking for a dedicated ST Windows app to debug BLE .Something that maybe connects to the ST USB dongle, and can run simple commands as connect, pair etc.Is there such a tool available?similar to this, but for windows :https://www.st.com/en/embedded-software/stbletoolbox.htmlThanks.
Using STM32WB, testing pairing-bonding. Using several BLE dongles for desktop PC.Peripheral - ST. (APP HeartRateRTOS example )Client - Windows 10 , BLE debug dongles.After pairing and bonding I read the bonded devices using:aci_gap_get_bonded_devicesI print the result and see an enormous number of addresses (all are the same).When I only paired 3 or maybe 4 devices.Here is the print-Log:06/09 16:06:48.797 Num_of_Addresses:241 err:0 06/09 16:06:48.854 i:0, type:0, adr:d1:af:3e:8c:ce:70 06/09 16:06:48.857 i:1, type:0, adr:d1:af:3e:8c:ce:70 06/09 16:06:48.860 i:2, type:0, adr:d1:af:3e:8c:ce:70 06/09 16:06:48.864 i:3, type:0, adr:d1:af:3e:8c:ce:70 06/09 16:06:48.867 i:4, type:0, adr:d1:af:3e:8c:ce:70 06/09 16:06:48.870 i:5, type:0, adr:d1:af:3e:8c:ce:70 06/09 16:06:48.873 i:6, type:0, adr:d1:af:3e:8c:ce:70 06/09 16:06:48.876 i:7, type:0, adr:d1:af:3e:8c:ce:70 06/09 16:06:48.879 i:8, type:0, adr:d1:af:3e:8c:ce:70 06/09 16
NUCLEO-LRWAN2�?� sensor 보드�?� 기본 �?재�?� firmware�?� souce code가 있으면 보내 주시면 �?사하겠습니다. i want a firmaware of F746RZ.STM32CubeExpansion_LRWAN_V2.0.0는 가지고 있는�?� 혹시 �?�것�?� 맞으면 어떻게 compile 해야하는지 알여주세요My project is breaking up.
智能穿戴产�?带�?牙5.0的芯片有没有推�??的?�?牙芯片 [�?制链接]这个�?牙芯片我们希望集�?更多的功能,比如内存有1M以上;有ADC采样,有OP�?放,或者内置有AFE电路;有充电管�?�(如果没有�?�以增加充电芯片,本身充电芯片体积�?会很大);需�?5.0或以上版本;带电�?监测功能或者�?�以外挂电�?计芯片;有串�?�或者IIC接�?�;这样的过功能�?牙芯片有没有�?�适的或者接近的?类似一个SOC的功能
Is there a way to send a single advertisement packet at a specific moment in code, ( without the mix/max interval time).I want to disable advertisement.And control it myself.
Hi, For my application, I have BLE connection between STM32WB55 (role = peripheral ) and mobile connection.I want to use BLE in low power mode such a way that, 1) If device is not paired MCU(M4) should wakeup and pair if device is available then sleep again.2) If already paired then collected the data at some interval.What is the best example/ best way to implement this scenario?Any suggestions would be helpful as I am beginner.
Hi, I'm using a custom board with STM32WB55 and faced with an issue related to FUS up and running. Initially, I was able successfully to upgrade FUS up to 1.1.2.0 via swd interface. Then I have updated the user key via USART embedded bootloader. Started from this point everything works fine until I performed the power cycle. After that, FUS stops working. When I'm trying to read FUS info I get "0x20030030 : EFF742A0"Before getting FUS info I always send STM32_Programmer_CLI -c port=swd -fusgetstate command several times and it replies "FUS_STATE_IDLE" every time.Read back DIT table shows results as follow:0x20030024 : 88842F65 04FF4224 E344FADB EFF742A00x20030034 : 3D4C3EF7 13CFC074 68D055F6 6FFE65C30x20030044 : F674573E 5FB11850 C24ADA6B ACBB243B0x20030054 : 4206EEEDAlso, I'm not able to upgrade FUS version up to v1.2.0. As I understand from the doc CM0+ core responsible for FUS running. Is that possible that this core not running anymore or stuck somewhere? If not, how to make FUS wo
I am working on the Programmable Voltage Detector (PVD) and was wondering if I can decrease the voltage instead of the default 3 volts it is outputting right now. I would like to decrease in different intervals to test the PVD.
HELLOI have a custom board with STM32WLE5J8I MCU and i want to make a LORAWAN End Node applicationI don't find any tutorial or video explaining step by step how to do this Thank you
Hi,I'm trying to swap the TX/RX pins of UART but I can't make it happen without the project configuration file that is not present in the Zigbee_SE_Msg_Server_Router project.I tried to change the pins in the 'hw_conf.h' file but that doesn't seem to change anything. Am I missing something?Thanks in advance!
..
This is the data I grabbed with bushound. As shown in the picture, when I send data through HID once, the USB will send empty data packets indefinitely, and subsequent data packets will cause the transmission to be stuck and repeated. I tested the USB driver I designed and the HID sample program of FW_WB_V1.11.0, both of which are the same phenomenon. Through jtag debugging, it is found that after sending data, the register USB_EPnR will repeatedly change between 0x3673 and 0x7633. This is the proof that USB is sending data cyclically, but I can’t find a way to stop or solve it.And this kind of problem has never appeared in the USB debugging of STM32F4.
Using example HeartRateRTOS. I see that device name is passed to 2 places. One doesn't cause it to change, the other does. Passing new name caused no change, (old name appeared in scan) :aci_gap_update_adv_dataPassing new device name to below, caused it to change:aci_gap_set_discoverablea. Why the duplication?b. Shouldn't changing the advertisement data (1.) be enough to change it?c. Same question for MAC , only aci_hal_write_config_data changes it, while the MAC is still advertised using aci_gap_update_adv_data.
*Moderation Edit: please do not post your email in the public area of this website*
Hello all! I am a recent graduate in Computer Engineering and I am taking my very first stab at firmware development. However, the board my customer picked, is proving to be the most annoying from the STM32WB series (regarding support, examples, tutorials, videos, etc.). I was moving along nicely on this board, until I was told to pass data over BLE (I can on UART). I have been grinding away on this guy for a week solid and I am at the point I am open to any outside advice.(Note: The STM32WB5M specific BVLPeripheral works perfectly for me. I can send audio both ways, but I don't need to send audio and that project is full of stuff we don't need (mainly Opus). My Senior CpE suggested using the STM32WB55's BLE P2P Server example and modifying it for the STM32WB5M.)Main question: Why does it seem impossible to find the .svd file for the STM32WB5MM (or STM32WB5xx)? It's ridiculous this board is not listed on the main ARM CMSIS website: https://developer.arm.com/tools-and-software/embedded/
I am intending to flash MicroPython into this board, where I understand there is extensive support for this. I would like to investigate the possibility of using ST-Link Utility to save the initial firmware that came along with the board, so that I will be able to rollback in the event I realize that MicroPython will not be good for my use-case.
Hi! I'm working with the LORA E5 trying to make a small librarie to easily send/receive data through LORA protocol (Not lorawan). The given examples (Ping-Pong) use the task scheduler and the Subghy app, wich im not planning on using. My question is: What do I have to enable in cubemx to make it work in it's minimum form (using radio.c)?I've merged all the files that i think are important in one single file, now the problem is how to initialize all the hardware. Do you have any info about that or know where to find info about it?Thank you very much.Have a nice day.
Hi community,I designed my own PCB and implemented the STM32WB5MMG.The device is a rather simple "Smart Home Outlet" that you can turn on/off with a Smartphone via BLE (it is just a fun project to learn some BLE).I verified that everything is working by disabling BLE and just uploading some simple FreeRTOS based code using CubeIDE. Now i want to turn on BLE. I configured everyting in CubeIDE/CubeMX:RTC, HSEM, WPAN..., no FreeRTOSI followed some examples from CubeIDE and noticed already that I have to hand over to the start the scheduler with the following.while(1) { UTIL_SEQ_Run( UTIL_SEQ_DEFAULT ); }Then I ran into the problem that the code got stuck really shortly after being started. The device does not start CPU2 properly i think.After following some more code I found that by using: LL_HSEM_1StepLock( HSEM, 5 );the device does not get stuck.UTIL_SEQ_RegTask(...)I can add my own task and let the onboard LED blink.But I can not figure out how to start BLE. Does anyone have an idea w
WATCH ON-DEMAND | STM32 Summit 2026
Already have an account? Login
Enter your E-mail address. We'll send you an e-mail with instructions to reset your password.