Broken FUS version
Hi,
I'm using a custom board with STM32WB55 and faced with an issue related to FUS up and running. Initially, I was able successfully to upgrade FUS up to 1.1.2.0 via swd interface. Then I have updated the user key via USART embedded bootloader. Started from this point everything works fine until I performed the power cycle. After that, FUS stops working. When I'm trying to read FUS info I get "0x20030030 : EFF742A0"
Before getting FUS info I always send STM32_Programmer_CLI -c port=swd -fusgetstate command several times and it replies "FUS_STATE_IDLE" every time.
Read back DIT table shows results as follow:
0x20030024 : 88842F65 04FF4224 E344FADB EFF742A0
0x20030034 : 3D4C3EF7 13CFC074 68D055F6 6FFE65C3
0x20030044 : F674573E 5FB11850 C24ADA6B ACBB243B
0x20030054 : 4206EEED
Also, I'm not able to upgrade FUS version up to v1.2.0.
As I understand from the doc CM0+ core responsible for FUS running. Is that possible that this core not running anymore or stuck somewhere? If not, how to make FUS working?
Thanks.