Skip to main content
Associate III
Jun 5, 2025 1:24 PM UTC
Solved

Can't do OTA updates again after modifying a non-OTA project into an OTA project?

 After performing an OTA update, the Bluetooth icon appears as shown in Figure 1, but it does not display the "STM_OTA" name.The correct result should look like Figure 2.

I followed the modification steps from this video, including adding the OTA Reboot Characteristic as shown:
https://www.youtube.com/watch?v=mRzZOa3jmuM&list=PLnMKNibPkDnG9JRe2fbOOpVpWY7E4WbJ-&index=9https://www.youtube.com/watch?v=mRzZOa3jmuM&list=PLnMKNibPkDnG9JRe2fbOOpVpWY7E4WbJ-&index=9

The chip I’m using is STM32WB55CGU6, with FUS version v2.0, and ST BLE Toolbox version 1.4.4.
The project has been uploaded in the attachment.

This topic has been closed for replies.

7 replies

Associate III
Jun 5, 2025 1:29 PM UTC

The project has been uploaded in the attachment.

Andrew Neil
Super User
Jun 5, 2025 1:31 PM UTC
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Associate III
Jun 5, 2025 1:35 PM UTC

This is not the same issue. This is a new problem. Currently, OTA updates can be successful, but it can only be updated once and cannot be updated again.

Andrew Neil
Super User
Jun 5, 2025 1:39 PM UTC

So is the previous one now resolved?

If so, please mark the solution in that thread.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
ShenChuanAnAuthorBest answer
Associate III
Jun 6, 2025 12:25 PM UTC
FilipKremen
ST Employee
Jun 6, 2025 1:20 PM UTC

Hello,

please read this document carefully.

Over-the-air application and wireless firmware update for STM32WB series microcontrollers - Application note

Also, I recommend having a look at BLE_HeartRate_ota example which can be helpful as a reference project.

 

Best regards,

Filip Kremen