BLE RF Testing Between Two Fasal Devices
- 4 replies
- 904 views
Hello ST Team,
I’m Shashank Hoysala from Wolkus Technologies.
We have two device variants, Fasal 5.0 and Fasal 6.0, which differ in hardware but both use the same STM IC (STM32WB5MMGH6TR). We attempted BLE RF testing following the procedure recommended by the ST team, including updating the Stack, FUS, and binary code.
Test Case 1:
BLE RF testing between a Fasal device (5.0 or 6.0) and the STM32WB5MMG Discovery Kit worked as expected. Communication was successfully established, and all required tests were completed without any issues.
Result: Pass
Test Case 2:
When performing the same testing between two identical Fasal devices (5.0 & 5.0 or 6.0 & 6.0) or between different Fasal devices (5.0 & 6.0), communication could not be established, and all tests failed.
Result: Fail
For your reference, I have attached a test setup photo and a video demonstrating Test Case 1.
My key question is: How can we perform BLE RF testing between two Fasal devices without using the Discovery Kit?
Thanks and regards,
Shashank Hoysala
Wolkus Technologies