Skip to main content
This topic has been closed for replies.

2 replies

Billy OWEN
ST Employee
Aug 15, 2025 4:15 PM UTC

Hi @grisom13 

 

This post has been escalated to the ST Online Support Team for additional assistance.  We'll contact you directly.

 

Regards,

Billy

ST Technical Moderator
Aug 18, 2025 11:13 AM UTC

Hello,

I guess that depends on what you are trying to achieve. If you just want to flash a UI to a device, you can do that directly using the "Run Target" button in TouchGFX Designer.

If you want to edit code, or are unable to connect your device to Windows, you should be able to generate code in Windows and open the CubeIDE project included in the project using CubeIDE in Mac OS.

The project file is updated with additional target files etc when generating code in Designer, so I would advise that you use the existing file instead of importing code to a new project.