Skip to main content
Mrohi
Associate III
July 16, 2019
Solved

I am using cube ide on my Mac OS . how I can use touchgfx with cube ide on Mac OS

..

Martin KJELDSEN
Martin KJELDSENBest answer
Principal III
August 8, 2019

Hi @Mrohi​,

Currently we do not support TouchGFX on MacOS. The Designer is supported on Windows alone and the tools that generate code for fonts and images are supported on windows and Linux. Even if the tools are relatively easy to port, the designer is not. Your only option is to use Cube IDE to generate your project on MacOS and then hand it over to a Windows VM, currently.

/Martin

25 replies

Martin KJELDSEN
Martin KJELDSENBest answer
Principal III
August 8, 2019

Hi @Mrohi​,

Currently we do not support TouchGFX on MacOS. The Designer is supported on Windows alone and the tools that generate code for fonts and images are supported on windows and Linux. Even if the tools are relatively easy to port, the designer is not. Your only option is to use Cube IDE to generate your project on MacOS and then hand it over to a Windows VM, currently.

/Martin

Mrohi
MrohiAuthor
Associate III
August 8, 2019
Ok thanks Martin for your email.
Thanking you
Mukesh
SPang.1
Associate II
October 15, 2020

Any update on TouchGFX Designer on MacOS ?

I'm using CubeIDE on MacOS and its a real pain to switch to a Windows machine for Designer.

Romain DIELEMAN
ST Employee
October 16, 2020

TouchGFX Designer is not supported on MacOS. It is not on our roadmap unfortunately.

KMill
Senior
April 5, 2023

Oh please! Go on! You know you want to ;)

Mrohi
MrohiAuthor
Associate III
October 15, 2020

any one can help for Install cube programer on Mac . I tried but can't see dmg file in download. thanking you.

mmcme.1
Visitor II
November 4, 2020

Very bad!

Can't run on Mac in the near future?

We'll have to look for another manufacturer ...

Martin KJELDSEN
Principal III
November 5, 2020

​Not in the "near near" future anyway :) Runs fine in a VM on Mac, though.

Good luck!

Associate II
August 26, 2025

But windows is a pain by itself !

SMour.1
Associate III
August 2, 2021

In my use case we bought a windows pc for one programmer to use touchgfx and the other programmers have to just build the project ,we can simply unignore the generated files and put them on the repository but that soemtimes is painfully slow , can someone on mac or linux build a cubemx+touchgfx project without windows ? (No need for the whole designer, just a cross platform code generation step)

KMill
Senior
November 9, 2022

Any news on Supporting macOS?

It's a show stopper for my company - which is a real shame.

I'd offer to port the deigner to macOS for you, if it helps?

Kyrpav
Associate III
April 5, 2023

Any new reply on this Support of macOS

Romain DIELEMAN
ST Employee
April 6, 2023

Hi,

This is still not in the near future plans unfortunately.

 /Romain

Kyrpav
Associate III
April 6, 2023

It seems that if you did not include it after 3 years it will never be, since also it is going to be much harder to restart everything from scratch. Am i correct if i assume that at the same time for marketing reasons there is not going to be any announcement that macOs is not going to be supported at all ?

Explorer II
July 26, 2023

Would be very helpful to have a Java version of touchGFX designer to be able to run on OSx. I think I will wait forever for this

CTapp.1
Senior III
February 1, 2024

Another Mac user here who really wants to use TouchGFX.

Is it possible to use TouchGFX on the Mac without using the designer?

 

All posts are made in a personal capacity. MISRA C++ Chair, MISRA C WG Member, Director The MISRA Consortium Limited (TMCL)
Visitor II
March 12, 2024

I started a project in TouchGFX Designer (Windows) and used dropbox as project folder. I was hoping I would then be able to open the .project file in CubeIDE MacOs, but I can't even see the file... (Yes I am showing hidden files in MacOs) 

What am I doing wrong?