Skip to main content
urbito
Senior II
Jul 18, 2023 4:49 AM UTC
Solved

TouchGFX + OpenAMP coexist issue

Hello community,

I am working on a project that involves the use of both CM7+CM4 cores from an stm32h7, to communicate both i need to use openamp. 

I have successfully made an standalone project that only have the openamp working, but when i port it to my actual project, it does not work/coexist with the touchgfxapp, i have found there an strange behaivour when i do initialize the MX_TouchGFX_Init before the MX_OPENAMP_Init, if i do the initialization that way, it would be "stuck" forever in the function: OPENAMP_Wait_EndPointready(&rp_endpoint);

If i do initialize first the OpenAMP it works fine, until i need to communicate, being able only to send one message and receive one answer and stuck forever in the "OPENAMP_check_for_message();" function.

I am going to put this functions (the initialization and also the message check) in freertos task because i have the suspect that this is due to "task/functions" priorities, and until now i have been working them outside the freertos and looking to call a custom function when needed.

Have someone been dealing with this kind of behaivour before?

I am using stm32cube ide 1.12.0 and touchgfx designer 4.21.3 under windows.

Hope to hear from you soon community :)

This topic has been closed for replies.
urbito
urbitoBest answer
Senior II
Sep 19, 2023 7:30 AM UTC

I found that i was working "wrong".

As mentioned, it was issues regarding the other tasks i was using. 

 

To solve the issue, i have had to place the OpenAMP init inside FreeRTOS. Then it worked fine. 

4 replies

Osman SOYKURT
ST Technical Moderator
Aug 23, 2023 10:26 AM UTC

Hello @urbito ,

I can't help you much on this I'm afraid, I don't know about OpenAMP, none of our TBS is using it. You'll maybe have more chances asking in this area of the forum but I can't guarantee it.

ST Software Developer | TouchGFX
urbito
urbitoAuthorBest answer
Senior II
Sep 19, 2023 7:30 AM UTC

I found that i was working "wrong".

As mentioned, it was issues regarding the other tasks i was using. 

 

To solve the issue, i have had to place the OpenAMP init inside FreeRTOS. Then it worked fine. 

Richard Lowe
Senior II
Sep 25, 2023 4:57 AM UTC

What does it mean "place the OpenAMP init inside FreeRTOS"? 

You put the OpenAMP init inside another task?
You put the OpenAMP init before the start of the scheduler?

I'm having the same issue, "stuck" forever in the function: OPENAMP_Wait_EndPointready(&rp_endpoint);

urbito
urbitoAuthor
Senior II
Sep 28, 2023 12:13 PM UTC

Actually i have place the OpenAMP Init in the TouchGFX Task, before the TouchGFX Init, but you can just place it in another task (i have had like that before), but since i do some communication once the TouchGFX app start, i need the connection before the touchgfx app. 

Give a shoot to both cases and see what works better to you.

 

greetings