Skip to main content
Associate III
Jan 24, 2025 11:14 AM UTC
Question

TouchGFX KeyBoard samples.

Hello All Members,

I am building one project using STM32 controller and using TouchGFX for creation of GUI for touchpanel.

I am trying to look for the QWERTY keyboard, where I can be able to have LOGIN Screen and can provide option for User to select Characters, Numbers and Special Characters to set their username and Password.

It would be great if someone could provide me a direction, where I can get the Qwerty Keybord for my TouchGFX project.

Also please let me know how I can customize the keyboard if required ?

 

BR,

Shiv

This topic has been closed for replies.

10 replies

urbito
Senior II
Jan 24, 2025 11:27 AM UTC

You should have a look on this post:

 

Share your Custom Widgets! - STMicroelectronics Community

 

there are couple of widgets and keyboards that may help you, also some examples on the TouchGFX app itself.

 

hope it helps.

 

Greetings

Osman SOYKURT
ST Technical Moderator
Jan 30, 2025 12:16 PM UTC

Hello @ShivDesh ,

I also recommend checking the Share your Custom Widgets! - STMicroelectronics Community thread as suggested by @urbito .

 

Have you been able to find what you need?

ST Software Developer | TouchGFX
Osman SOYKURT
ST Technical Moderator
Feb 14, 2025 9:00 AM UTC

Hello @ShivDesh ,

Did you find a solution to your issue?

ST Software Developer | TouchGFX
ShivDeshAuthor
Associate III
Feb 17, 2025 5:23 AM UTC

Hello @Osman SOYKURT ,

 

Not yet able to customize the Keyboard as needed but got one keyboard which I am using temporally for now.

It would be helpful to all Users if there is default inbuild Keyboard provided in touchgfx.

BR,

Shivprasad

Osman SOYKURT
ST Technical Moderator
Feb 17, 2025 9:58 AM UTC

Hello @ShivDesh ,

The easiest way would be to reuse and customize the custom container shared in here. I understand your need of having a native keyboard widget, this will be communicated to my team.

ST Software Developer | TouchGFX
Osman SOYKURT
ST Technical Moderator
Feb 17, 2025 12:08 PM UTC

You're welcome @ShivDesh ,

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question. Thanks :)

ST Software Developer | TouchGFX
ShivDeshAuthor
Associate III
Feb 24, 2025 5:42 AM UTC

Yes Osman,

Actually, I am still looking for a good solution.

If there is any document to do it or some direction you could provide that would be great.

What I need to follow to have a keyboard which can be customized. I mean having Enter space, char, num, special char, etc in it and changes to be done for it ?

If you could provide a source code and let me know the changes and steps to do it, that would be very helpful.

Thanks :) 

 

Osman SOYKURT
ST Technical Moderator
Feb 25, 2025 10:34 AM UTC

Hello @ShivDesh ,

I do not have other ideas than the ones that have been suggested already. 
If you need help to customize the Keyboard custom container, I recommend reaching out to our the ST Online Support Center. They can provide you with the necessary guidance, documentation, and source code to help you achieve your customization goals.

ST Software Developer | TouchGFX
ShivDeshAuthor
Associate III
Feb 26, 2025 6:45 AM UTC

Hello @Osman SOYKURT ,

 

Thanks for providing the direction, Yes for sure will contact the Support team, have raised a case and hopefully will get the required details from them.

 

BR,

Shiv