Skip to main content
SV_it
Associate
July 24, 2021
Solved

TouchGFX 4.17.0 ,"you are not connected to internet" error is showing

  • July 24, 2021
  • 60 replies
  • 12565 views

Hi,

when TouchGFX 4.17.0 is opened I'm getting an error stating no internet connectivity even though my laptop is connected to internet . also in the selection of boards I'm not getting any board option .

thanks and regards

sinduja

This topic has been closed for replies.
Best answer by YGroh.1

Solved.

Guess the server was just down...

60 replies

bvege.1
Associate
July 25, 2021

I have the same issue after updating from previous version v4.16.

Thanks,

VBK

DSafa.1
Visitor II
July 25, 2021

i also have same problem..

my connection internet no have problem.. no use proxy.. and i think good connection..

already instal and uninstal.. even redownload the software on website.. but still same..

try instal version 4.17.0 and 4.16.1 same problem..0693W00000D0Xi3QAF.jpganyone can help.. pls.

Thanks

Deni

QLiu.4
Visitor II
July 25, 2021

me too...0693W00000D0XqCQAV.png

GMont.3
Visitor II
July 25, 2021

I have the same issue, version 4.17 " You are not connected to internet and no demo or examples are available.

Anyway, the application is great! Thanks.

VAgga
Associate III
July 25, 2021

Hi,

I am also facing the same issue with all versions of TouchGFX.  " You are not connected to internet and no demo or examples are available

IGomesMSc
Associate II
July 25, 2021

Hi,

I also have same problem...

YGroh.1
Visitor II
July 25, 2021

Hi,

I am having the same problems. No Internet connection, no demos, no examples, no boards to select...

Due to other problems I also just set up a completely new Windows system and newly installed all the latest STM Software with default settings. Still doesnt work...

YGroh.1
YGroh.1Best answer
Visitor II
July 26, 2021

Solved.

Guess the server was just down...

MG32
Visitor II
September 13, 2021

Hi,

I have the same problem with 4.17.0:

"No Internet connection"

Is the server down again?

Or could it be a problem with internet settings?

How can a proxy be configured in TouchGFX designer?

Thanks.

Romain DIELEMAN
ST Employee
September 13, 2021

Hi,

The server is not down at the moment. Could you try to open an internet browser and re open TouchGFX Designer again ?

/Romain

MG32
Visitor II
September 14, 2021

Hi,

  • internet browser open at start of TouchGfx Designer: error 409
  • internet browser closed at start of TouchGfx Designer: error 407

Please see messages from log file below.

Thanks.

-----------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------

Messages from log file (with internet browser open) => error 409:

2021-09-14 07:44:39,835 [1] INFO TouchGFXDesigner.App: Logging configured

2021-09-14 07:44:40,777 [1] ERROR Utils.WebHandling.WebHandler: The remote server returned an error: (409) Conflict.

System.Net.WebException: The remote server returned an error: (409) Conflict.

  at System.Net.HttpWebRequest.GetResponse()

  at System.Net.WebClient.GetWebResponse(WebRequest request)

  at System.Net.WebClient.OpenRead(Uri address)

  at Utils.WebHandling.WebHandler.RequestWithStringResponse(Uri uri)

2021-09-14 07:44:41,496 [1] INFO TouchGFXDesigner.Main.MainWindow: Application started

2021-09-14 07:44:41,497 [1] INFO TouchGFXDesigner.Main.MainWindow: Username: ***

2021-09-14 07:44:41,497 [1] INFO TouchGFXDesigner.Main.MainWindow: Designer version: 4.17.0

2021-09-14 07:44:41,497 [1] INFO TouchGFXDesigner.Main.MainWindow: Designer installation path: C:\TouchGFX\4.17.0\designer

2021-09-14 07:44:41,497 [1] INFO TouchGFXDesigner.Main.MainWindow: Windows version: Microsoft Windows NT 10.0.19042.0

2021-09-14 07:44:41,497 [1] INFO TouchGFXDesigner.Main.MainWindow: Current culture: de-DE

2021-09-14 07:44:41,502 [1] INFO TouchGFXDesigner.Main.MainWindow: Current culture time seperator: :

2021-09-14 07:44:41,502 [1] INFO TouchGFXDesigner.Main.MainWindow: Current culture date seperator: .

2021-09-14 07:44:41,504 [1] INFO TouchGFXDesigner.Main.MainWindow: Installed .NET version(s): v2.0.50727 2.0.50727.4927 SP2v3.0 3.0.30729.4926 SP2v3.5 3.5.30729.4926 SP1v4 (Client 4.8.04084 Full 4.8.04084 ) v4.0 (Client 4.0.0.0 )  

2021-09-14 07:44:45,705 [17] ERROR Utils.WebHandling.WebHandler: The remote server returned an error: (409) Conflict.

System.Net.WebException: The remote server returned an error: (409) Conflict.

  at System.Net.HttpWebRequest.GetResponse()

  at Utils.WebHandling.ServerRequest.GetResponse()

  at Utils.WebHandling.WebHandler.RequestHeadStatusResponse(Uri uri)

-----------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------

Messages from log file (with internet browser closed) => error 407:

2021-09-14 07:39:52,556 [1] INFO TouchGFXDesigner.App: Logging configured

2021-09-14 07:39:53,473 [1] ERROR Utils.WebHandling.WebHandler: The remote server returned an error: (407) Proxy Authentication Required.

System.Net.WebException: The remote server returned an error: (407) Proxy Authentication Required.

  at System.Net.HttpWebRequest.GetResponse()

  at System.Net.WebClient.GetWebResponse(WebRequest request)

  at System.Net.WebClient.OpenRead(Uri address)

  at Utils.WebHandling.WebHandler.RequestWithStringResponse(Uri uri)

2021-09-14 07:39:54,183 [1] INFO TouchGFXDesigner.Main.MainWindow: Application started

2021-09-14 07:39:54,185 [1] INFO TouchGFXDesigner.Main.MainWindow: Username: ***

2021-09-14 07:39:54,185 [1] INFO TouchGFXDesigner.Main.MainWindow: Designer version: 4.17.0

2021-09-14 07:39:54,185 [1] INFO TouchGFXDesigner.Main.MainWindow: Designer installation path: C:\TouchGFX\4.17.0\designer

2021-09-14 07:39:54,185 [1] INFO TouchGFXDesigner.Main.MainWindow: Windows version: Microsoft Windows NT 10.0.19042.0

2021-09-14 07:39:54,185 [1] INFO TouchGFXDesigner.Main.MainWindow: Current culture: de-DE

2021-09-14 07:39:54,191 [1] INFO TouchGFXDesigner.Main.MainWindow: Current culture time seperator: :

2021-09-14 07:39:54,192 [1] INFO TouchGFXDesigner.Main.MainWindow: Current culture date seperator: .

2021-09-14 07:39:54,194 [1] INFO TouchGFXDesigner.Main.MainWindow: Installed .NET version(s): v2.0.50727 2.0.50727.4927 SP2v3.0 3.0.30729.4926 SP2v3.5 3.5.30729.4926 SP1v4 (Client 4.8.04084 Full 4.8.04084 ) v4.0 (Client 4.0.0.0 )  

MG32
Visitor II
October 6, 2021

Hi,

unfortunately, your file STM32G071-NUCLEO-DEMO-3.0.1.tpa is not recognized by TouchGFX 4.170.0 Designer.

Can you please upload a suitable version for 4.17.0?

Thanks.

Romain DIELEMAN
ST Employee
October 7, 2021

Hi,

The file does work on my side this is strange. Just to be sure are you looking in the right place ? The nucleo demo you asked is found under the Board Specific Demo tab in the Demos section.

/Romain

MG32
Visitor II
October 7, 2021

Hello,

I wanted to create a new application (starting from a blank screen) for X-NUCLEO-GFX01M1 (STM32G071-Nucleo):

Create New => Show All => STM32G071-Nucleo did not appear with your originally uploaded STM32G071-NUCLEO-DEMO-3.0.1.tpa.

Then I realized that tpa is just a zip.file and that it contains a json file. In this json file, I changed 

"Type": "TGAPP"

to

"Type": "TGAT"

and zipped it to a tpa file again.

After that the board appeared in "Create New" dialog.

So now it works for me.

Thanks.

Romain DIELEMAN
ST Employee
October 7, 2021

Board specific demos do not appear when you go in the "Create New" section, it will only show TBS. I guess you were looking for the STM32G0 Nucleo tbs instead then, good to hear you were able to adapt it and that it works :thumbs_up:

​

/Romain