Skip to main content
Associate II
Jul 22, 2025 6:03 AM UTC
Question

Timestamp on X axis label

Hi,

I'm currently working with the Dynamic Graph widget in TouchGFX, and I want to display X-axis labels in the format hh:mm:ss to show timestamps (e.g., 00:01:10, 00:01:20, etc.).

Right now, the X-axis labels are just integers, in the range which correspond to the maximum X-range I’ve set in the widget.

Is there any example or recommended method to customize the axis labels on the Dynamic Graph to show such formatted timestamps instead of plain integers?

Any suggestions or code references would be appreciated.

Thanks in advance!

This topic has been closed for replies.

1 reply

ST Employee
Jul 22, 2025 7:37 AM UTC
Louis BOUDOST Software Engineer | TouchGFX