Skip to main content
Caan
Associate III
Dec 24, 2020 11:02 AM UTC
Question

INtegration Error STM32cubeIDE 1.50 With TouchGFX 4.1.50

I am using STM32cubeIDE 1.50 With TouchGFX 4.1.50 for STM32F7508-DK Kit

But the is some problem with the integration of these Software and BSP, So I have to manually Add the paths and File in between ToucgGFX and STM32CubeIDE. After adding all the required work I am getting the following errors.

c:\st\stm32cubeide_1.5.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.7-2018-q2-update.win32_1.5.0.202011040924\tools\arm-none-eabi\bin\ld.exe: cannot find ../../ExtMem_Boot/Binary/Bootloader.bin

c:\st\stm32cubeide_1.5.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.7-2018-q2-update.win32_1.5.0.202011040924\tools\arm-none-eabi\bin\ld.exe: cannot find ../../ExtMem_Boot/Binary/Bootloader.bin

This topic has been closed for replies.

2 replies

MM..1
Super User
Dec 24, 2020 11:56 AM UTC
Visitor II
Jul 21, 2023 6:43 AM UTC

Hello Caan.

Check the path to the bootloader.bin file in the section entry of the STM32Hxxxxxxx_FLASH.ld file.

---------------------------------

 

TARGET(binary) /* specify the file format of binary file */

INPUT (../../ExtMem_Boot/bootloader.bin) /* bootloader bin file path (relative to the output folder)*/

OUTPUT_FORMAT(default) /* restore the out file format */

 

/* Sections */

SECTIONS

{

.bootloader :

{

. = ALIGN(4);

KEEP(../../ExtMem_Boot/bootloader.bin)

} > BOOTLOADER

---------------------------------

Check the ../../ExtMem_Boot/bootloader.bin path location and modify it accordingly.

Best Regards,

maple