Skip to main content
Associate III
Nov 4, 2025 6:02 AM UTC
Solved

how to setup LTDC

have a STM32F429I-DISCO board, start to a new touchgfx project from cubeide,run part file to completed touchgfx setup, cubeide compile project OK, debugging -> white screen! 

want to konw how to setup LTDC(double buffer -> by address, by allocate  single buffer ->by address, by allocate)

This topic has been closed for replies.
mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Nov 6, 2025 1:37 PM UTC

@redstone8415 

As stated by @mathiasmarkussen , why don't you start from TouchGFX designer based on TBS available and select STM32F429-DISC board as shown below?:

mALLEm_0-1762436234230.png

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

4 replies

ST Technical Moderator
Nov 5, 2025 9:17 PM UTC

Hello @redstone8415 

To resolve a white screen issue, check the LTDC Clock setup, and ensure the timing and polarity settings are correct.

Ensure also to use the correct physical connections and verify the jumper settings (JP3 and CN4 are set to "on") following the Getting started with the STM32F429 Discovery kit (page 9)

For LTDC configuration, refer to this application note: AN4861: LCD-TFT display controller (LTDC) on STM32 MCUs - Application Note

How to set up the LTDC peripheral to interface wit... - STMicroelectronics Community

 

 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Associate III
Nov 6, 2025 3:16 AM UTC

LTDC:

double buffer ->by address

0xC0000000

0xC0010000

compiled OK

still is white screen

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Nov 6, 2025 1:37 PM UTC

@redstone8415 

As stated by @mathiasmarkussen , why don't you start from TouchGFX designer based on TBS available and select STM32F429-DISC board as shown below?:

mALLEm_0-1762436234230.png

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
ST Technical Moderator
Nov 6, 2025 12:46 PM UTC

Try starting your project from the TouchGFX Designer instead. A complete Board Setup is supplied for STM32F429I-DISCO. You can than modify according to your needs from there - or you can analyze the project to figure out what you need to change in your own project if you prefer.