Skip to main content
Associate
Mar 21, 2025 3:00 AM UTC
Question

STM32F030F4P6 option byte programming

Can recognize the chip, but can not burn and read the flash problem. In this case, is the chip broken or the chip locked?

There is also a case that the chip can be identified as burning, but it cannot run the normal working program

This topic has been closed for replies.

2 replies

TDK
Mar 21, 2025 12:23 PM UTC

Is this a genuine programmer? The serial number "123456" is suspect.

TDK_0-1742559782658.png

Can you connect over SWD?

"If you feel a post has answered your question, please click ""Accept as Solution""."
Andrew Neil
Super User
Mar 21, 2025 12:43 PM UTC
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.