Skip to main content
STsch.1
Associate III
Dec 28, 2021 10:49 AM UTC
Question

SBSFU Flash overflow

Hi,

I have some trouble with using the SBSFU. In the first place, I could not build the SECoreBin project, but I found out, it was the path length in Windows making me the trouble. Now, after solving this and building a complete new project example, I see a very strange flash usage for this:

0693W00000HpwfTQAR.pngThe SE_Entry... has a huge flash overflow. Is this a problem? I see also the same thing, when I build other example projects.

Now, when I try to debug the whole thing on a board by activating the debug optimizer, I directly fall into a hardfault and I don't see, what the problem really is. So I expect somehow this to be the problem, but I cannot really be sure.

This topic has been closed for replies.

2 replies

Bubbles
ST Employee
Jan 4, 2022 10:16 AM UTC

Hi @STsch.1​ ,

look at the start address, you'll see it once again in the end of the table with 59% full only. There are sub-regions inside the SE_Binary region defined for keys and this tool just doesn't interpret it correctly.

Try building a project with protections disabled and debug enabled first. It's set for release and debug disabled by default.

BR,

J

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
STsch.1
STsch.1Author
Associate III
Jan 4, 2022 10:19 AM UTC

Hi Jhoud,

Thank you, I could solve this already, the SBSFU works now on a STM32F722. I had something wrong in the linkerscript.

The problem I still could not solve is here:

https://community.st.com/s/question/0D53W00001HaaHjSAJ/sbsfu-start-in-different-flash-memory-sector

I don't see, how I can start the SBSFU at a different address in the flash, since I need the smaller sectors for the application data.