Skip to main content
DonPavlov
Associate II
Sep 30, 2020 7:06 AM UTC
Question

Running the Homework for the L5 Board a second time. Now i get errors

Hi.,

Because i wanted to verify if the processes worked as well on my work provided Laptop. I ran the homework a second time.

The TFM Homework of course resulted in mutliple Errors and nothing worked. But now i can't even use the L5 Board anymore. I get no output on the Serial and the usb part shows a fail.txt with the following content:

The interface firmware FAILED to reset/halt the target MCU

Trying to connect the STCubeProgrammer also now fails with: DEV_TARGET_NOT_HALTED

So i can't manually wipe the device and restore it again.

Quick help would be appreciated.

    This topic has been closed for replies.

    15 replies

    PYada.1
    Associate III
    Aug 19, 2021 9:14 AM UTC

    Thank you so much @Frantz LEFRERE​ 

    I am able to connect it by putting the board in boot mode. My RSS version(read from 0x0BF97FFE) is 0. I have tried to disable the trust zone, but it is not disabling it.

    ALso I am following video but I am not able to disable trust zone

    Frantz LEFRERE
    ST Technical Moderator
    Aug 19, 2021 9:17 AM UTC

    If you're able to connect, you should be able to do a RDP regression. Do you confirm ?

    To disable TZEN, you need to have a secure code that launch a non secure code. Once that's on you target, you can change RDP to level 0.5.

    Then you should be able to connect (hotplug mode) .

    Then at the same time you should change TZEN and RDP level to 0.

    PYada.1
    Associate III
    Aug 19, 2021 9:52 AM UTC

    @Frantz LEFRERE​ ,

    I have uploaded nonsecure images using loader images(Generated from TFM test named "tfm_ns_enc_sign.bin"). After that, I Have tried to reduce the RDP level to 0.5, that my board is again not able to connect, Then after I have followed the same procedure, and was able to connect the board again. But I am not able to disable trust Zone. Can you help me with it?

    PYada.1
    Associate III
    Aug 20, 2021 12:43 PM UTC

    Now I am able to flash my normal application (without a bootloader).

    The steps are as following

    1) Connect the board to STM32 cube programmer

    2) Change RDP level to 0 i.e.0xaa

    3) Disable trust zone by unchecking TZEN in user configuration of option bytes

    4) Click on APply

    5) Remove write protection by changing write protection end location > start location

    After following above steps I am able load demo application.

    @Frantz LEFRERE​ , Thank you so much for your support.