Question
Running the Homework for the L5 Board a second time. Now i get errors
Hi.,
Because i wanted to verify if the processes worked as well on my work provided Laptop. I ran the homework a second time.
The TFM Homework of course resulted in mutliple Errors and nothing worked. But now i can't even use the L5 Board anymore. I get no output on the Serial and the usb part shows a fail.txt with the following content:
The interface firmware FAILED to reset/halt the target MCU
Trying to connect the STCubeProgrammer also now fails with: DEV_TARGET_NOT_HALTED
So i can't manually wipe the device and restore it again.
Quick help would be appreciated.