Skip to main content
Associate III
May 15, 2024 8:44 AM UTC
Question

Problems with RDP regression

Hi

When I was returning from RDP level 1 to 0 the stm32cube programmer program crashed and now every time I try to access the microcontroller several different cases happen:

1- Connect and instantly lose the connection giving the next error: Error: Data read failed
2-Cannot connect to access port 0! If you are trying to connect to a device with TrustZone enabled, try connecting with HotPlug mode. If you are trying to connect to a device that supports debug authentication with a certificate or password, open your device using it.
3- Detects the id 0x00 when it should be 0x482, Error: Unable to get core ID

 

This topic has been closed for replies.

2 replies

ST Technical Moderator
May 16, 2024 2:59 PM UTC
In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Jeff Tenney
Senior
May 25, 2024 8:25 PM UTC

Hi @Istillaga did you resolve this issue?  I'm having the same problem - but I was disabling TZ when stm32cube programmer had an error.