TODAY | STM32 Summit 2026
Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.
Most recent activity
Hi, I have the STM32F427VI, I don't know how this happend but now is read/write protected Level1. How can I reset this, I want to disable read protection at all to burn my application.Now I can't read the memory with STM Utility with J-TAG and coudn't erase memory with Demonstrator GUI via RS232. Please see the attached image.
Hi,Although not specified in the reference manual it looks like the CRC process within the FLASH module (see section 4.3.12) has to have start and end addresses aligned to possibly the CRC_BURST size (I've only tried 128 byte bursts so far). If not aligned the same data contents produces different CRC results depending on the values before and after the data.Some might say this is implied when described in the CRC paragraph but the HAL code does not check for it and the documentation for the address registers do not mention it (sections 4.9.20 and 4.9.21 plus those for bank 2).This is a fairly important thing to know if you intend to compare the CRC that the STM FLASH module calculates with one that was calculated somewhere else.Hope this info prevents someone else wasting an afternoon finding it out.Nigel
I receive the mail to download the X-CUBE-SBSFU but the link seems not workin
I haven't received the mail with X-SBSFU link
On the pagehttps://www.st.com/en/microcontrollers-microprocessors/stm32f7x5.htmllegend says that STM32F765 has HW crypto (dark blue color). However datasheet and reference manual do not confirm that. Reference manual RM0410 says that 77xxx models have crypto.My question is - does 765 model has crypto? If not, please correct the web pages.
I have sent a request to download the Library hand have gotten the validation and download link, however, the "Get Software" button is showing "Validating" button instead.
hello i try to test xcube-cryptolib rsa in blank project , my develop board stm32f429 disc1 and i added all lib files when i try to build get error justcollect2.exe: error: ld returned 1 exit statusmake: *** [makefile:44: test.elf] Error 1i cant understatnd the error so where should i look to find error p.s. sry for languagethanks
STM32Cube Programmer v2.4 (also tried v2.3)Windows 10 Pro (build 18363) and Mac (Catalina 10.15.4)STM32F405 custom board, STM32F407 on DISCOVERY boardI cannot unset the read protection of the MCU via the Cube programmer when interfacing to the factory boot loader over the serial port. It recognizes that the MCU is present and that it is under RDP. It then tries to unset RDP, but fails with a timeout.I can successfully unset RDP using the factory boot loader over the UART using the stm32flash program. The fact that the Cube programmer fails with both my own PCB and the standard DISCOVERY development PCB suggests to me it is not a hardware issue.The Cube programmer can set RDP over serial port, and it can set / clear it using ST-Link. I've tried it on Windows and Mac, same results.I've been working on and off on my firmware for 9 months, but since I normally use the ST-Link or a secondary UART bootloader, I am not sure whether this behavior is new, or has always existed but I didn't catc
Hello,This question is the follow-up of this one:https://community.st.com/s/global-search/Setting%20of%20GPIO%20PUPDR%20and%20OTYPER%20for%20SPI%20pinsI thought I had fixed it thanks to the GPIO setting but it was just bad luck.My setup is:two Nucleo STM32H743the master is using on SPI1the slave is using SPI2 (with SPI1 I have no issue)clock setup is: for master VOS1, Sysclk 400MHz, HCLK 200, PCLK 100, spi_ker_clk 200 and SPI baudrate prescaler at 8. For master every clock divided by 2 (parameter M to setup ref1_ck of PLL1 was changed)GPIO: high freq / push-pull / no pull down (tried with pull down, no difference)slave receives correctly all the timemaster never receives answer from the slaveSPI setup at master side to receive the answer from slave: simplex receive only, CRC enabled, datawidth 8 bits, 5 bytes to receiveI completely unplugged the MISO wire. On master side I of course still gets the EOT event (as expected) but I expect to get a CRC error since I should receive crappy dat
I'm trying port the SBSFU example STM32L476 board to our MCU which is STM32L475. Fortunately they are very similar. I'm going through the code and it makes sense but I could not find a single reference about porting it. ST has documents that explain what is going on but not how to port it. Which files should I be modified? I am going over all the source codes (.c, .h). Not sure what parts of the linker file (or any other files I'm not aware of) should be modified. A practical guide would have been useful. A little rant: I wish this feature was implemented in the CubeMX, that would have made life a lot easier for people who don't have a long background in fw development.
I've been just bitten by https://community.st.com/s/feed/0D50X00009XkW6NSAV . [reconstructed] In an already proven working piece of code, I first check if an array's first word is equal to a constant (signature), then I reset the CRC and then feed it in a for loop by that array (including its first word, i.e. the signature). A newer version of gcc optimized this more aggressively than previous gcc version, and as from the signature test it "knew" that the first word of array is equal to a constant (which it already held in a register), it generated a write from that register immediately after the write to CRC reset, and only after that fed the remainder of the array in the loop. I've checked RM0090 which is currently in version 18, and there's still no mention that I'd have to wait until the reset bit gets autocleared, or any specified time after writing the reset. ST, can this please be specified. Also, isn't the same problem present in other STM32 models? JW&
..
Hi,I am working on p-nucleo-wb55 and run SBSFU example successfully. now i want replace default user application with my application as a secure application (.sfb). I refer AN5056(Integration guide for the X-CUBE-SBSFU) section 8.1 How to make an application SBSFU compatible. but i am woking on AC6 IDE and example steps are for the IAR IDE.So can you please tell me what linker script (.ld) changes require to make application SBSFU compatible and as specially how to make bin file length multiple of 16 byte which required during aes encryption.Thanks,Arjun
Hi,I am testing SBSFU in p-nucleo-wb55. when i am flashing user_app.sfb it flash successfully at slot1 (Download Area) but can not decrypt and hang at below STATE can you please help me how to resolve this issue and also tell me how to enable debug log in 2_Images_SECoreBin.= [SBOOT] System Security Check successfully passed. Starting... = [FWIMG] Slot #0 @: 8012000 / Slot #1 @: 8047000 / Swap @: 807e000 ====================================================================== = (C) COPYRIGHT 2017 STMicroelectronics = = = = Secure Boot and Secure Firmware Update = ====================================================================== = [SBOOT] SECURE ENGINE INITIALIZATION SUCCESSFUL = [SBOOT] STATE: CHECK STATUS ON RESET INFO: A Reboot has been triggered by a Software reset! Consecutive Boot on error counter = 0 INFO: Last execution detected error was:No error. Success. = [SBOOT] STATE: CHECK NEW FIRMWARE TO DOWNLOAD = [SBOOT] STATE: CHECK USER FW STATUS N
Hi there. I have been using the wolfssl lib for a while on the freescale mcu mk82fn256xxx and the performance have been greate so far. Wc_generateSignature performs a signature within milliseconds. Recently I switched from freescale to STM, SMT32F437VG serie. This mcu has a RNG, CRYPTO and HASH engine. When it comes to the wc_GenerateSignature I can make the difference between two of them. STM MCU takes too long to perform the signature (about 4.5 seconds). Is there any way to improve the signature process? I am not sure but I think that the difference between two MCUs relies on the PKA(Public Key Accelerator). Any help is appreciated.Regards
I have used STM32H750VB as my main controller for a Project and in that i am in need of AES Encryption to be done..With the help from our community friends i am able to integrate the AES part in my main coding..I have used the 192 bit plain text array(Plaintext[16]) with the 192 bit key ( AESKey192[6]) and 128 bit initialization Vector( AESIV_CBC[4] ) and obtained the 192 bit output encrypted array (CiphertextAESCBC192[16]) given in the attached notepad. ..I am a novice so kindly explain or give me the links where i can study about the same. I am having the following doubts1.Is the size of the encrypted data same as that of input data?2.When i try to transfer the encrypted array through UART the 32 bit data cannot be transferred properly i am getting some special characters and i have tried splitting the data as 8 bit and now i am getting a result but i don't know whether it is correct or not? (the image is attached as UART Op)3.When i tried checking the obtained result the link f
I'm trying to use EEPROM emulation API in a project. I have downloaded the expansion package. Based on AN4894 I need core and porting to be included in my project so I copied them under a new directory in Middleware and included the path. Then added the eeprom_emul.h to my project. However stm32l4xx_ll_crc.h is included in the eeprom_emul.h which is not in my project. I activated the crc in cubemx and regenerated the code but this file is missing. Would appreciate any help.
Hi All,I am using X-CUBE-CRYPTOLIB for AES ECB encryption/decryption on STM32H7 micro and using the F7 example code and library(libSTM32CryptographicV3.0.0_CM7_GCC_ot.a), provided in the crypto package. But the comparison of encrypted message fails with expected cipher text. FYI i have enabled CRC clock. Please help me out to resolve it quickly. Herewith i have attached the code for your reference
I have created a simple function to encrypt a message using the AES CBC flow suggested in the documentation (AES_CBC_Encrypt_Init, AES_CBC_Encrypt_Append, AES_CBC_Encrypt_Finish), and then using the same flow to decrypt (AES_CBC_Decrypt_Init, AES_CBC_Decrypt_Append, AES_CBC_Decrypt_Finish). I am using a fixed Key vector (32 bytes) and a fixed InitializationVector (16 bytes) and I'm using these same arrays in decryption as in encryption. But I don't get the original input message back. Here is the code:uint32_t doSimpleEncrypt(){ // AES context, error status and output length. AESCBCctx_stt AESctx; uint32_t errorStatus = AES_SUCCESS; int32_t outputLength = 0; const uint8_t Plaintext[PLAINTEXT_LENGTH] = {0x61, 0x62, 0x63, 0x64, 0x65, 0x66, 0x67, 0x68, 0x69, 0x6a, 0x6b
I am using bootloader to update my firmware and I am using dual bank to update code. When I working on bank 1, new code sending to bank2 after reset I am starting bank2 successfly, but I want to use Read Out Projection in my MCU.If I use Read Out Protection I have some question about that:1) If the read out protection enable, can I use dual bank?2) If the read out protection enable, can I update firmware with IAP-Tftp ?
We have two microcontroller, one is the STM32H7 and another one without hardware CRC (need to be software CRC through an algorithm).I use SPI communication with this hardware CRC32 and I would like to know the software algorithm able to have the same value as for the hardware CRC calculation. I can see proposal of algorithm up to STM32F4, but for newer version of microcontroller such STM32H7, I just see anything.Of course, I tried the CRC algorithm of the previous version but doesn't work.
I'm trying to enable the OB_RDP_Level_1 for a STM32L151CC but It fails. The MCU becomes bricked. I can't even boot to DFU. I need to first start ST link utility and set read out protection level 0, and then do a chip erase. But I noticed that bit OPTVERR = 1 indicating that the option bytes are faulty. I have tried a fulle chip erase and it does not set the OPTVERR to zero. Is it possible that I have a special STM32 that always start up with OPTVERR = 1? I have tested on some evaluation boards and they have OPTVERR = 0 at start.
We have an STM32F37II device in an older generation of a product that ECCkeygen() works as expected. But in a new version of the product, which uses the same MCU and cyrpto libraries, and which uses nearly identical firmware (it was ported from the older device), the ECCkeygen() function works for the localPublicKey X keys, but not for the Y keys. the pmY->mNumDigits comes out of ECCkeygen as 1 instead of 12 and that causes the Y keys to be mostly 0's. I believe that the arguments going into the function are correct. Our flow follows the ECC Key Generation flow chart (RNG init, ECC curve init, publicKey point init, privateKey point init, ECCkeygen). None of these return failing statuses.Do you know why ECCkeygen would return the Y mNumDigits of 1 instead of 12?Thanks in advance for your help.
Hi everyone,I have a problem about the integration of the SEGGER embOS RTOS with SBSFU.I have already succeeded with FreeRTOS but I would like to use embOS for my project. The "SECoreBin" project compiles well, I added the instruction to deactivate the systick in the SBSFU project just after "SFU_LL_SB_SRAM_Erase ();".When I run my "user app" project my interrupt "systick_handle" does not work.Have you ever used embOS with SBSFU ? Do you have any advice ?I've been struggling with this problem for several days now :(Best regards, Hugo
Already have an account? Login
Enter your E-mail address. We'll send you an e-mail with instructions to reset your password.