TODAY | STM32 Summit 2026
Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.
Most recent activity
We are updating our buildtools to GNU Tools for STM32 11.3.rel1 for a new project that is using an existing SBSFU 2.4.0 based bootloader from a previous project that was using an older compiler. Trying to compile the bootloader gives following errors: data_init.c: In function 'LoopCopyDataInit': data_init.c:46:29: error: array subscript 'uint32_t {aka volatile long unsigned int}[0]' is partly outside array bounds of 'uint8_t[1]' {aka 'unsigned char[1]'} [-Werror=array-bounds] 46 | dst[i] = src[i]; | ~~~^~~ data_init.c:36:24: note: while referencing '_sidata' 36 | extern uint8_t _sidata asm("_sidata"); | ^~~~~~~ data_init.c:46:20: error: array subscript 'uint32_t {aka volatile long unsigned int}[0]' is partly outside array bounds of 'uint8_t[1]' {aka 'unsigned char[1]'} [-Werror=array-bounds] 46 | dst[i] = src[i]; | ~~~^~~ data_init.c:82:24: note: while referencing '_sdata' 82 | extern uint8_t _sdata asm("_sdata"); | ^~~~~~ data_init.c: In function
Currently developing a product to update the firmware of a product through SWD, i encounter an issue with the flash of the target (STM32G070RB).After multiple changes in the RPD (from 0->1 & 1->0) the flash of the MCU can't be erased. Some word will not erase to 0xFFFFFFFF, but instead will be at 0xFFFF0080. Once it's in that state, changing the RDP to trigger a mass erase will not fix the flash. The STLink is unable to mass erase or page erase the chip, and also unable to program anything to the chip.Initially i though that my programmer was the issue of the flash error of the target. But when it happens it was when changing the RDP from 1 to 0 with the STLink. I was not sure of that on the first occurrence of the issue. But today it happened again, while not using my own programmer at all.So i am now sure that it happen after changing the RDP from 1 to 0 using the STLinkV3.Does anyone already encounter this issue?
When I Update WRP option bytes in stm32u585 via program and call OB_launch is resetting device continuously.Here is the code snippet. any other configurations I am missing??
I'm migrating from an F4. So this is all new to me. Need help getting started. I currently have: A primary bootloader. It checks the application flash for a stored signature every boot An application flash. It's up to 896KB. 2MB Flash, two banks for flash. When I update I alternate the banks. This is mainly done manually and not using an bank selection. All sectors are 128KB which wastes a lot of flash because my bootloader is near 20KB. My firmware updates OTA/FOTA over Wifi. Because I don't have external flash, I need to download blocks to the alternate bank, collect all, and check them for completeness. The bootloader will check them next boot. I've been studying the iROT, uROT, RSS, SFU, Product State, Debug Authentication. SFU is not for me. I don't need strong security at a contract manufacturer. Not yet. We program in house I think there might be a way for me to get rid of the flash authenticity of the primary bootloader. I feel like this is part of what iROT or uROT does? I
Hello SBSFU users !The latest release of STM32CubeIDE 1.9.0 is introducing GNU Tools version 10.3 as toolchain. This new toolchain creates an issue in the SBSFU final build.A new release of X-CUBE-SBSFU is coming in around one month to fix this but, in the meanwhile, I would like to share with you the changes needed to be able to use this version of STM32CubeIDE.First, the issue is related the the ability to call services in the secure engine. So, if you do not need this feature, just remove it.Here is how to do this.1- Open Properties of your user application2- in C/C++ Build/Settings/MCU GCC Linker/Miscellaneous, remove the content of Additional objects. Something like "./../../2_Images_SBSFU/STM32CubeIDE/Debug/se_interface_app.o"3- Also remove in your code any call to SE_*. The common service implemented is usually SE_APP_GetActiveFwInfoThat's it.Now, if you use the SE service, here is what you need to do. The following is the description of the changes done in the SBSFU provided in
I have Downloaded STM32CubeExpansion_Crypto_V3.1.0 library. I am trying to use it for STM32L431RBTx Microcontroller. But I am getting error as shown in following images.What am I missing to do?Please help. Building target: _V0.1.elf" @"objects.list" -llibSTM32CryptographicV3.0.0_CM4_GCC_ot -lmc:/ac6/systemworkbench/plugins/fr.ac6.mcu.externaltools.arm-none.win32_1.13.2.201705091103/tools/compiler/bin/../lib/gcc/arm-none-eabi/5.4.1/../../../../arm-none-eabi/bin/ld.exe: cannot find -llibSTM32CryptographicV3.0.0_CM4_GCC_otcollect2.exe: error: ld returned 1 exit statusI have also tried by removing the prefix 'lib' from library .a file name. Then I am getting following error.Invoking: MCU GCC Linkerarm-none-eabi-gcc -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -L"D:\L4\STM32CubeExpansion_Crypto_V3.1.0\Fw_Crypto\STM32L4\Middlewares\ST\STM32_Cryptographic\Lib" -specs=nosys.specs -specs=nano.specs -T"../STM32L431RBTx_FLASH.ld" -Wl,-Map=output.map -Wl,--gc-sections -o "Hotel_
need to transfer some string to PC via USB config. Here am implementing simple code here. But no responses in hyper terminal. Kindly help me. Am using Nucleo-STM32H563ZI board.//=======================================while (1){/* USER CODE END WHILE *//* USER CODE BEGIN 3 */HAL_PCD_EP_Transmit(&hpcd_USB_DRD_FS, *data, data, 10);HAL_GPIO_TogglePin(LED_GPIO_Port, LED_Pin);HAL_Delay(1000);}/* USER CODE END 3 */
Hi @ChannelIm using the TF-M Application package for the STM32U585 development board from ST. My query is as per the memory map of the Internal Flash has a combined storage of 826kb for secure and non secure image.(Please refer to the figure below). But my project requirement needs more space and hence need to store the primary slot and bootloader associated partition in the internal flash and needs the secondary slot storage to be implemented in the external flash(for backup purpose). How can this requirement be achieved without altering the PSA Certified TF-M Bootloader Implementation.(Please suggest if there is an alternate approach).My application size (secure +non secure) would consume nearly the 826 kb or less. Please suggest any detailed approach on how this requirement can be achieved.2. One more query is like which all crypto schemes have been implemented with the help of the PSA API in the released ST Package. and is there any particular guidance on the usage for t
Hi All,I have a problem with tag generating for CRYP_AES_GCM_GMAC. The main crypting is fully working, but AuthTag is generated wrongly. It is strongly depend when the generating is started. When you change for (int i = 0; i < 10000; i++) {}; you will receive different values. I have no idea, what is wrong. (CRC clocks on)Supposed data: uint8_t tag[16] = { 19, 74, 107, 250, 55, 74, 33, 198, 182, 189, 43, 1, 146, 146, 24, 92 };Milanvoid TestCryptoAES(void){ CRYP_HandleTypeDef hcryp; uint8_t InitVector[AES_BLOCK_SIZE] = { 10, 0, 0, 0, 4, 3, 2, 1, 100, 231, 96, 38, 0, 0, 0, 2 }; uint8_t AES128key[AES_BLOCK_SIZE] = { 118, 101, 114, 121, 118, 101, 114, 121, 115, 101, 99, 114, 116, 107, 101, 121 }; // input "raw" data uint8_t plainText[AES_BLOCK_SIZE] = { 1, 2, 0, 12, 1, 2, 3, 4, 0, 0, 0, 10, 0, 0, 0, 0, }; // input crypted data uint8_t&
I would like to use the mbedTLS version 2.28.2.v2 on the secure boot for stm32h743ii controller. I have downloaded SBSFU v2.6.2 and Built the secure boot binary on top of the example project from H753 2_images_OSC folder. Secure boot is running the target hardware. But the .sfb file is not upgradable with the secure boot and it throws the FW authentication error.I suspect that the .sfb file created by windows executable exe is not using the integrated mbedTLS version 2.28.2.v2 somehow. Please suggest the next step.Regards,Rakkumuthu R
We have one STM32h563zi board on which first We blink the normal led program, After that We perform the Secure Boot by taking the reference from STmicro official website, Secureboot run successfully. We run the regression script .Now the board should come out from the Secure boot, but When we try to blink the led program, it's not blinking.When we are try to debug it it's showing hard fault.Why ?
Hello all.Another question regarding SBSFU, this time 1 image version.When we download new image via YMODEM, when does decryption process happen?1. Is new image first downloaded into active image slot and then decrypted?2. Is new image downloaded and decrypted at the same time, which is basically decryption on the fly, but that requires special hardware accelerator? Thanks in advance!
Ask this at arm.com, but maybe it is STM32U5 specific:I try run an unprivileged application in secure mode and get a strange behavior:STM32U5 has TZ enabled, all application runs in secure mode.1) LR = 0xffff_fff9, CONTROL = 1 => BX LR increments the SP, but all registers become 0 (including PC and XPSR!)2) When setting CONTROL = 1 and executing SVC, SP is decremented correctly, but nothing is stored on the stack?I check all errata I could find, but no hint.If TZ is disabled, the system behaves normal.42Bastian
Hi Community,I'm porting STM32G071 SBSFU to STM32G0B1RE and Customizing UART to USB CDC.I'm using Nucleo-G0B1RE dev kit and STMCubeIde for development.1. I'm able to build, load, run both STM32G071 SBSFU and UserApp without any changes. but when I change project global symbol STM32G071xx to STM32B1xx in properties->Settings->Preprocessor->Define Symbols. The have made appropriate changes after loading USERApp causes hard fault and resetting device.2. Also tried changing sbsfu and fwimg .ld files for rom and ram address with/without changing define symbols above mentioned also had similar issue.Now I am stuck without knowing what needs to change and how to port the code to STM32G0B1 ?Can you please help with require changes to port from STM32G071 to STM32G0B1 ? TIA,Tarun
Hi,I changed symbol in the properties tab to adapt STM32G0B1xx drivers causing hard fault after loading User App. The hard fault occurs in sbsfu while verifying the user fw signature.can someone help me why fw signature verification failed just changing symbol to STM32G0B1xx ?
I am using the SBSFU STM32CubeExpansion_SBSFU_V2.6.2 version for my custom board STM32H743VI controller. I have ported the STM32H7B3I-DK project for H743 controller for COM port and changed the crypto scheme to SECBOOT_ECCDSA_WITHOUT_ENCRYPT_SHA256. I am getting below logs and hangs. It hangs in the below code,SE_ErrorStatus SE_VerifyHeaderSignature(SE_StatusTypeDef *peSE_Status, SE_FwRawHeaderTypeDef *pxFwRawHeader){ SE_ErrorStatus e_ret_status; uint32_t primask_bit; /*!< interruption mask saved when disabling ITs then restore when re-enabling ITs */ /* Check if the call is coming from SFU code */ __IS_SFU_RESERVED();#ifdef SFU_ISOLATE_SE_WITH_MPU if (0x0U != SE_IsUnprivileged()) { TRACE("\r\n inside privilege"); uint32_t params[1] = {(uint32_t)pxFwRawHeader}; SE_SysCall(&e_ret_status, SE_CRYPTO_HL_AUTHENTICATE_METADATA, peSE_Status, &params); TRACE("\r\n after secall"); }After SE_SysCall() call,
Dear Sir.I am trying to work with the examples of TFM_Appication and SBSFU_Boot examples of STMCube_FW_U5_V1.2.0 when compilng I get the error Error: Missing option '-S' / '--slot-size'.postbuild.sh failedmake[1]: *** [makefile:92: post-build] Error 1make: *** [makefile:60: all] Error 2"make -j16 all" terminated with exit code 2. Build might be incomplete.Error: Missing option '-S' / '--slot-size'.postbuild.sh failedmake[1]: *** [makefile:92: post-build] Error 1make: *** [makefile:60: all] Error 2"make -j16 all" terminated with exit code 2. Build might be incomplete.Please Advise,
Hi Guys,Ported SBSFU 2.6.2 to STM32G0B1CEU6 (512K FLASH and 64K RAM) based on Nucleo-G071RB example.Modified mapping_fwimg.ld as below: /* Slots must be aligned on 2048 bytes (0x800) */ /* swap (4 kbytes) */ __ICFEDIT_SWAP_start__ = 0x08042000; __ICFEDIT_SWAP_end__ = 0x08042FFF; /* Active slot #1 (200 kbytes) */ __ICFEDIT_SLOT_Active_1_start__ = 0x08010000; __ICFEDIT_SLOT_Active_1_end__ = 0x08041FFF; __ICFEDIT_SLOT_Active_1_header__ = __ICFEDIT_SLOT_Active_1_start__; /* Dwl slot #1 (200 kbytes) */ __ICFEDIT_SLOT_Dwl_1_start__ = 0x08043000; __ICFEDIT_SLOT_Dwl_1_end__ = 0x08074FFF; /* Slots not configured */ __ICFEDIT_SLOT_Active_2_header__ = 0x00000000; __ICFEDIT_SLOT_Active_2_start__ = 0x00000000; __ICFEDIT_SLOT_Active_2_end__ = 0x00000000; __ICFEDIT_SLOT_Active_3_header__ = 0x00000000; __ICFEDIT_SLOT_Active_3_start__ = 0x00000000; __ICFEDIT_SLOT_Active_3_end__ = 0x00000000; __ICFEDIT_SLOT_Dwl_2_start__ = 0x00000000; __ICFEDIT_SLOT_Dwl_2_end__ = 0x00000000; __ICFEDI
Error in final launch sequence:Failed to execute MI command:load D:\\STUSER\\STM32CubeIDE\\workspace_1.13.0\\TEST190923\\Debug\\TEST190923.elfError message from debugger back end:Error finishing flash operation
Hello all,I have a question about possibility of splitting/dividing FLASH sector for active/download image slots.A bit more context... My target MCU is STM32F756ZGTx, here is its FLASH memory map:What we want to do is: assign sector 4 (128 kB) and sector 5 (256 kB) as a download image slot; assign sector 6 (256 kB) and half of sector 7 (1/2 * 256 kB = 128 kB) as an active image slot.My question is: can we do that?As far as I understand, SWAP and active/download slots should be aligned with FLASH sectors, so the answer would be "NO", but maybe I'm wrong.Thank in advance!
Good morning, I am facing an issue related to the usage of the CRC on the G070RB microcontroller (and user manual RM0454), specifically concerning the use of hardware-based CRC-16 MODBUS for a project currently under development at the company where I work. I have observed that when the CRC polynomial is set to 16 bits, the CRC chip processes the entire DR (Data Register) as 32 bits. In other words: my sequence 0xF704 is treated as 0x0000F704, where the chip first applies the CRC to the initial two bytes (0x0000) and then uses its CRC as the initial CRC to compute 0xF704. Consequently, through the microcontroller, I obtain a final CRC of 0xD747 instead of the expected 0x4346. Is there a way to apply the CRC only to 0xF704 while "masking" the 0x0000 in front of it? This issue becomes apparent when sending an odd number of 16-bit packets. Below is a draft of the code I have used: // Enable CRCuint32_t *RCC_AHB = 0x40021038;*RCC_AHB |= (1 << 12);// Set RefIn, RefOut bit by bit and P
..
Hi ST fanboys, I am using the STM32WL55 device and have implemented the latest cryptolib (4.1).This is all working fine with correct AES encryption and decryption, up to the moment that I start implementing the low power features and switch of all unused clocks and blocks. At that point the cryptolib features stop working.Sadly the Cryptolib documentation (what is available when looking hard) does not specify what hardware features of the STM32WL device are used ie. what clocks, what HW blocks???Can somebody point these out so I can activate those blocks when I come out of standby/stop mode and so that I can turn them off again when going into standby/stop mode.Features used in Crypto are TRNG, AES_CBC, AES-CTR thanks in advance
I am unable to import the TFM app for the B-U585I-IOTO2A board using MacOS Ventura 13.5.1. Every time I attempt it the importer takes a long time, then fails with a 'Fail on internal error' message. I am using the Import STM32Cube Example method of importing. In order to fix the problem I have done the following:1. Deleted and reinstalled STM32CubeIDE 1.13.12. Deleted and reinstalled the U5 library version 1.3.03. Rebooted the MacBook computerThese did not help at all. I have successfully installed the 3 required TFM projects for the STM32L562E-DK board. Those three projects installed in just a few seconds. It seems there is something wrong with the U5 TFM project. If I can provide further information, please let me know.
Hi,I've been exploring cryptography support on the STM32 uCs, especially on the L4 series. I'm able to run the X-CUBE-CRYPTOLIB code to perform AES-GCM, but it's very slow. It takes roughly 4ms to encrypt and tag 80 bytes, with a master clock of 8MHz. From looking at the debugger, it seems like the AES hardware peripheral is not being used, so it makes sense it's performing so poorly. I couldn't find any define in the .h files to configure it to use hardware support and I'm seeing conflicting statements from differents pieces of documentation. The Reference Manual for the L4 family states that "The AES peripheral provides hardware acceleration to AES cryptographic algorithms packaged in STM32 cryptographic library.".This version of the library documentation (from 2015) states that: "For dedicated devices some algorithms are supported with hardware acceleration, to optimize the performance and the footprint usage"However, the more recent version states that: "To benefit from STM32
Already have an account? Login
Enter your E-mail address. We'll send you an e-mail with instructions to reset your password.