Skip to main content
vik1970va
Associate II
Jan 28, 2020 4:44 AM UTC
Solved

Work with FSMC and two devices, problems with choosing one device

Hello,

My program uses two FSMC_Bank1 for the tft screen and memory (62WV51216ALL), NORSRAM3 is used for memory and NORSRAM4 for the screen, a problem has been identified that when accessing NORSRAM3 (memory), the CS signal (FSMC_NE3) goes low and remains so permanently. The same thing happens with the signal for the CS screen (FSMC_NE4) and when garbage from points are written to the memory on the screen. How can I return the CS signals to their normal position after accessing the right data source?

This topic has been closed for replies.
waclawek.jan
waclawek.janBest answer
Super User
Jan 29, 2020 12:15 PM UTC

At this point I'm out of ideas.

You may want to try to ask for help ST directly through the web support form.

JW

12 replies

waclawek.jan
waclawek.janBest answer
Super User
Jan 29, 2020 12:15 PM UTC

At this point I'm out of ideas.

You may want to try to ask for help ST directly through the web support form.

JW