Skip to main content
vik1970va
Associate II
Jan 28, 2020 4:44 AM UTC
Solved

Work with FSMC and two devices, problems with choosing one device

Hello,

My program uses two FSMC_Bank1 for the tft screen and memory (62WV51216ALL), NORSRAM3 is used for memory and NORSRAM4 for the screen, a problem has been identified that when accessing NORSRAM3 (memory), the CS signal (FSMC_NE3) goes low and remains so permanently. The same thing happens with the signal for the CS screen (FSMC_NE4) and when garbage from points are written to the memory on the screen. How can I return the CS signals to their normal position after accessing the right data source?

This topic has been closed for replies.
waclawek.jan
waclawek.janBest answer
Super User
Jan 29, 2020 12:15 PM UTC

At this point I'm out of ideas.

You may want to try to ask for help ST directly through the web support form.

JW

12 replies

vik1970va
vik1970vaAuthor
Associate II
Jan 28, 2020 6:45 AM UTC

STM32F407ZET

init SRAM

 readWriteTiming.FSMC_AddressSetupTime = 0x0F;	 
 readWriteTiming.FSMC_AddressHoldTime = 0x02;	
 readWriteTiming.FSMC_DataSetupTime = 0x0F;		 	 
 readWriteTiming.FSMC_BusTurnAroundDuration = 0x00;
 readWriteTiming.FSMC_CLKDivision = 0x00;
 readWriteTiming.FSMC_DataLatency = 0x00;
 readWriteTiming.FSMC_AccessMode = FSMC_AccessMode_B;	 
 
 
 
 FSMC_NORSRAMInitStructure.FSMC_Bank = FSMC_Bank1_NORSRAM3;
 FSMC_NORSRAMInitStructure.FSMC_DataAddressMux = FSMC_DataAddressMux_Disable; 
 FSMC_NORSRAMInitStructure.FSMC_MemoryType =FSMC_MemoryType_SRAM;// FSMC_MemoryType_SRAM; //SRAM 
 FSMC_NORSRAMInitStructure.FSMC_MemoryDataWidth = FSMC_MemoryDataWidth_16b;
 FSMC_NORSRAMInitStructure.FSMC_BurstAccessMode =FSMC_BurstAccessMode_Disable;// FSMC_BurstAccessMode_Disable; 
 FSMC_NORSRAMInitStructure.FSMC_WaitSignalPolarity = FSMC_WaitSignalPolarity_Low;
 FSMC_NORSRAMInitStructure.FSMC_AsynchronousWait=FSMC_AsynchronousWait_Disable;
 FSMC_NORSRAMInitStructure.FSMC_WrapMode = FSMC_WrapMode_Disable; 
 FSMC_NORSRAMInitStructure.FSMC_WaitSignalActive = FSMC_WaitSignalActive_BeforeWaitState; 
 FSMC_NORSRAMInitStructure.FSMC_WriteOperation = FSMC_WriteOperation_Enable;	
 FSMC_NORSRAMInitStructure.FSMC_WaitSignal = FSMC_WaitSignal_Disable; 
 FSMC_NORSRAMInitStructure.FSMC_ExtendedMode = FSMC_ExtendedMode_Enable;
 FSMC_NORSRAMInitStructure.FSMC_WriteBurst = FSMC_WriteBurst_Disable; 
 FSMC_NORSRAMInitStructure.FSMC_ReadWriteTimingStruct = &readWriteTiming;
 FSMC_NORSRAMInitStructure.FSMC_WriteTimingStruct = &readWriteTiming;
 FSMC_NORSRAMInit(&FSMC_NORSRAMInitStructure); 
 
 	FSMC_NORSRAMCmd(FSMC_Bank1_NORSRAM3, ENABLE); // BANK3	

init TFT

readWriteTiming.FSMC_AddressSetupTime = 0XF;	 // 1/168M=6ns*16=96ns	
 readWriteTiming.FSMC_AddressHoldTime = 0x00;	 
 readWriteTiming.FSMC_DataSetupTime = 24;			//6*25=150ns
 readWriteTiming.FSMC_BusTurnAroundDuration = 0x00;
 readWriteTiming.FSMC_CLKDivision = 0x00;
 readWriteTiming.FSMC_DataLatency = 0x00;
 readWriteTiming.FSMC_AccessMode = FSMC_AccessMode_A;	
 
 
	writeTiming.FSMC_AddressSetupTime =8;	 //ַ֘HCLK =48ns 
 writeTiming.FSMC_AddressHoldTime = 0x00;			
 writeTiming.FSMC_DataSetupTime = 8;		 //HCLK=54ns
 writeTiming.FSMC_BusTurnAroundDuration = 0x00;
 writeTiming.FSMC_CLKDivision = 0x00;
 writeTiming.FSMC_DataLatency = 0x00;
 writeTiming.FSMC_AccessMode = FSMC_AccessMode_A;	
 
 
 FSMC_NORSRAMInitStructure.FSMC_Bank = FSMC_Bank1_NORSRAM4;
 FSMC_NORSRAMInitStructure.FSMC_DataAddressMux = FSMC_DataAddressMux_Disable; 
 FSMC_NORSRAMInitStructure.FSMC_MemoryType =FSMC_MemoryType_SRAM;// FSMC_MemoryType_SRAM; //SRAM 
 FSMC_NORSRAMInitStructure.FSMC_MemoryDataWidth = FSMC_MemoryDataWidth_16b;
 FSMC_NORSRAMInitStructure.FSMC_BurstAccessMode =FSMC_BurstAccessMode_Disable;// FSMC_BurstAccessMode_Disable; 
 FSMC_NORSRAMInitStructure.FSMC_WaitSignalPolarity = FSMC_WaitSignalPolarity_Low;
	FSMC_NORSRAMInitStructure.FSMC_AsynchronousWait=FSMC_AsynchronousWait_Disable; 
 FSMC_NORSRAMInitStructure.FSMC_WrapMode = FSMC_WrapMode_Disable; 
 FSMC_NORSRAMInitStructure.FSMC_WaitSignalActive = FSMC_WaitSignalActive_BeforeWaitState; 
 FSMC_NORSRAMInitStructure.FSMC_WriteOperation = FSMC_WriteOperation_Enable;	
 FSMC_NORSRAMInitStructure.FSMC_WaitSignal = FSMC_WaitSignal_Disable; 
 FSMC_NORSRAMInitStructure.FSMC_ExtendedMode = FSMC_ExtendedMode_Enable; 
 FSMC_NORSRAMInitStructure.FSMC_WriteBurst = FSMC_WriteBurst_Disable; 
 FSMC_NORSRAMInitStructure.FSMC_ReadWriteTimingStruct = &readWriteTiming;
 FSMC_NORSRAMInitStructure.FSMC_WriteTimingStruct = &writeTiming; 
 
 FSMC_NORSRAMInit(&FSMC_NORSRAMInitStructure); 
 
 FSMC_NORSRAMCmd(FSMC_Bank1_NORSRAM4, ENABLE); // BANK1 

waclawek.jan
Super User
Jan 28, 2020 8:16 AM UTC

Read out and check/post content of FSMC registers.

JW

vik1970va
vik1970vaAuthor
Associate II
Jan 28, 2020 12:36 PM UTC

По�?ле запи�?и в пам�?ть

0690X00000Bwk1AQAR.png

waclawek.jan
Super User
Jan 28, 2020 2:38 PM UTC

This looks to be OK, I don't see anything obviously wrong here.

If you use the two peripherals separately (i.e. initialize only one of them in FSMC) they work OK?

Try to disable Bank1.

JW

vik1970va
vik1970vaAuthor
Associate II
Jan 29, 2020 4:08 AM UTC

Hello,

when one of the devices is turned off, the behavior of the CS (NE3 or NE4) signals becomes normal. disconnected separately the memory on the NE 4 logical analyzer; SWITCHED NORMALLY; turned off the screen (by setting comments on the screen); NE 3 switching is normal (attachment). The combined operation of the screen and memory causes a single change in the signal from 1 -> 0 at the outputs of NE 3 and NE 4

0690X00000BwlsPQAR.png

vik1970va
vik1970vaAuthor
Associate II
Jan 29, 2020 4:47 AM UTC

Changed the initialization order, at the beginning of the screen then the memory. The screen selection signal NE 4 now works fine. BUT the memory selection signal does not work. In the attachment, the screen from the moment the microcontroller resets.0690X00000BwltDQAR.png

Maybe something is wrong with the memory access? I give all the pieces of the appeal code:

void fsmc_sram_test_1(void)
{ u16 temp=0;
 fsmc_sram_test_write(0x0000,0xBBAA);
 temp=fsmc_sram_test_read(0X0000);
 LCD_ShowxNum(60,190,temp,6,16,0);
 printf("Data SINGL:%x\r\n",temp);
}
/*****************************************************/
void FSMC_SRAM_WriteBuffer(u16* pBuffer,u32 WriteAddr,u32 n)
{
	for(;n!=0;n--) 
	{										 
		*(vu16*)(Bank1_SRAM3_ADDR+WriteAddr)=*pBuffer;	 
		WriteAddr++;
		pBuffer++;
	} 
}																			 
/*****************************************************/
void FSMC_SRAM_ReadBuffer(u16* pBuffer,u32 ReadAddr,u32 n)
{
	for(;n!=0;n--) 
	{											 
		*pBuffer++=*(vu16*)(Bank1_SRAM3_ADDR+ReadAddr); 
		ReadAddr++;
	} 
} 
/*****************************************************/
void fsmc_sram_test_write(u32 addr,u16 data)
{			 
	FSMC_SRAM_WriteBuffer(&data,addr,1);
}
/*****************************************************/
u16 fsmc_sram_test_read(u32 addr)
{
	u16 data;
	FSMC_SRAM_ReadBuffer(&data,addr,1);
	return data;
}

vik1970va
vik1970vaAuthor
Associate II
Jan 29, 2020 5:37 AM UTC

Compulsory measures to return the signal have no effect :(

 *(vu16*)(Bank1_SRAM3_ADDR+0x0000)=0xBBAA; 
 GPIO_PinAFConfig(GPIOG,GPIO_PinSource10,GPIO_AF_RTC_50Hz); 
 GPIO_SetBits(GPIOG, GPIO_Pin_10);
 GPIO_PinAFConfig(GPIOG,GPIO_PinSource10,GPIO_AF_FSMC); 

In the simulator, everything is fine and in the iron there is no reaction to these actions.

waclawek.jan
Super User
Jan 29, 2020 8:10 AM UTC

Did you try to disable FSMC Bank1?

JW

vik1970va
vik1970vaAuthor
Associate II
Jan 29, 2020 8:23 AM UTC

I do not understand why disable FSMC Bank1?

I turned off the devices one at a time and the selection line began to work in both cases. The collaboration of the devices is incorrect, but turning off FSMC Bank1 how will I work with a memory chip and a screen? Separately, port Port G -> pin 10 switches normally without problems.

waclawek.jan
Super User
Jan 29, 2020 11:26 AM UTC

OK so let's call it subbank1, whatever.

In short, set FSMC_BCR1.MBKEN to 0 (as you can see on your screenshot above, it's set to 1 - that's the reset value for it). You can simply set the whole FSMC_BCR1 register to 0.

JW

vik1970va
vik1970vaAuthor
Associate II
Jan 29, 2020 12:02 PM UTC

disabled both bank1 and bank2, the result is the same NE3 does not respond

0690X00000BwnRBQAZ.png