Question
Why chaining TIM5 to TIM3 fail ?
I'm using a STM32L486RG and i try to chain TIM5 to TIM3 and it fail (TIM3->CNT doesn't increment). The other chaining combinations work correctly. Here is my test code:
#include <assert.h>
#include <stdbool.h>
#include "stm32l4xx.h"
#define TIM_MASTER TIM5
#define TIM_SLAVE TIM3
#define TIM_TS_ITR TIM_TS_ITR2 // look for "TIMx Internal trigger connection" in RM0351
static TIM_HandleTypeDef master_timer;
static TIM_HandleTypeDef slave_timer;
/**
* @brief This function is executed in case of error occurrence.
* @param file: The file name as string.
* @param line: The line in file as a number.
* @retval None
*/
void _Error_Handler(char *file, int line)
{
assert(false);
}
void master_init(void)
{
TIM_MasterConfigTypeDef master_config;
master_timer.Instance = TIM_MASTER;
master_timer.Init.Prescaler = (SystemCoreClock / 1000000) - 1; // 1 us tick
master_timer.Init.CounterMode = TIM_COUNTERMODE_UP;
master_timer.Init.Period = 0xFFFF;
master_timer.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
if (HAL_TIM_Base_Init(&master_timer) != HAL_OK) {
_Error_Handler(__FILE__, __LINE__);
}
master_config.MasterOutputTrigger = TIM_TRGO_UPDATE;
master_config.MasterOutputTrigger2 = TIM_TRGO2_UPDATE;
master_config.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
if (HAL_TIMEx_MasterConfigSynchronization(&master_timer, &master_config)
!= HAL_OK) {
_Error_Handler(__FILE__, __LINE__);
}
HAL_TIM_Base_Start(&master_timer);
}
void slave_init(void)
{
TIM_SlaveConfigTypeDef slave_config;
slave_timer.Instance = TIM_SLAVE;
slave_timer.Init.Prescaler = 0;
slave_timer.Init.CounterMode = TIM_COUNTERMODE_UP;
slave_timer.Init.Period = 0xFFFF;
slave_timer.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
if (HAL_TIM_Base_Init(&slave_timer) != HAL_OK) {
_Error_Handler(__FILE__, __LINE__);
}
slave_config.SlaveMode = TIM_SLAVEMODE_EXTERNAL1;
slave_config.InputTrigger = TIM_TS_ITR;
if (HAL_TIM_SlaveConfigSynchronization(&slave_timer, &slave_config)
!= HAL_OK) {
_Error_Handler(__FILE__, __LINE__);
}
HAL_TIM_Base_Start(&slave_timer);
}
void HAL_TIM_Base_MspInit(TIM_HandleTypeDef* tim_handle)
{
if (tim_handle->Instance == TIM1) {
__HAL_RCC_TIM1_CLK_ENABLE();
} else if (tim_handle->Instance == TIM2) {
__HAL_RCC_TIM2_CLK_ENABLE();
} else if (tim_handle->Instance == TIM3) {
__HAL_RCC_TIM3_CLK_ENABLE();
} else if (tim_handle->Instance == TIM4) {
__HAL_RCC_TIM4_CLK_ENABLE();
} else if (tim_handle->Instance == TIM5) {
__HAL_RCC_TIM5_CLK_ENABLE();
} else if (tim_handle->Instance == TIM8) {
__HAL_RCC_TIM8_CLK_ENABLE();
} else if (tim_handle->Instance == TIM15) {
__HAL_RCC_TIM15_CLK_ENABLE();
}
}
int main(void)
{
HAL_Init();
master_init();
slave_init();
while (true) {
}
}
#ifdef USE_FULL_ASSERT
/**
* @brief Reports the name of the source file and the source line number
* where the assert_param error has occurred.
* @param file: pointer to the source file name
* @param line: assert_param error line source number
* @retval None
*/
void assert_failed(uint8_t* file, uint32_t line)
{
/* User can add his own implementation to report the file name and line number,
ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
assert(false);
}
#endif