Skip to main content
chris239955_stm1_stmicro_com
Associate II
October 28, 2018
Question

Master/Slave problem on TIM3 in STM32L476 - slave not counting when ITR2 selected

Hello,

I am working on the NUCLEO-L476RG board. I am trying to use two pairs of counters in master/ slave mode. In the first chain TIM2 is the master and TIM4 is the slave so in SMCR of TIM4 ITR1 is selected and this works as expected. In the second chain TIM5 is the master and TIM3 is the slave so in SMCR of TIM3 ITR2 is selected and this does not work. Using the debugger I can see that TIM5 is counting but TIM3 is not. Also I have configured GPIO so that I can see action on oscilloscope.

I have tried setting SMCR of TIM3 to ITR0 (TIM1 master) and that works

I have tried setting SMCR of TIM3 to ITR1 (TIM2 master) and that works

I have tried setting SMCR of TIM3 to ITR3 (TIM4 master) and that works

Why does TIM3 not count when SMCR is set to ITR2 and TIM5 is master?

Reference Table 201 in RM0351

In all instances the master TIM has MMS in CR2 set to 2, UPDATE.

Thanks,

Chris

This topic has been closed for replies.

13 replies

Tesla DeLorean
Guru
October 28, 2018

Confirming your experience, on NUCLEO-L476RG

Here CNT at HAL_Delay(1000) intervals, TIM3 does not increment when TIM5 TRGO UPDATE is the ITR source, masters here dividing down 80 MHz to 1 Hz

TIM3:   0 TIM2:  14 TIM5:  14

TIM3:   1 TIM2:  45 TIM5:  45

TIM3:   2 TIM2:  75 TIM5:  75

TIM3:   3 TIM2: 105 TIM5: 105

TIM3:   4 TIM2: 135 TIM5: 135

TIM3:   5 TIM2: 165 TIM5: 165

TIM3:   6 TIM2: 195 TIM5: 195

TIM3:   7 TIM2: 225 TIM5: 225

TIM3:   8 TIM2: 255 TIM5: 255

TIM3:   9 TIM2: 285 TIM5: 285

TIM3:  10 TIM2: 315 TIM5: 315

TIM3:  11 TIM2: 345 TIM5: 345

TIM3:  12 TIM2: 375 TIM5: 375

TIM3:  13 TIM2: 405 TIM5: 405

TIM3:  14 TIM2: 435 TIM5: 435

TIM3:  15 TIM2: 465 TIM5: 465

TIM3:  16 TIM2: 495 TIM5: 495

TIM3:  17 TIM2: 525 TIM5: 525

TIM3:  18 TIM2: 555 TIM5: 555

TIM3:  19 TIM2: 585 TIM5: 585

TIM3:  20 TIM2: 615 TIM5: 615

TIM3:  21 TIM2: 645 TIM5: 645

TIM3:  22 TIM2: 675 TIM5: 675

..

Older manual, but consistent, and not working as described

0690X000006CGkyQAG.png

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
waclawek.jan
Super User
October 28, 2018

It's TIM15 not TIM5. Try.

@Imen DAHMEN​  can you please put it up to the list of things to fix in the documentation. Thanks.

JW

Tesla DeLorean
Guru
October 29, 2018

Yes, TIM15 seems to be what it is, stupid docs..

TIM3:  0 TIM15:  14

TIM3:  1 TIM15:  35

TIM3:  2 TIM15:  55

TIM3:  3 TIM15:  75

TIM3:  4 TIM15:  95

TIM3:  5 TIM15: 115

TIM3:  6 TIM15: 135

TIM3:  7 TIM15: 155

TIM3:  8 TIM15: 175

TIM3:  9 TIM15: 195

TIM3:  10 TIM15: 215

TIM3:  11 TIM15: 235

TIM3:  12 TIM15: 255

TIM3:  13 TIM15: 275

TIM3:  14 TIM15: 295

TIM3:  15 TIM15: 315

..

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
waclawek.jan
Super User
October 29, 2018

If you wonder how did I find out: remember how I always brag about the Interconnections chapter? Turns out in this case it was the one which contained the correct information...

;)

Jan

waclawek.jan
Super User
October 29, 2018

You have to look at the column, as it's TIM3's perspective as Slave, selected in TIM3_SMCR.TS

0690X000006CGrpQAG.png

JW

Tesla DeLorean
Guru
October 29, 2018

Ok, I was playing across not down. Wouldn't this table be more useful with boxes saying ITRx​?

​

Like playing battleships via sudoku.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
chris239955_stm1_stmicro_com
Associate II
October 29, 2018

In the timer section of the Reference Manual this is the information presented.0690X000006CGutQAG.png

I have been looking briefly through some of the Reference Manuals for STM32F family members and there is no Interconnection details section and I have always relied on the corresponding table to that inserted above. The other families present the TIM3-TIM5 connection and so the question is why make this change for the STM32L4xx series? And why not correct the information presented in the above table, this is after all revision 6 of RM0351. The same error is present in RM0392. It might be useful to have a bit in TIM3 OR1 or OR2 that enabled TIM3-TIM5 connection, just a thought!

Tesla DeLorean
Guru
October 29, 2018

Over the years I've concluded that some offices and conference rooms have low oxygen levels leading to mistakes and poor decisions. ​Or it could be that things aren't well thought through, and no one checks for accuracy and completeness of anything anymore.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
ST Technical Moderator
October 29, 2018

Hello,

This is raised internally for check and correction.

Kind Regards,

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
chris239955_stm1_stmicro_com
Associate II
October 29, 2018

Hello Imen,

Why has the change been made to replace TIM5 with TIM15 on ITR2? I ask because this now makes STM32L series different from the STM32F series.

I imagine it is too late to add a bit in an option register to make an option of either TIM5 or TIM15 for compatibility.

Kind regards,

Chris

waclawek.jan
Super User
October 29, 2018

Is there no related clickey in CubeMX?

JW