Skip to main content
albert2
Associate II
Oct 24, 2019 1:14 PM UTC
Question

Why an STM32L476's RTC counts more than 24h and don't icnreases the day

I've designed a board that has a STM32L476.

This part is supplied using a triple system of dual battery + power ( when it is available)

We've manufactured more than 20k units of them and they are working ok

A few days ago 2 boards came back to our design lab that exhibit the following symptoms :

-> The RTC keeps counting past 23:59:59 until 39:59:59

-> Neither on 23h nor 39h rollover the day gets increased

-> When trying to set the time we get the following data:

If the time is less than 20h, 20h get added to it

Else the hour is correctly set

-> Rollover behavior don't changes

If we force a reset of the CPU, the problem dissapears.

More data:

-> The RTC access is done using HAL libs.

-> The RTC isn't reset when setting the date/time

We still have one untouched board for testing, but any try to use a debugger would trigger a CPU reset, making the probblem dissapear. (This is why we lost ont of the boards )

Does anybody have a hint about what the problem could be ?

    This topic has been closed for replies.

    33 replies

    Associate III
    Dec 3, 2024 6:25 AM UTC

    Hi. Is this issue resolved?