Skip to main content
Associate III
Aug 8, 2024 2:35 PM UTC
Solved

Vrefint reads as 0 on some boards

I have got 3 identical boards with STM32u5a5. For improving ADC accuracy I want to calibrate Vref using Vrefint. This is working fine on one board, but on the other two boards Vrefint reads as 0 using the same software. Other ADC channels seem to work on all boards.

Vrefint has been enabled and a delay has been added giving Vrefint time to settle.

On the working device I get ADC values around 24600 for Vrefint (left aligned), on the non-working devices exactly 0.

Since everything is working fine on one device, I wonder what could be the issue on the other two devices.

This topic has been closed for replies.
Amel NASRI
Amel NASRIBest answer
ST Technical Moderator
Aug 9, 2024 3:41 PM UTC

Hi @Meixner ,

In the current driver implementation, we have following sequence of code in HAL_ADCEx_Calibration_Start():

 /* Use a Data Memory Barrier instruction to avoid synchronization issues when accessing ADC registers */
 MODIFY_REG(hadc->Instance->CR, ADC_CR_CALINDEX, 0x9UL << ADC_CR_CALINDEX_Pos);
 __DMB();
 MODIFY_REG(hadc->Instance->CALFACT2, 0xFFFFFF00UL, 0x03021100UL);
 __DMB();
 SET_BIT(hadc->Instance->CALFACT, ADC_CALFACT_LATCH_COEF);

Are you using an older version than 1.6.0for STM32CubeU5 firmware package?

-Amel

To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.

8 replies

MeixnerAuthor
Associate III
Aug 9, 2024 8:56 AM UTC

I have found a difference: On the working devices code was compiled with optimizations turned off, on the failing devices, the code was compiled with optimizations turned on in gcc.

I have tracked down the failing code to the ADC calibration. The calibration code is essentially the same as in HAL_ADCEx_Calibration_Start(). Enabling gcc optimizations makes the code fail.

MeixnerAuthor
Associate III
Aug 9, 2024 9:13 AM UTC

Replacing

MODIFY_REG(hadc->Instance->CR, ADC_CR_CALINDEX, 0x9UL << ADC_CR_CALINDEX_Pos);
MODIFY_REG(hadc->Instance->CALFACT2, 0x00FF0000UL, 0x00020000UL);
SET_BIT(hadc->Instance->CALFACT, ADC_CALFACT_LATCH_COEF);

in HAL_ADCEx_Calibration_Start() by

MODIFY_REG(hadc->Instance->CR, ADC_CR_CALINDEX, 0x9UL << ADC_CR_CALINDEX_Pos);
__NOP();
__NOP();
MODIFY_REG(hadc->Instance->CALFACT2, 0x00FF0000UL, 0x00020000UL);
SET_BIT(hadc->Instance->CALFACT, ADC_CALFACT_LATCH_COEF);

fixed the issue.

Amel NASRI
Amel NASRIBest answer
ST Technical Moderator
Aug 9, 2024 3:41 PM UTC

Hi @Meixner ,

In the current driver implementation, we have following sequence of code in HAL_ADCEx_Calibration_Start():

 /* Use a Data Memory Barrier instruction to avoid synchronization issues when accessing ADC registers */
 MODIFY_REG(hadc->Instance->CR, ADC_CR_CALINDEX, 0x9UL << ADC_CR_CALINDEX_Pos);
 __DMB();
 MODIFY_REG(hadc->Instance->CALFACT2, 0xFFFFFF00UL, 0x03021100UL);
 __DMB();
 SET_BIT(hadc->Instance->CALFACT, ADC_CALFACT_LATCH_COEF);

Are you using an older version than 1.6.0for STM32CubeU5 firmware package?

-Amel

To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.
waclawek.jan
Super User
Aug 12, 2024 12:30 PM UTC

Hi @Amel NASRI ,

e.g.

https://community.st.com/t5/stm32-mcus-products/adc-calibration-doesn-t-complete-on-stm32g0c1re/td-p/590459

https://community.st.com/t5/stm32-mcus-products/adc-register-adrdy-never-sets-when-i-enable-the-adc-so-it-keeps/m-p/106159/highlight/true#M17007

Maybe they are moot: I don't have the time/resources/abilities, nor access to the internal design, to judge and bring definitive conclusions about them.

Maybe there are more which went below my radar. I tend to ignore ADC-related threads, as I usually can't help, because ADC is very complicated (in a usually underappreciated way) and the details differ significantly between the individual families (ADC is perhaps the most varying module of them all).

JW