Question
Variables in domain D2 are not initialized ... here's why
By default, the variables in the D2 domain (SRAM1, SRAM2 and SRAM3) are not initialized by the linker because DATA_IN_D2_SRAM is not defined in the file system_stm32h7xx.c.
DATA_IN_D2_SRAM is used by SystemInit () which is called by the STM32H7xx_Startup.s file.
It would be preferable for DATA_IN_D2_SRAM to be defined by default, which would avoid looking long hours for the reasons why variables initialized in RAM1..3 are not ... don't you think so?
Best regards
Jean-Louis