Skip to main content
Sany
Associate III
Dec 19, 2024 2:33 PM UTC
Solved

STM32U575 GPDMA1 Configuration Problem

Hello,

I have a board with a STM32U575RGTX CPU, and i use SPI1 with a 2.8" TFT ILI9341 Display.
I got problems with the GPDMA1 configuration, and need help.

main.c:

 

 

int main(void)
{

 /* USER CODE BEGIN 1 */

 /* USER CODE END 1 */

 /* MCU Configuration--------------------------------------------------------*/

 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();

 /* USER CODE BEGIN Init */

 /* USER CODE END Init */

 /* Configure the system clock */
 SystemClock_Config();

 /* USER CODE BEGIN SysInit */

 /* USER CODE END SysInit */

 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_GPDMA1_Init();
 MX_CRC_Init();
 MX_TIM2_Init();
 MX_SPI1_Init();
 MX_ICACHE_Init();
 /* USER CODE BEGIN 2 */

 _lcd = ili9341_new(&hspi1, LCD_RESET_GPIO_Port, LCD_RESET_Pin, LCD_NSS_GPIO_Port, LCD_NSS_Pin, LCD_DC_GPIO_Port, LCD_DC_Pin, isoLandscape, LCD_CS_GPIO_Port,LCD_CS_Pin, LCD_IRQ_GPIO_Port, LCD_IRQ_Pin, itsNONE, itnNormalized);
 ili9341_fill_screen(_lcd, ILI9341_RED); // FILL SCREEN RED
 /* USER CODE END 2 */

 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 while (1)
 {
 /* USER CODE END WHILE */

 /* USER CODE BEGIN 3 */
 }
 /* USER CODE END 3 */
}

 

 

ILI9341:

 

 

void ili9341_fill_screen(ili9341_t *lcd, ili9341_color_t color)
{
 ili9341_fill_rect(lcd, color,
 0, 0, lcd->screen_size.width, lcd->screen_size.height);
}

void ili9341_fill_rect(ili9341_t *lcd, ili9341_color_t color,
 int16_t x, int16_t y, uint16_t w, uint16_t h)
{
 // verify we have something within screen dimensions to be drawn
 if (ibNOT(ili9341_clip_rect(lcd, &x, &y, &w, &h)))
 { return; }

 uint32_t num_pixels = w * h;
 uint32_t rect_wc = num_pixels;

 uint32_t block_wc = rect_wc;
 if (block_wc > __SPI_TX_BLOCK_MAX__)
 { block_wc = __SPI_TX_BLOCK_MAX__; }

 // fill entire block with ordered color data
 uint16_t color_le = __LEu16(&color);
 for (uint16_t i = 0; i < block_wc; ++i)
 { spi_tx_block[i] = color_le; }

 // select target region
 ili9341_spi_tft_set_address_rect(lcd, x, y, (x + w - 1), (y + h - 1));
 ili9341_spi_tft_select(lcd);

 HAL_GPIO_WritePin(lcd->data_command_port, lcd->data_command_pin, __GPIO_PIN_SET__);

 // repeatedly send MIN(remaining-words, block-words) words of color data until
 // all rect words have been sent.
 uint32_t curr_wc;
 while (rect_wc > 0) {
 curr_wc = rect_wc;
 if (curr_wc > block_wc)
 { curr_wc = block_wc; }
 ili9341_transmit_color(lcd, curr_wc * 2/*16-bit words*/, spi_tx_block, ibYes);
 rect_wc -= curr_wc;
 }

 ili9341_spi_tft_release(lcd);
}

void ili9341_transmit_color(ili9341_t *lcd, uint16_t size, uint16_t color[]/* already byte-swapped (LE) */, ili9341_bool_t wait)
{
 if ((NULL == lcd) || (0 == size) || (NULL == color))
 { return; }
 HAL_SPI_Transmit_DMA(lcd->spi_hal, (uint8_t *)color, size);
 if (ibOK(wait))
 { ili9341_transmit_wait(lcd); }
}

 

 

When i use HAL_SPI_Transmit_DMA, then the colors on the TFT are not correct (Red=Magenta,Green=Green,Blue=Black), if i change the code to HAL_SPI_Transmit without DMA, then the colors are correct... what can be wrong in my DMA Config?

Here is my config:

spi1.pngspi2.pngspi3.png

SPI is configured with 8-Bit and MSB.

This topic has been closed for replies.
Imen.DBest answer
ST Technical Moderator
Dec 19, 2024 5:46 PM UTC

Hello @Sany 

Please follow the steps in this article to start your project and configure the GPDMA: 

How to configure the GPDMA - STMicroelectronics Community

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks

2 replies

Imen.DBest answer
ST Technical Moderator
Dec 19, 2024 5:46 PM UTC

Hello @Sany 

Please follow the steps in this article to start your project and configure the GPDMA: 

How to configure the GPDMA - STMicroelectronics Community

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Sany
SanyAuthor
Associate III
Dec 19, 2024 6:40 PM UTC

Hello @Imen.D ,

Thanks for this Article, that helps me.

my configuration for the GPDMA is correct, but i forgot to activate "Source Address Increment After Transfer" and changed the Data Width to Byte, and it works.