Skip to main content
Associate
May 5, 2026 8:25 AM UTC
Solved

STM32U5 Flash endurance ?

Hello,

I am working on a project where I need to both read and write regularly into the STM32 flash memory. I have some concerns and questions regarding its endurance.

First off, I posted a question not long ago about writing to FLASH using ST EEPROM library. I was wondering why upon writing to a variable, it did not effectively write it into flash. This is essentially due to how the library itself works. Hence why I can not really use it to manage flash wearing, because I need the writing to happen precisely when I call a write function due to the fact that my product can be power off at any moment.

So going back to the reference manual RM0456, I came upon section 7.3.8 which states:

"Each flash memory page can be written and erased 10 000 or 100 000 times. A maximum of
32 pages (256 Kbytes) per bank feature this increased endurance of 100 kcycles. This
enhanced endurance can be used for data storage that usually needs more intensive
cycling capability than code storage.
Any flash page can be chosen to be cycled up to 100 kcycles. As soon as a page is above
10 kcycles, it is considered as high cycling page (even if not yet at 100 kcycles). The
application must take care not to exceed 32 pages cycled more than 10 000 times."

 

This paragraph makes me wonder about a few things:

  • What kind of FLASH memory is embedded into the STM32U5 (NOR or NAND) ?
  • What is the reason for the wearing of FLASH ? Is it writing into the FLASH or is it erasing it (mass erase or page erase) ? For instance, does writing only 0 into the flash wear it ?
  • What is ST's recommended way to deal with flash wearing ? How does one tell the flash controller to configure a page do be cycled up to 100k cycles rather than 10k ? Is it through an option byte in flash registers ? Is it something else ? Is there a library that handle FLASH wearing ?

Thanks in advance

 

waclawek.jan
waclawek.janBest answer
Super User
May 12, 2026 2:58 PM UTC

This has been discussed here several times, e.g. here and  here.

> What kind of FLASH memory is embedded into the STM32U5 (NOR or NAND) ?

It doesn't matter, as it's the behaviour which matters, not the moniker.

Besides, the basic physical principle (i.e. floating gate) is identical for both, and thus the basic wear mechanisms are identical, too.

> What is the reason for the wearing of FLASH ? Is it writing into the FLASH or is it erasing it (mass erase or page erase) ? For instance, does writing only 0 into the flash wear it ?

Both writing and erasing. The datasheet number is usually given for write-erase cycle. There may be multiple writes to different portions of a page, if the given FLASH allows it (and in STM32 FLASH, it does, as the write granule is quad-word).

Besides individual pages having a cycle limit, there is also a cumulative cycle limit for the whole FLASH (or a bank), due to wear of the HV sources/switches needed for the FLASH operations. This is probably the reason for the "only 32 pages per bank may be cycled up to 100k" limit.

There are also secondary issues like crosstalk between neighbouring rows, which gets worse with increasing number of cycles.

> What is ST's recommended way to deal with flash wearing ?

Don't wear it beyond what's specified. How do you achieve that, it's up to you and the application.

In some applications, for example, it may be perfectly OK to maintain a counter in one word of the cycled page, and when this counter reaches the limit, the product simply stops working. You'd consider this to be outrageous for most applications, but there are applications out there where this is perfectly OK.

A common strategy is to reduce cycles per change, e.g. you won't erase the whole page and then write a single value, but design some journaling method to allow multiple writes of the same "variable" into a page. Using multiple pages is another strategy to reduce wear on individual page. Another strategy is to have a backup power source - usually a large enough capacitor - to extend runtime beyond primary power failure (suitably monitored), to allow writeback from RAM cache to FLASH/EEPROM.

There are too many options for one library to be reasonably effective for all of them, so in most of the cases it's more reasonable to write your own solution tailor-fit to your application.

There may be also no solution for you within the constraints given by FLASH endurance and your application's requirements. In that case you may want to consider different physical approach, e.g. using battery backup (all STM32 have a couple of battery-backup registers in RTC/TAMP; some STM32 do have battery-backup RAM - not the 'U5 but you there may consider using some of the ultralow-power modes which support RAM retention); or fast high-cycle nonvolatile memories like FRAM or MRAM.

> How does one tell the flash controller to configure a page do be cycled up to 100k cycles rather than 10k? 

You don't. The specifaction is, that you may wear *any* page beyond 10k, but only 32 pages per bank. So you choose, which pages are you going to wear significantly (i.e. use in EEPROM-like role), but only can choose only 32 pages to do so.

Also note, that once you wear a page beyond 10k, a different max programming/erasing timing applies for that page (see datasheet). While from this fact it may appear that there's some abrupt change at 10k (which would imply an embedded counter), no, that's simply that the programming/erasing times increase with wear and ST gives an upper bound to them based on testing.

JW

5 replies

cflAuthor
Associate
May 12, 2026 1:25 PM UTC

Does anyone have any answer for me ?

mƎALLEm
ST Technical Moderator
May 12, 2026 1:42 PM UTC

Hello,

I cannot answer all of your questions. 

Meanwhile:

- The internal memory is a NOR flash not a NAND flash.

- The EEPROM emulation library X‑CUBE‑EEPROM implements already the wear leveling:

AN4894 "How to use EEPROM emulation on STM32 MCUs" 

mALLEm_0-1778593219829.png

mALLEm_0-1778593436909.png

- Writing 0 is considered as a write to the Flash so indeed it wear it.

Good luck.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
cflAuthor
Associate
May 12, 2026 2:06 PM UTC

Thank you for the answer. I have already taken a look at X-CUBE-EEPROM. It doesn't seem to be working for my case because I need data to be written directly to be resilient to a power loss. The answer one of your colleague gave me was that a page is never fully written until it is completely full in RAM, which then triggers a page transfer.

mƎALLEm
ST Technical Moderator
May 12, 2026 2:13 PM UTC

Ok. need to separate questions here.


@cfl wrote:

It doesn't seem to be working for my case because I need data to be written directly to be resilient to a power loss. 


In that case you need to rework the algorithm to fit your needs. But that will definitely increase the Flash wearing.

Better to keep the EEPROM emulation algorithm implementation in the other discussion in this link.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
waclawek.jan
waclawek.janBest answer
Super User
May 12, 2026 2:58 PM UTC

This has been discussed here several times, e.g. here and  here.

> What kind of FLASH memory is embedded into the STM32U5 (NOR or NAND) ?

It doesn't matter, as it's the behaviour which matters, not the moniker.

Besides, the basic physical principle (i.e. floating gate) is identical for both, and thus the basic wear mechanisms are identical, too.

> What is the reason for the wearing of FLASH ? Is it writing into the FLASH or is it erasing it (mass erase or page erase) ? For instance, does writing only 0 into the flash wear it ?

Both writing and erasing. The datasheet number is usually given for write-erase cycle. There may be multiple writes to different portions of a page, if the given FLASH allows it (and in STM32 FLASH, it does, as the write granule is quad-word).

Besides individual pages having a cycle limit, there is also a cumulative cycle limit for the whole FLASH (or a bank), due to wear of the HV sources/switches needed for the FLASH operations. This is probably the reason for the "only 32 pages per bank may be cycled up to 100k" limit.

There are also secondary issues like crosstalk between neighbouring rows, which gets worse with increasing number of cycles.

> What is ST's recommended way to deal with flash wearing ?

Don't wear it beyond what's specified. How do you achieve that, it's up to you and the application.

In some applications, for example, it may be perfectly OK to maintain a counter in one word of the cycled page, and when this counter reaches the limit, the product simply stops working. You'd consider this to be outrageous for most applications, but there are applications out there where this is perfectly OK.

A common strategy is to reduce cycles per change, e.g. you won't erase the whole page and then write a single value, but design some journaling method to allow multiple writes of the same "variable" into a page. Using multiple pages is another strategy to reduce wear on individual page. Another strategy is to have a backup power source - usually a large enough capacitor - to extend runtime beyond primary power failure (suitably monitored), to allow writeback from RAM cache to FLASH/EEPROM.

There are too many options for one library to be reasonably effective for all of them, so in most of the cases it's more reasonable to write your own solution tailor-fit to your application.

There may be also no solution for you within the constraints given by FLASH endurance and your application's requirements. In that case you may want to consider different physical approach, e.g. using battery backup (all STM32 have a couple of battery-backup registers in RTC/TAMP; some STM32 do have battery-backup RAM - not the 'U5 but you there may consider using some of the ultralow-power modes which support RAM retention); or fast high-cycle nonvolatile memories like FRAM or MRAM.

> How does one tell the flash controller to configure a page do be cycled up to 100k cycles rather than 10k? 

You don't. The specifaction is, that you may wear *any* page beyond 10k, but only 32 pages per bank. So you choose, which pages are you going to wear significantly (i.e. use in EEPROM-like role), but only can choose only 32 pages to do so.

Also note, that once you wear a page beyond 10k, a different max programming/erasing timing applies for that page (see datasheet). While from this fact it may appear that there's some abrupt change at 10k (which would imply an embedded counter), no, that's simply that the programming/erasing times increase with wear and ST gives an upper bound to them based on testing.

JW