Skip to main content
Associate II
February 20, 2026
Solved

STM32L476RET6 no pinout for ADC1_IN0? How to calculate VDDA with Vrefint?

Hi,

I am making updates to a custom PCB where I would like to add ADC functionality. My board is powered by batteries and I expect the supply voltage to fluctuate slightly and I need the ADC conversions to be accurate. The reference manual says I can use the internal Vrefint to calculate what the value of VDDA/VREF+ so that I may calculate my conversions with better accuracy. Additionally, I wanted to follow this guide (https://community.st.com/t5/stm32-mcus/how-to-use-the-stm32-adc-s-internal-reference-voltage/ta-p/621425) to understand how I may implement this in firmware.

The issue I see now is that on the chip's datasheet it mentions that Vrefint is internally connected to ADC1_IN0, however, ADC1_IN0 has no pinout on this package of the chip. Furthermore, in STM32CubeMX the ADC1_IN0 channel is not able to be selected (although Vrefint channel is able to be selected).

Now I have some confusion since the datasheet mentions the internal connection. Maybe this package does not have this available? But STM32CubeMX allows me to select the Vrefint channel still, so I may not understand something.

Is there some way I may achieve ADC accuracy with some other method? Or perhaps I am missing some information?

Please let me know if anyone may be able to help me understand this better.

Thank you,

Kaitlyn

TDK
TDKBest answer
February 20, 2026

VREFINT is an internal net. It is not exposed on a pin.

In STM32CubeMX, the Vrefint channel is the ADC1_IN0 channel. It's available on all packages.

"If you feel a post has answered your question, please click ""Accept as Solution""."

4 replies

TDK
TDKBest answer
February 20, 2026

VREFINT is an internal net. It is not exposed on a pin.

In STM32CubeMX, the Vrefint channel is the ADC1_IN0 channel. It's available on all packages.

"If you feel a post has answered your question, please click ""Accept as Solution""."
KRauccioAuthor
Associate II
February 20, 2026

Thank you for your clarification. I had known Vrefint was internally connected, but I had assumed that the channel would need to at least be enabled or have a pinout. I see this is different from other chips like the one used in the guide.

I understand now.

Thank you,

Kaitlyn

TDK
February 20, 2026

The guide enables two channels: channel 0 and VREFINT. They are independent. On that chip, channel 0 is not VREFINT.

The VREFINT channel is never exposed on a pin. It is always internal-only.

"If you feel a post has answered your question, please click ""Accept as Solution""."