Skip to main content
Associate
September 18, 2024
Solved

STM32H725 usb missing ux_dcd_stm32.h

  • September 18, 2024
  • 2 replies
  • 1196 views

Subject: STM32H7 USBX Virtual COM Port Setup - Missing ux_dcd_stm32.h File

Hello ST Community,

I'm working on setting up a USB Virtual COM port on an STM32H7 microcontroller using Azure RTOS (AzureRTOS-H7). I'm encountering an issue with missing USBX files, specifically the STM32 device controller driver header.

**Project Details:**
- Microcontroller: STM32H7 (specific model: STM32H725RGVX)
- IDE: STM32CubeIDE (Version: 1.16.0)
- Azure RTOS Package Version: 3.3.0

I Have tried

  1. Created a new STM32H7 project in STM32CubeIDE
  2. Enabled USB in the .ioc file(Device Only)
  3. Configured USBX middleware
  4. Checked the following packages in the manager
    1. Core System
    2. UX Device CoreStack
    3. UX Device Class CDC ACM
  5. Enable the the USB USBX

**Issue:**
After enabling USB in the .ioc file and generating the code, I'm getting the following error when trying to compile:

```
app_usbx_device.h:32:10: fatal error: ux_dcd_stm32.h: No such file or directory
```

Any guidance or suggestions would be greatly appreciated. Thank you in advance for your help!

[Your Name/Username]

This topic has been closed for replies.
Best answer by Imen.D

Hello @MiB_s,

Make sure to Include the correct paths to your include directories.

This article may help you: How to implement the USB device composite class in... - STMicroelectronics Community

You can also refer to this github repository : 

x-cube-azrtos-h7/Middlewares/ST/usbx/common/usbx_stm32_device_controllers/ux_dcd_stm32.h at d3b54df40c7a6a6ccaa998cfec71cbe148299726 · STMicroelectronics/x-cube-azrtos-h7 (github.com)

2 replies

Imen.DBest answer
ST Technical Moderator
September 18, 2024
In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
MiB_sAuthor
Associate
September 18, 2024

It seems that the file is missing when i generate the project, i tried to copy the ux_dcd_stm32.h into the folder(\Middlewares\ST\usbx\common\usbx_device_classes\inc\) and this seems to fix the problem building the project. So thanks for the help!