Skip to main content
Associate II
June 16, 2025
Solved

STM32H7 FMC and 16bits device

  • June 16, 2025
  • 11 replies
  • 2215 views

Hello,

I'm kind of newbie in the STM32 world, I'm more used with another brand of 32bits microcontroller that also have a "parrallel port" for interfacing external ram device.

My concern is about the FMC on the STM32H7.

I want to read/write a 16bits device.

Currently I'm using this configuration (almost the default one) :

Alex_J_0-1750105595053.png

My code for testing a write operation :

Alex_J_2-1750105719339.png

....

Alex_J_1-1750105684339.png

 

I can't see any problem in the code but when I check signals with an oscilloscope, I can see that the CPU is issuing 4 consecutive write operation :

Alex_J_3-1750105798354.png

 

A0 / A1 are also increasing as if the CPU is writing to 4 different places.

How can it be possible.

I have seen in the datasheet that when AXI bus and external bus is different size, it can occurs. But in that case how to perform a correct 16 bit operation ??

Other people seems to have this kind of trouble but nobody replied with a solution :

https://community.st.com/t5/stm32-mcus-products/h7-series-fmc-question/td-p/131535

https://community.st.com/t5/stm32-mcus-embedded-software/fmc-accessed-in-32-bit-but-cs-asserted-for-twice-long-64-bits/m-p/274657

Thanks in advance for any help

 

 

This topic has been closed for replies.
Best answer by Alex_J

Currently, I manage to make it work but it's not the way I thought.

I had to change the bank address to 0xC0000000

and deactivate MPU.

I can see one write cycle and my device is now working as expected.

But I'm not sure it's a good idea to deactivate the MPU.

I later found this related thread :

https://community.st.com/t5/stm32-mcus-touchgfx-and-gui/stm32h743ii-fmc-8080-lcd-spurious-writes/td-p/354191

 

By the way, it's sad that cubeide didn't warm you about the bank remapping needed in 16 bits mode needed for sram/nor/lcd..

11 replies

TDK
June 16, 2025

The HAL_SRAM_Write_16b function only does 32-bit word-aligned accesses. There may be an underlying hardware reason for this. To write 16 bits, it reads 32 bits, applies the mask, then writes 32 bits.

stm32h7xx-hal-driver/Src/stm32h7xx_hal_sram.c at 85d65b023f9621e417177a87553d25b7b387239f · STMicroelectronics/stm32h7xx-hal-driver

Four CS operations matches this behavior. Two 16-bit reads plus two 16-bit writes.

 

If you want a 16-bit access, I'd just do a 16-bit access write.

*(volatile uint16_t*)address = value;

"If you feel a post has answered your question, please click ""Accept as Solution""."
Alex_JAuthor
Associate II
June 16, 2025

@TDK Thanks for your fast answer, but I quickly tried your solution :

Alex_J_0-1750108261731.png

But I still get the 4 write operations.

The goal is to write to a peripheral that will only accept one write operation by 16bits data. 

Pavel A.
June 16, 2025

While waiting for better answers, can you do another quick experiment?

Using the MPU disable caching on your external memory window.

Per AN4839, the 0x60000000-0x7FFFFFFF range on STM32H7 is "normal memory", cacheable. What you see could be loading the 32-byte cache line and write back.

Also, check the suitable memory mode for FMC: should it be "SRAM" or other? 

 

Alex_JAuthor
Associate II
June 17, 2025

@Pavel A.

Thanks for your answer, but currently, caching is disable for this region :

Alex_J_0-1750136745544.png

 

 

waclawek.jan
Super User
June 17, 2025

> when I check signals with an oscilloscope, I can see that the CPU is issuing 4 consecutive write operation :

How do you know those are *write* operations? Which signal do you display there?

Do you have that area set as Device or as Memory in MPU?

JW

Alex_JAuthor
Associate II
June 17, 2025

I'm sorry that I forgot to mention that the signal shown is the WE send from the STM32 to the device.

waclawek.jan
Super User
June 18, 2025

Do you have the used FMC memory area set as Device or as Memory in MPU?

JW

Alex_JAuthor
Associate II
June 18, 2025

@waclawek.jan 

Either I don't know where to search for this option, either it did not exist xD :

Alex_J_0-1750276998280.png

 

Alex_J_1-1750277036714.png

 

 

Edit :

I also try to deactivate the MPU without success, I still have 4 write cycle.

waclawek.jan
Super User
June 19, 2025

waclawekjan_0-1750310238108.png

I don't use CubeMX and have no idea how those clickable things translate to the MPU settings, sorry. Maybe somebody more versed in Cube/CubeMX will chime in.

(I should have written "Normal" instead of "Memory" above).

I don't know which 'H7 you are using, so I looked into RM0433 (for 'H743 and kin) and there's an option to remap the SRAM/NOR area of FMC to a different address, which is by default set to Device:

waclawekjan_1-1750310595243.png

The remap in the 'H743 is accomplished through setting the FMC_BCR1.BMAP bitfield

waclawekjan_2-1750310685226.png

 

However, if you apply MPU settings onto a memory area, its those MPU settings which override the defaults, so here you would perhaps want to do only the remap without using MPU at all.

Again, I have no idea how is this clicked in CubeMX.

And still, this is just one thing to try, I don't say this will certainly solve your problem. The Cortex-M7 is an overcomplicated beast and the 'H7 in particular adds a couple of extra layers of complexities to it.

JW

 

Pavel A.
June 19, 2025

I'm looking at one project for STM32H753 with FPGA, there we defined the FMC "instance" type as NOR, not as SRAM. The windows addresses are in 0x60000000 range; set in MPU as non-shared device; not remapped.

32-bit accesses to the FPGA work just fine, no unexpected behavior.