Skip to main content
Associate II
Apr 8, 2026 7:37 AM UTC
Solved

STM32H563ZIT6 cannot receive RS485 at high baud rates (e.g. 12 Mbaud)

TX works but RX interrupt not triggered

 

Hello,

I am currently using a custom board based on STM32H563ZIT6. My goal is to establish communication over RS485 between the STM32 and a PC (using Hterm). The system is designed to receive a command and send a response.


Communication Details:

  • Interface: RS485 (half-duplex)
  • PC Tool: Hterm
  • Converter: USB COM 485 PLUS 4
  • Packet size: Very small (typically 4 bytes)
  • Transmission interval: ≥ 300 ms

Current Situation:

  • Communication works perfectly between 115200 and 2,000,000 baud
  • I am trying to increase the baud rate up to 12 Mbaud

Problem:

At 12 Mbaud:

  • STM32 → PC communication works correctly
    (I can see transmitted data on Hterm)
  • PC → STM32 communication does NOT work
    • STM32 does not receive any data
    • RX interrupt is not triggered at all
    • It behaves as if no data is arriving

Additional Notes:

  • I have checked the termination resistor, and it seems correct
  • The data sent from PC is valid (verified from Hterm)
  • UART baud rate is configured up to 12.5 Mbaud in CubeMX
  • The issue only appears at very high baud rates

What I Suspect:

  • Possible limitation of RS485 converter at high baud rates
  • UART sampling/timing issues at 12 Mbaud
  • Interrupt-based reception may not be sufficient at such speeds
  • Hardware limitations (signal integrity, cable, etc.)

Questions:

  1. Is it realistic to achieve 12 Mbaud over RS485 in this setup?
  2. Could this be a limitation of the USB-RS485 converter?
  3. Are there any specific STM32 UART settings required for such high speeds?
  4. Should DMA be used instead of interrupt for reliable reception?
  5. Are there known limitations for STM32H5 series UART at these speeds?

Any insights or similar experiences would be very helpful.

Thanks in advance!

MES98Best answer
Associate II
Apr 15, 2026 3:06 PM UTC

Thank you all for your support and valuable suggestions.

I would like to briefly summarize the issue and the solution, in case it helps others in the future.

Initially, when using interrupt-based reception, I was able to reach up to around 4 Mbaud reliably.
After switching to DMA, I was able to increase this up to 8 Mbaud.

However, I could never reach the 10 Mbaud value stated in the datasheet — at that speed, I was neither able to receive nor transmit data reliably.

While going through the datasheets more carefully, I noticed that the UART clock is 24 MHz, and in simple terms, the achievable baud rates follow a relation like 24 / n (Mbaud).

Based on this, I tested different baud rates again:

  • My device still cannot reliably communicate at 10 Mbaud
  • But interestingly, it works perfectly at 12 Mbaud

So it seems that certain baud rates are more “naturally aligned” with the clock configuration, while others are not achievable due to divider limitations.


Thanks again to everyone for the help.
Have a great day!

41 replies

mƎALLEm
ST Technical Moderator
Apr 8, 2026 9:52 AM UTC

Hello @MES98 and welcome to the ST community,

You said the Rx interrupt is not triggering at all at 12 Mbaud but it does at lower baud rates.

Are you sure there is no interrupt triggered at all? did you set a breakpoint in the Rx interrupt callback?

Try also to use DMA for the reception.

 


@MES98 wrote:
  1. Could this be a limitation of the USB-RS485 converter?

It could be.

What about the RS485 transceiver you are using from STM32 side? does it support a communication up to 12MBaud?

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
MES98Author
Associate II
Apr 8, 2026 10:01 AM UTC

I put a breakpoint in the UART Rx callback, and no interrupt is triggered at all.

Also, I discovered something interesting: when I connect two RS485 lines directly to each other, the STM32 is able to send and receive data at 12 Mbaud without any issues.

Based on this, I suspect that the problem is related to Windows, Hterm, or the USB COM485 PLUS 4 converter, rather than the STM32 or my code.

mƎALLEm
ST Technical Moderator
Apr 8, 2026 10:02 AM UTC

@MES98 wrote:

Based on this, I suspect that the problem is related to Windows, Hterm, or the USB COM485 PLUS 4 converter, rather than the STM32 or my code.


Indeed! 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Andrew Neil
Super User
Apr 8, 2026 10:38 AM UTC

@MES98 wrote:
  • Possible limitation of RS485 converter at high baud rates

 

2. Could this be a limitation of the USB-RS485 converter?


Have you tried using an oscilloscope to see what's actually happening on the wires - particularly at the STM32's RX pin?

That would soon show you if there's a hardware/connectivity issue ...

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
MES98Author
Associate II
Apr 8, 2026 2:03 PM UTC

Yes, I checked the signals with an oscilloscope, including at the STM32 RX pin, and everything looks fine.

Also, communication works without any issues up to 2 Mbaud.

unsigned_char_array
Lead III
Apr 8, 2026 10:45 AM UTC

At such high baudrates I recommend using the DMA to receive. An interrupt for each character is not fast enough. Though you should be getting interrupts.


Aside from the termination resistor have you checked the bias network?


Check the drive enable delay. I needed to set it to maximum to avoid corrupting the last bit. Disabling the drive too soon or too late can cause corrupted bits.

 

Have you used a logic analyzer to check the signal integrity at the MCU pins?

"Kudo posts if you have the same problem and kudo replies if the solution works.Click ""Accept as Solution"" if a reply solved your problem. If no solution was posted please answer with your own."
Andrew Neil
Super User
Apr 8, 2026 2:08 PM UTC

@MES98 wrote:
  • Communication works perfectly between 115200 and 2,000,000 baud
  • I am trying to increase the baud rate up to 12 Mbaud


Use the scope to see what's different (apart from just bit timing) between 2M and 12M baud.

Have you tried to narrow down where the failure actually starts between 2M and 12M ?

eg, try 7M - ie, halfway between 2 & 12

  • If that works, try 9.5M - ie, halfway between 7 & 12
  • If that fails, try 4.5M - ie, halfway between 2 & 7

etc, etc, ...

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Visitor II
Apr 9, 2026 3:17 AM UTC

I see a huge negative going spike at the start of frame, at all baud rates.

Will this cause a problem for start detection?

Can you also check if the probe ground is connected by a very short wire to circuit ground? Not the usual long tail crocodile.

 

Ozone
Principal
Apr 9, 2026 5:58 AM UTC

> I see a huge negative going spike at the start of frame, at all baud rates.

Basically on every falling edge.
I suppose this is an artifact, because the probe and the way it is attached are not appropriate for RF.

Mind you, a digital (square-wave) signal requires a bandwidth significantly higher than the bps number.

Andrew Neil
Super User
Apr 9, 2026 9:26 AM UTC

Also, those edges look rather slow

12MBaud.jpg

As @Ozone said, hard to tell if that's real, or an artifact of the scope and/or probe ...

 

@MES98 Doesn't your scope have a way to download screennshots?

That would give much better results than trying to photograph the screen!

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Ozone
Principal
Apr 9, 2026 10:18 AM UTC

> Also, those edges look rather slow

Yes, I very much agree. Although I'm not sure how the scope bandwidth, resolution and probe attachment affect this.
Probably one of the lower-end scopes, with 2 channels, 8-bit resolution and around 100MHz.

I suppose your are aware of the Laplace / Fourier theorems, and the bandwidth requirement this implies. There does not seem much beyond the second harmonic present in the shown signal.

 

mƎALLEm
ST Technical Moderator
Apr 9, 2026 9:35 AM UTC

@MES98 

Just to be sure, what GPIO speed you set for the Tx and Rx pins? Did you set them to "Very High"?

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
MES98Author
Associate II
Apr 9, 2026 11:00 AM UTC

@Kalpak I don’t think it is causing a problem, but honestly I’m not sure why it appears.
If it were an issue, I would expect it to also affect communication at 2 Mbaud or 4 Mbaud, but those work without any problems.

Also, I am not using a long crocodile ground lead. As you suggested, I am measuring the differential lines using a very short, thin ground connection.

@Ozone You might be right. I don’t have very deep experience in this area, and my oscilloscope is relatively old, so the measurements might be affected by its limitations.

 

@unsigned_char_array I am already measuring it in this way :(

 

@Andrew Neil Unfortunately, my oscilloscope does not support direct screenshot export.
However, I can capture the signal using single trigger mode and then take a picture of the screen.


@mƎALLEm Yes, the GPIO speed is set to Very High.
You can also see it in the image I shared.
There might still be a misconfiguration in other settings though.

 

@Ozone 

Yes, you guessed my oscilloscope quite well :D I am using a GW Instek GDS-1104S, and it does have some limitations.

By the way, the transmitted data is just a 4-byte packet.
What would you recommend I try next?

At the moment, I am planning to test using the LPUART peripheral, which theoretically supports much higher baud rates (up to 50 Mbaud).
I will share an update if I observe any changes.

MES98_0-1775732380101.png

MES98_1-1775732427345.png

 

Pavel A.
Apr 9, 2026 11:36 AM UTC

Can it be unhandled RX overrun or error condition?

 

Michal Dudka
Lead
Apr 9, 2026 6:10 PM UTC

You're not so much interested in the waveform on the RS485, but rather in the signal waveform after the receiver on the STM32 side. Measure it as accurately as possible directly at the STM32's RX pin. This will help you determine whether the problem lies with the STM32 or is a signal integrity issue.
If you find that the signal is fine there, use an oscilloscope to measure its actual bit rate precisely. Next, you should verify the actual speed at which the UART on the STM32 is operating (12 Mbit is already very high and may hit the "divider" limits). You can do this either by calculating it from the values read from the registers, or more simply by sending something (to TX) and measuring it with an oscilloscope.

BTW: The manual for the USB-COM485-PLUS2 (Version 1.3) states:
"Serial port speed up to 10Mbps"

MES98Author
Associate II
Apr 10, 2026 3:53 PM UTC

@Pavel A. @Michal Dudka @Andrew Neil @mƎALLEm  @Ozone Thank you for the detailed explanation.

After checking the datasheet more carefully, I realized that the maximum supported speed is actually 10 Mbaud, not 12 Mbaud. However, I am currently unable to communicate reliably even at 8 Mbaud.

I would like to share an important update — I believe I have finally identified the root cause of the issue.

The problem is related to a UART overrun error.

For example:

  • At around 6 Mbaud, if I send data byte by byte, the STM32 is able to receive it correctly
  • In that case, the data accumulates in my ring buffer, and I can process it as expected

However:

  • My actual goal is to send a 4-byte packet at once
  • At higher baud rates (6 / 8 / 10 Mbaud), this causes an overrun, and data is lost

I tried increasing the RX FIFO threshold to FULL, which improved the situation slightly, but I am still only able to reliably receive up to 3 bytes at once


Constraint:

  • I am required to use interrupt-based reception
  • Unfortunately, using DMA is not an option in my case

Question:

Is there any recommended way to handle high baud rate UART reception (6–10 Mbaud) using interrupts only, without causing overrun?

Are there specific FIFO, interrupt, or buffering strategies that could help in this scenario?


Any suggestions or best practices would be greatly appreciated.

Andrew Neil
Super User
Apr 10, 2026 4:04 PM UTC

@MES98 wrote:
  • I am required to use interrupt-based reception

Why ?

This is exactly the kind of situation that DMA is for!

As @Ozone said previously, "High interrupt loads ... can easily consume most of the available core performance".

That's why we have  DMA - to offload that burden!

 

You haven't shown your code - how are you handling the interrupt?

It will probably need to be well-optimised - straight HAL probably won't hack it.

How to insert source code

 


@MES98 wrote:

Is there any recommended way to handle high baud rate UART reception .


DMA.

 


@MES98 wrote:

 

Any suggestions or best practices 


Use DMA.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.