Skip to main content
Associate III
Jun 6, 2024 1:16 PM UTC
Solved

STM32H5 ECC errors and ICACHE invalidation

Should ICACHE be invalidated when a double ECC error occurs?

This topic has been closed for replies.
Sarra.SBest answer
ST Employee
Jun 20, 2024 8:56 AM UTC

Hello @PieterG, sorry for the delayed answer, 

When two ECC errors occur during a read, the flash interface sets the double error detection flag ECCD in the FLASH_ECCDETR register

and when this flag is raised, an NMI is generated, and the software must invalidate the instruction cache (CACHEINV = 1) in the NMI interrupt service routine when the ECCD flag is set.

I hope that answers your question! 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

6 replies

ST Employee
Jun 7, 2024 3:55 PM UTC
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
PieterGAuthor
Associate III
Jun 7, 2024 5:54 PM UTC

Maybe I've overlooked it, but I have read the article several times and it does not mention how ECC errors are to be handled?

 

I am quite sure that I read about invalidating ICACHE after a double ECC error, but I cannot find it anymore in the official documentation, nor any of the examples.

Does it make any sense to invalidate ICACHE when a double ECC error occurs in FLASH? Or is there no need for that? 

Sarra.SBest answer
ST Employee
Jun 20, 2024 8:56 AM UTC

Hello @PieterG, sorry for the delayed answer, 

When two ECC errors occur during a read, the flash interface sets the double error detection flag ECCD in the FLASH_ECCDETR register

and when this flag is raised, an NMI is generated, and the software must invalidate the instruction cache (CACHEINV = 1) in the NMI interrupt service routine when the ECCD flag is set.

I hope that answers your question! 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
PieterGAuthor
Associate III
Jun 20, 2024 9:43 AM UTC

Thank you @Sarra.S for your answer.

I guess invalidating the ICACHE is only necessary when ICACHE is enabled for the flash sector in which the error occurred? (in other words, I do not have to invalidate ICACHE for double ECC errors in OTP / EDATA for which I disabled caching in the MPU)

ST Employee
Jun 20, 2024 10:39 AM UTC

Yes! 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.