Skip to main content
MTE_MMO
Associate
March 31, 2022
Solved

STM32G0B1 EXTI DMA GPIO

Hello dear All,

On STM32G0B1 I'm trying to capture PORTD[0-7] value with DMA on EXTI0 event (PD0 falling edge)

(Read PORTD value in EXTI0 interrupt is too slow for this application -> PORTD change value before entering IRQHandler())

I configure EXTI and DMA2_Ch3 in MX but PORTD value is NOT trasfered in my destination variable on event.

However, by using HAL_DMA_Start_IT(), function DMA1_Ch4_7_DMA2_Ch1_5_DMAMUX1_OVR_IRQHandler() is called.

Could you please help me to do a well configuration in order to transfert PORTD->IRD value in my destination variable "u8_tst_1" with DMA on PD0 falling edge event ? :|

Let see source code below.

My Environment:

STM32CubeIDE v1.8.0

STM32CubeMX v6.4.0-RC4

STM32Cube_FW_G0_V1.5.0

NUCLEO-G0B1RE

Windows 10 Pro 21H2

/* Private variables ---------------------------------------------------------*/
DMA_HandleTypeDef hdma_dma_generator0;
/* USER CODE BEGIN PV */
volatile uint8_t u8_tst_1;
/* USER CODE END PV */
 
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_DMA_Init(void);
/* USER CODE BEGIN PFP */
 
/* USER CODE END PFP */
 
/**
 * @brief The application entry point.
 * @retval int
 */
int main(void)
{
 /* USER CODE BEGIN 1 */
 
 /* USER CODE END 1 */
 
 /* MCU Configuration--------------------------------------------------------*/
 
 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();
 
 /* USER CODE BEGIN Init */
 
 /* USER CODE END Init */
 
 /* Configure the system clock */
 SystemClock_Config();
 
 /* USER CODE BEGIN SysInit */
 
 /* USER CODE END SysInit */
 
 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_DMA_Init();
 /* USER CODE BEGIN 2 */
 HAL_DMAEx_EnableMuxRequestGenerator(&hdma_dma_generator0);
 HAL_DMA_Start_IT(&hdma_dma_generator0, (uint32_t)&GPIOD->IDR, (uint32_t)&u8_tst_1, 1);
 /* USER CODE END 2 */
 
 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 while (1)
 {
 /* USER CODE END WHILE */
 
 /* USER CODE BEGIN 3 */
 }
 /* USER CODE END 3 */
}
 
 
/**
 * Enable DMA controller clock
 * Configure DMA for memory to memory transfers
 * hdma_dma_generator0
 */
static void MX_DMA_Init(void)
{
 /* Local variables */
 HAL_DMA_MuxRequestGeneratorConfigTypeDef pRequestGeneratorConfig = {0};
 
 /* DMA controller clock enable */
 __HAL_RCC_DMA2_CLK_ENABLE();
 
 /* Configure DMA request hdma_dma_generator0 on DMA2_Channel3 */
 hdma_dma_generator0.Instance = DMA2_Channel3;
 hdma_dma_generator0.Init.Request = DMA_REQUEST_GENERATOR0;
 hdma_dma_generator0.Init.Direction = DMA_PERIPH_TO_MEMORY;
 hdma_dma_generator0.Init.PeriphInc = DMA_PINC_DISABLE;
 hdma_dma_generator0.Init.MemInc = DMA_MINC_DISABLE;
 hdma_dma_generator0.Init.PeriphDataAlignment = DMA_PDATAALIGN_BYTE;
 hdma_dma_generator0.Init.MemDataAlignment = DMA_MDATAALIGN_BYTE;
 hdma_dma_generator0.Init.Mode = DMA_NORMAL;
 hdma_dma_generator0.Init.Priority = DMA_PRIORITY_VERY_HIGH;
 if (HAL_DMA_Init(&hdma_dma_generator0) != HAL_OK)
 {
 Error_Handler( );
 }
 
 /* Configure the DMAMUX request generator for the selected DMA channel */
 pRequestGeneratorConfig.SignalID = HAL_DMAMUX1_REQ_GEN_EXTI0;
 pRequestGeneratorConfig.Polarity = HAL_DMAMUX_REQ_GEN_FALLING;
 pRequestGeneratorConfig.RequestNumber = 1;
 if (HAL_DMAEx_ConfigMuxRequestGenerator(&hdma_dma_generator0, &pRequestGeneratorConfig) != HAL_OK)
 {
 Error_Handler( );
 }
 
 /* DMA interrupt init */
 /* DMA1_Ch4_7_DMA2_Ch1_5_DMAMUX1_OVR_IRQn interrupt configuration */
 HAL_NVIC_SetPriority(DMA1_Ch4_7_DMA2_Ch1_5_DMAMUX1_OVR_IRQn, 0, 0);
 HAL_NVIC_EnableIRQ(DMA1_Ch4_7_DMA2_Ch1_5_DMAMUX1_OVR_IRQn);
}
 
 
/**
 * @brief GPIO Initialization Function
 * @param None
 * @retval None
 */
static void MX_GPIO_Init(void)
{
 GPIO_InitTypeDef GPIO_InitStruct = {0};
 
 /* GPIO Ports Clock Enable */
 __HAL_RCC_GPIOD_CLK_ENABLE();
 
 /*Configure GPIO pin : CLK_L1_Pin */ // <- PD0
 GPIO_InitStruct.Pin = CLK_L1_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_IT_FALLING;
 GPIO_InitStruct.Pull = GPIO_PULLUP;
 HAL_GPIO_Init(CLK_L1_GPIO_Port, &GPIO_InitStruct);
}
 
 
/**
 * @brief This function handles DMA1 Ch4 to Ch7, DMA2 Ch1 to Ch5 and DMAMUX1 Overrun Interrupts.
 */
void DMA1_Ch4_7_DMA2_Ch1_5_DMAMUX1_OVR_IRQHandler(void)
{
 /* USER CODE BEGIN DMA1_Ch4_7_DMA2_Ch1_5_DMAMUX1_OVR_IRQn 0 */
 
 /* USER CODE END DMA1_Ch4_7_DMA2_Ch1_5_DMAMUX1_OVR_IRQn 0 */
 HAL_DMA_IRQHandler(&hdma_dma_generator0);
 // Handle DMAMUX
 // Handle DMA2_Channel3
 HAL_DMAEx_MUX_IRQHandler(&hdma_dma_generator0);
 /* USER CODE BEGIN DMA1_Ch4_7_DMA2_Ch1_5_DMAMUX1_OVR_IRQn 1 */
 
 /* USER CODE END DMA1_Ch4_7_DMA2_Ch1_5_DMAMUX1_OVR_IRQn 1 */
}
 

This topic has been closed for replies.
KnarfB
KnarfBBest answer
Super User
April 7, 2022

3 replies

KnarfB
KnarfBBest answer
Super User
April 7, 2022
MZamu.1
Associate
July 15, 2024

Hi all,
I have the same problem on STM32H723.
In the H7 series, GPIO also does not work with DMA?

MTE_MMO
MTE_MMOAuthor
Associate
April 24, 2022

Thanks @KnarfB​ 

Could be great if their is an ST desciption document for DMA compatible modules ?

BR