STM32F446ZE not booting
Hello,
some of our boards do not boot after powering them. We realised that most of the time this happens, the 1.2V at VCAP1 and VCAP2 == 0V. At our boards the BYPASS_REG pin is floating. So there are two questions for us now:
1. Could the floating BYPASS_REG pin cause our Problems?
2. does the BYPASS_REG pin have an internal pulldown resistor?
We also realised, that if we add a 10µF capacitor to the NRST pin, the board will boot everytime. (Normaly there is a 100nF capacitor)
Thank you in advance :)