Skip to main content
shravan
Associate II
June 12, 2017
Question

STM32F429 external nor flash data not persistent using FSMC

  • June 12, 2017
  • 6 replies
  • 1738 views
Posted on June 12, 2017 at 14:24

Hi,

I am using STM32F429ZET6 controller in my custom board. I have used JS28F00AM29EWHA Nor flash from micron.The interface between the controller and external nor is a parallel bus. I have made FMC_Init and GPIO_Init in the following way. I have refereed the 

http://www.st.com/content/ccc/resource/technical/document/application_note/3f/38/6c/cc/0b/7b/41/b7/DM00228015.pdf/files/DM00228015.pdf/jcr:content/translations/en.DM00228015.pdf

 from st for fsmc. I have also cross verified the code from 

https://community.st.com/0D50X00009XkZtLSAV

. My issue is I get wrong manufacturer code and device_id. And also checked with the write and read functionality, but when I reset my debug session and read the previously written addresses I always get zero's. I am not getting where I am going wrong. Any help or suggestion will be of great help.

https://community.st.com/community/stm32-community/stm32-forum

‌

/*fsmc init as follows */

void NOR_FLASH_Init(void)

{

hnor.Instance = FMC_NORSRAM_DEVICE;

hnor.Extended = FMC_NORSRAM_EXTENDED_DEVICE;

hnor.Init.NSBank = FMC_NORSRAM_BANK1;

hnor.Init.DataAddressMux = FMC_DATA_ADDRESS_MUX_DISABLE;

hnor.Init.MemoryType = FMC_MEMORY_TYPE_NOR;

hnor.Init.MemoryDataWidth = FMC_NORSRAM_MEM_BUS_WIDTH_16;

hnor.Init.BurstAccessMode = FMC_BURST_ACCESS_MODE_DISABLE;

hnor.Init.WaitSignalPolarity = FMC_WAIT_SIGNAL_POLARITY_LOW;

hnor.Init.WrapMode = FMC_WRAP_MODE_DISABLE;

hnor.Init.WaitSignalActive = FMC_WAIT_TIMING_BEFORE_WS;

hnor.Init.WriteOperation = FMC_WRITE_OPERATION_ENABLE;

hnor.Init.WaitSignal = FMC_WAIT_SIGNAL_DISABLE;

hnor.Init.ExtendedMode = FMC_EXTENDED_MODE_ENABLE;

hnor.Init.AsynchronousWait = FMC_ASYNCHRONOUS_WAIT_DISABLE;

hnor.Init.WriteBurst = FMC_WRITE_BURST_DISABLE;

hnor.Init.ContinuousClock = FMC_CONTINUOUS_CLOCK_SYNC_ONLY;

hnor.Init.PageSize = FMC_PAGE_SIZE_NONE;

/* Timing */

NOR_Timing.AddressSetupTime = 15;

NOR_Timing.AddressHoldTime = 15;

NOR_Timing.DataSetupTime = 10;

NOR_Timing.BusTurnAroundDuration = 15;

NOR_Timing.CLKDivision = 16;

NOR_Timing.DataLatency = 17;

NOR_Timing.AccessMode = FMC_ACCESS_MODE_B;

/* ExtTiming */

ExtTiming.AddressSetupTime = 15;

ExtTiming.AddressHoldTime = 15;

ExtTiming.DataSetupTime = 255;

ExtTiming.BusTurnAroundDuration = 15;

ExtTiming.CLKDivision = 16;

ExtTiming.DataLatency = 17;

ExtTiming.AccessMode = FMC_ACCESS_MODE_B;

/* Initialize the NOR controller */

if (HAL_NOR_Init(&hnor, &NOR_Timing, &NOR_Timing) != HAL_OK)

{

/* Initialization Error */

while(1);

}

/*♯♯-2- Read & Check the NOR device IDs ♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯*/

/* Read NOR memory ID */

if(HAL_NOR_Read_ID(&hnor, &NOR_Id) != HAL_OK)

{

/* NOR read ID Error */

while(1);

}

/* Test the NOR ID correctness */

if((NOR_Id.Manufacturer_Code != (uint16_t)MANUFACTURER_CODE) ||

(NOR_Id.Device_Code1 != (uint16_t)DEVICE_CODE1))

{

/* NOR ID not correct */

//while(1);

}

/*♯♯-3- Erase NOR memory ♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯*/

/* Return to read mode */

HAL_NOR_ReturnToReadMode(&hnor);

/* Erase the NOR memory block to write on */

HAL_NOR_Erase_Block(&hnor, WRITE_READ_ADDR, NOR_BANK_ADDR);

/* Return the NOR memory status */

if(HAL_NOR_GetStatus(&hnor, NOR_BANK_ADDR, NOR_TIMEOUT_VALUE) !=

HAL_NOR_STATUS_SUCCESS)

 {

 while(1);

 }

}

/***GPIO init **/

static void MX_GPIO_Init(void)

{

GPIO_InitTypeDef GPIO_Init_Structure;

// Enable FMC clock

__HAL_RCC_FMC_CLK_ENABLE();

// Enable GPIOs clock

__HAL_RCC_GPIOD_CLK_ENABLE();

__HAL_RCC_GPIOE_CLK_ENABLE();

__HAL_RCC_GPIOF_CLK_ENABLE();

__HAL_RCC_GPIOG_CLK_ENABLE();

// Common GPIO configuration

GPIO_Init_Structure.Mode = GPIO_MODE_AF_PP;

GPIO_Init_Structure.Pull = GPIO_NOPULL;

GPIO_Init_Structure.Speed = GPIO_SPEED_HIGH;

GPIO_Init_Structure.Alternate = GPIO_AF12_FMC;

//Data and address lines

GPIO_Init_Structure.Pin = GPIO_PIN_0 | GPIO_PIN_1 | GPIO_PIN_8 | GPIO_PIN_9 | GPIO_PIN_10| GPIO_PIN_11| GPIO_PIN_12 | GPIO_PIN_13 |

GPIO_PIN_14| GPIO_PIN_15;

HAL_GPIO_Init(GPIOD, &GPIO_Init_Structure);

GPIO_Init_Structure.Pin = GPIO_PIN_2 | GPIO_PIN_3 | GPIO_PIN_4 | GPIO_PIN_5 | GPIO_PIN_6 |

GPIO_PIN_7 | GPIO_PIN_8 | GPIO_PIN_9 | GPIO_PIN_10 | GPIO_PIN_11 |

GPIO_PIN_12 | GPIO_PIN_13 | GPIO_PIN_14 | GPIO_PIN_15;

GPIO_Init_Structure.Mode = GPIO_MODE_AF_PP;

GPIO_Init_Structure.Pull = GPIO_NOPULL;

GPIO_Init_Structure.Speed = GPIO_SPEED_HIGH;

GPIO_Init_Structure.Alternate = GPIO_AF12_FMC;

HAL_GPIO_Init(GPIOE, &GPIO_Init_Structure);

GPIO_Init_Structure.Pin = GPIO_PIN_0 | GPIO_PIN_1 | GPIO_PIN_2 | GPIO_PIN_3 | GPIO_PIN_4 | GPIO_PIN_5 | GPIO_PIN_12 | GPIO_PIN_13 | GPIO_PIN_14 | GPIO_PIN_15;

GPIO_Init_Structure.Mode = GPIO_MODE_AF_PP;

GPIO_Init_Structure.Pull = GPIO_NOPULL;

GPIO_Init_Structure.Speed = GPIO_SPEED_HIGH;

GPIO_Init_Structure.Alternate = GPIO_AF12_FMC;

HAL_GPIO_Init(GPIOF, &GPIO_Init_Structure);

GPIO_Init_Structure.Pin = GPIO_PIN_0 | GPIO_PIN_1 | GPIO_PIN_2 | GPIO_PIN_3 | GPIO_PIN_4 | GPIO_PIN_5 | GPIO_PIN_13 | GPIO_PIN_14;

GPIO_Init_Structure.Mode = GPIO_MODE_AF_PP;

GPIO_Init_Structure.Pull = GPIO_NOPULL;

GPIO_Init_Structure.Speed = GPIO_SPEED_HIGH;

GPIO_Init_Structure.Alternate = GPIO_AF12_FMC;

HAL_GPIO_Init(GPIOG, &GPIO_Init_Structure);

Thanks.

#fmc #stm32f4-external-nor-flash #flash-read-and-write #js28f00am29ewha
This topic has been closed for replies.

6 replies

Tesla DeLorean
Guru
July 18, 2017
Posted on July 18, 2017 at 15:09

>>

My issue is I get wrong manufacturer code and device_id

So what does it read? If the data bus is wrong then the chip is unlikely to recognize the commands sent to it.

Have you thoroughly reviewed the schematic design?

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
waclawek.jan
Super User
July 18, 2017
Posted on July 18, 2017 at 15:16

Have you thoroughly reviewed the schematic design?

One remark for debugging: parallel memories can be easily 'bit-banged', ie. the protocol can be easily tested by 'manually' manipulating the address/data/control lines, with pins set as GPIO inputs/outputs as appropriate, rather than AF.

This can be done from the debugger, without a single line of code.

JW

shravan
shravanAuthor
Associate II
July 19, 2017
Posted on July 19, 2017 at 10:28

Hi JW,

I am not getting how to proceed. Could you please elaborate on the method you mentioned in your reply.

Regards,

Shravan