STM32F4: changing clock speed dynamically (runtime). What do I need to look out for?
I'm writing an application for a STM32F407 that requires very high speed ADC for 6 channels (two for each ADC, using regular simultaneous scanned mode), then once a series of conditions are met, perform quite a few cross correlation calculations for very long sequences, requiring the fastest performance possible. I'm using the SPL libraries, incidentally, not the HAL/CubeMX
Due to how the clocks work on a F407, the fastest ADC conversion cycle happens with a 144MHz clock. But the max clock is 168MHz, and that's ~16% faster when performing DSP operations. I do understand how to set the clock for both 144MHz and 168MHz, with all the right PLL_M, N, P and Q values
I was thinking of setting the board up at boot with 144MHz. sample with the fastest ADC clock and, once my conditions are met, switch the clock to 168MHz before performing the cross correlations. Whatever time it takes to dynamically change the clock, I'll more than make it up while running the long (>2 seconds) calculations 16% faster
This article seems to indicate a way to do it http://embeddedsystemengineering.blogspot.com/2015/06/stm32f4-discovery-tutorial-4-configure.html
What would happen if I boot the system with 144MHz clock, switch to 168MHz, then back to 144MHz for another cycle and so on? It seems to work, but I'm not sure if I'm missing any downside not showing up in a short test (or reliability issues over time). I also plan to use USB, so I understand the need to always have a 48MHz clock for that