Skip to main content
hello
Associate III
June 20, 2012
Question

STM32F107VC CAN bus pin remap

  • June 20, 2012
  • 20 replies
  • 4300 views
Posted on June 20, 2012 at 23:19

hi.

i am using the STM32F107VC board from IAR i have some example code for CAN but in my Board they used the PD0 and PD1 for CAN i dont know how to remap it in my code. i have 2 board and i want to sent data between 2 boards.

void GPIO_Configuration(void)

{

  GPIO_InitTypeDef  GPIO_InitStructure;

  

 // GPIO_PinRemapConfig(GPIO_Remap2_CAN1 , ENABLE);

  /* Configure CAN pin: RX */

  //GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0;

  GPIO_InitStructure.GPIO_Pin = GPIO_Pin_CAN_RX;

  GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IPU;

  GPIO_Init(GPIO_CAN, &GPIO_InitStructure);

  

  /* Configure CAN pin: TX */

  //GPIO_InitStructure.GPIO_Pin = GPIO_Pin_1;

  GPIO_InitStructure.GPIO_Pin = GPIO_Pin_CAN_TX;

  GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP;

  GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;

  GPIO_Init(GPIO_CAN, &GPIO_InitStructure);

  

  GPIO_PinRemapConfig(GPIO_Remap_CAN , ENABLE);

}

can any one pls help me solve this problem..

thanks...

    This topic has been closed for replies.

    20 replies

    Tesla DeLorean
    Guru
    June 20, 2012
    Posted on June 21, 2012 at 00:50

    Probably not enabling the AFIO clock.

    /* Enable GPIOD and AFIO clocks for remapping */
    RCC_APB2PeriphClockCmd(RCC_APB2Periph_AFIO | RCC_APB2Periph_GPIOD, ENABLE);
    /* Configure CAN1 RX pin */
    GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0;
    GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IPU;
    GPIO_Init(GPIOD, &GPIO_InitStructure);
    /* Configure CAN1 TX pin */
    GPIO_InitStructure.GPIO_Pin = GPIO_Pin_1;
    GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP;
    GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
    GPIO_Init(GPIOD, &GPIO_InitStructure);
    /* Remap CAN1 GPIOs */
    GPIO_PinRemapConfig(GPIO_Remap2_CAN1 , ENABLE); /* PD 0 and 1 */
    /* CAN1 Periph clock enable */
    RCC_APB1PeriphClockCmd(RCC_APB1Periph_CAN1, ENABLE);
    /* CAN1 register init */
    CAN_DeInit(CAN1);
    // ...

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    hello
    helloAuthor
    Associate III
    June 20, 2012
    Posted on June 21, 2012 at 01:15

    i change accordingly but It also not working....

    readme.txt say's like

    Connectivity line devices are STM32F105xx and STM32F107xx microcontrollers.

    STM3210C-EVAL (STM32F10x -- Connectivity line)

    my LED r connected in my board to PC.06, PC.07, PC.08 and PC.09 pins

    which suits with set-up 

    - STM3210B-EVAL Set-up  

        - Use LED1, LED2, LED3 and LED4 leds connected respectively to PC.06, PC.07, PC.08

          and PC.09 pins

        - Use Push Button connected to PB9      

        - Connect a female/female CAN cable between at least 2 EVAL CAN connectors 

          (on STM3210B-EVAL (CN2)/ STM3210E-EVAL (CN4) boards) 

          - Connector 1 DB9_PIN2 to Connector 2 DB9_PIN2  (CAN_L)

      - Connector 1 DB9_PIN5 to Connector 2 DB9_PIN5  ( GND )

      - Connector 1 DB9_PIN7 to Connector 2 DB9_PIN7  (CAN_H) 

      @note JP3 must be fitted.

      

    @note Any unit in the CAN bus may play the role of sender (by pressing on the 

          key) or receiver.

    so because of LED i am using STM3210B-EVAL Set-up 

     

    how can i change the LED pin if i use 

    STM3210C-EVAL Set-up 

        - Use LED1, LED2, LED3 and LED4 connected respectively to PD.07, PD.13, PF.03

          and PD.04 pins

        - Use Push Button connected to PB9

        - Connect a female/female CAN cable between at least 2 EVAL CAN connectors 

          (on STM3210E-EVAL (CN2)/ STM3210C-EVAL (CN3) boards)

           - Connector 1 DB9_PIN2 to Connector 2 DB9_PIN2  (CAN_L)

       - Connector 1 DB9_PIN5 to Connector 2 DB9_PIN5  ( GND )

       - Connector 1 DB9_PIN7 to Connector 2 DB9_PIN7  (CAN_H) 

      @note JP6 or JP5 must be fitted.

    as in my board LED r connected to PC.06, PC.07, PC.08 and PC.09 pins

    thanks...

    Tesla DeLorean
    Guru
    June 21, 2012
    Posted on June 21, 2012 at 02:35

    Ok, so what board do you actually have? Does it have a revision number?

    The STM3210C-EVAL, from ST, has CN3 connected to PD0,1 for CAN1 and LD1/LED1 is PD7

    Get a schematic for your IAR board and determine what is connected where.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    hello
    helloAuthor
    Associate III
    June 21, 2012
    Posted on June 21, 2012 at 03:12

    thanks for your reply..

    i use

    IAR KickStart Kit for STM32F107VC

    i have attached theschematic of my board in this.

    in my board the pin are

    LED1(STAT1)- PC6

    LED2(STAT2)- PC7

    LED3(STAT3)- PC8

    LED4(STAT4)- PC9

    CAN1_TX - PD1

    CAN1_RX - PD0

    CAN1_CNTRL - PD14

    there is Jumper settings in my board:

    CAN1_T

    OPEN- CAN1 Termination Disable

    CLOSE- CAN1 Termination Enable(Default)

    i have not change any of jumper its CLOSE i guess...

    thanks...

    ________________

    Attachments :

    IAR-STM32F107VC-SK_REV-1.pdf : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0fw&d=%2Fa%2F0X0000000bea%2FmJ66jtfM39hbTgLWLlmyEJ8r_R87kfybaO3TzS1ZflU&asPdf=false
    Tesla DeLorean
    Guru
    June 21, 2012
    Posted on June 21, 2012 at 04:37

    Then you'll need to configure PD14 as a GPIO output, and drive it appropriately to enable the transceiver. The ST boards have a jumper to VCC or GND

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    hello
    helloAuthor
    Associate III
    June 21, 2012
    Posted on June 21, 2012 at 11:24

    can you please expline me shortly about GPIO config PD14...

    Tesla DeLorean
    Guru
    June 21, 2012
    Posted on June 21, 2012 at 23:15

    can you please expline me shortly about GPIO config PD..

    Really? If I scan the schematic and datasheet correctly :

    /* Configure PD14 in output pushpull mode */
    GPIO_InitStructure.GPIO_Pin = GPIO_Pin_14;
    GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
    GPIO_InitStructure.GPIO_Mode = GPIO_Mode_Out_PP;
    GPIO_Init(GPIOD, &GPIO_InitStructure);
    Then
    GPIO_SetBits(GPIOD, GPIO_Pin_14); // Set Transceiver in Transmit Enable (Dominant when CAN_TX LOW, otherwise Recessive)
    
    or
    GPIO_ResetBits(GPIOD, GPIO_Pin_14); // Set Transceiver in Receive Only
    

    http://www.ti.com/lit/ds/symlink/sn65hvdpdf

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    hello
    helloAuthor
    Associate III
    June 21, 2012
    Posted on June 22, 2012 at 00:51

    Hi,

    thanks for your reply and for your time

    i did so still no change...i am trying it for long time but noting happening...

    Tesla DeLorean
    Guru
    June 21, 2012
    Posted on June 22, 2012 at 01:05

    Time to break out the oscilloscope.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    hello
    helloAuthor
    Associate III
    June 21, 2012
    Posted on June 22, 2012 at 01:25

    Thanks..

    i will check it from my university in morning.

    thanks for your help...

    /* Configures LED 1..4 */

      STM_EVAL_LEDInit(LED1);

      STM_EVAL_LEDInit(LED2);

      STM_EVAL_LEDInit(LED3);

      STM_EVAL_LEDInit(LED4);

    af for configuration for my project it use PD.07, PD.13, PF.03 and PD.04 pins

    but i need to chage it to PC.06, PC.07, PC.08 and PC.09 pins according to my board 

    how it can be done?