Skip to main content
SSaiy.1
Associate III
Feb 13, 2023 1:04 PM UTC
Solved

STM32 L412 Timer interrupt not working

I am using STM32L412 microcontroller and doing baremetal programming for timer interrupt. I am using Timer 6 and base clock of 4MHZ is used as HCLK. However my interrupt is not firing below mentioning my code. count variable is also not updating

int main(void)

{

LedConfig();

StartTimer6();

  /* Loop forever */

while(1)

{

count=1;

}

}

void LedConfig(void)

{

/*Enable Clock for Port B. */

RCC->AHB2ENR |= (1U<<1);

/*Configure GPIOB_13 as general purpose output*/

GPIOB->MODER |= (1U<<26);

GPIOB->MODER &= ~(1U<<27);

}

void StartTimer6(void)

{

RCC->APB1ENR1 |= (1U<<4);

TIM6->PSC = 1000;

TIM6->ARR = 4000;

TIM6->EGR |= (1U<<0);

TIM6->DIER |= (1U<<0);

TIM6->CR1 |= (1U<<0);

NVIC_EnableIRQ(TIM6_IRQn);

}

void TIM6_IRQHandler(void)

{

if(TIM6->SR & (1U<<0))

{

GPIOB->ODR ^= (1U<<13);

TIM6->SR &= ~(1U<<0);

}

}

    This topic has been closed for replies.
    SSaiy.1
    SSaiy.1Best answer
    Associate III
    Feb 14, 2023 10:41 AM UTC

    Thanks @KnarfB as you said IRQ handler was different the actual one is TIM6_DACUNDER_IRQHandler. After I changed the handler name the code started working

    14 replies

    waclawek.jan
    Super User
    Feb 14, 2023 11:01 AM UTC

    Nice catch, @KnarfB​ !

    > TIM6_DACUNDER_IRQHandler

    I've never seen handler name like this. As I've said above, I would like to know where that startup_stm32l412rbtx.s is from.

    JW